--------------
Legal Notices
--------------
© 2006,
UGS Corp.
All Rights Reserved
Software, file formats, and audiovisual displays may be used pursuant to the
applicable Software License Agreement and contain confidential and proprietary
information of UGS Corp.; which is protected by
copyright and trade secret law. Such materials may not be reproduced or
transferred to other documents or used or disclosed to others for manufacturing
or for any other purpose except as specifically authorized within the terms of
the Software License Agreement, or as specifically authorized in writing by
UGS Corp.
UGS Corp.
5800 Granite Parkway
Suite 600
Plano, TX. 75024
--------------------
End of Legal Notices
--------------------
--------------
Release Notes:
--------------
Product: Solid Edge
Version: 18.00.03.04
Date: 17-Feb-2006
This release of Solid Edge has been certified to run on the following:
• Windows XP Professional® operating system (32-bit) running Service Pack 2
• Windows XP Professional® operating system (64-bit) running on EM64T hardware
• Windows 2000 Professional® operating system running Service Pack 4
• Internet Explorer 6.0 or higher
This Update can be instaled installed on top of Version: 18.00.00.69, 18.00.01.08,
or 18.00.02.04.
Note: Updates are all inclusive and can be installed on top of the base release
or any released UPdate.
--------------------
End of Release Notes
--------------------
------------------------------------
This Update addresses the following:
------------------------------------
=====Assembly=====
PR 5366576: Fixed a problem where entries in Calculation Tab do not increment with Japanese version
PR 5370911: Fixed a problem where you cannot select patterned parts in pathfinder when exploding
PR 1494460: Fixed a problem where Peer variables are not working when assembly is opened with all inactive parts.
PR 2060582: Fixed a problem with delimitation line of add-in menu
PR 5336939: Fixed a problem where Assembly feature holes are losing relationships after an edit.
PR 5355277: Fixed a problem where Add buttons (Shaft dialog) are missing directional arrows on Jpn Eng Ref
PR 5361280: Fixed a problem where "edit in SE compression spring designer" doesn't work
PR 5391954: Fixed a problem where Asm is not showing part geometry when a variable in the top level is changed
PR 1476826: Fixed a problem where relationships are not updating after editing parts.
PR 1494338: Fixed a problem where you were unable to convert an assembly to STEP
PR 1494392: Fixed a problem with Standard Parts - English names in German version.
PR 5365219: Fixed a problem with typos in Russian Standard Parts UI
PR 5395519: Fixed a problem where the fillet weld options dialog not showing the correct values when editing a fillet weld.
PR 5384474: Fixed a problem where printing reports truncates column titles on Jpn version
PR 5399647: Fixed a problem with truncated text on a dialog for Extension Spring in Engineering Reference.
PR 5402912: Fixed a problem in Engineering Reference where the teeth in small spurgears will not get created.
=====Part=====
PR 1483470: Fixed a problem that caused when placing Fillet in Sketch with Included edges
PR 2060127: Fixed a problem with incorrect value of mass when 'Show units in value fields' is unchecked.
PR 5313893: Fixed a problem where embedded periods are allowed in FOP member names.
PR 5369357: Fixed a problem where Blue Dots fail to place when the point is a B-spline's control point.
PR 5374396: Fixed a problem where a Step file exported from SEv18 is at the wrong scale
PR 5391741: Fixed a problem where feet and inches do not show up correctly in parts list
PR 2062020: Fixed a problem where "Zoom to Error Elements" does not zoom to the correct elements when part/psm file is in place activated from asm.
PR 1466602: Fixed a problem where a Sheet metal part is not being computed when the material name is changed
=====Draft=====
PR 1451474: Fixed a problem where Drawing views do not trim correctly when exported to AutoCad format.
PR 5372853: Fixed a problem where this draft file fails to save after updating views.
PR 5371659: Fixed a problem where detached dimension can't be re-attached or replaced
PR 5384074: Fixed a problem where you cannot open this Draft file after saving
PR 1494225: Fixed a problem importing DWG into V18 - no problem with V17
PR 1500968: Fixed a problem where dimensions jump to detail views when converting a view to 2D.
PR 2060967: Fixed a problem where Detail View translation does not translate custom border
PR 5384067: Fixed a problem where parts list is not being set out of date after changing occurrence properties.
PR 5404583 : Fixed a problem where multiple 2d model views are created on dwg export paper space
PR 5390686: Fixed a problem where changing a dimension to dual units results in an abort.
PR 1493661: Fixed a problem where V15 user views with non-rectangular cropping become uncropped.
PR 1495867: Fixed a problem with Unable to open Draft File in V18.
PR 5373067: Fixed a problem with Draft views becoming corrupt
PR 5391158: Fixed a problem where a draft file will not open in V18
PR 5403694: Fixed a problem where Dimensions connected to bend centerlines are detaching on file open.
PR 5408896 : Fixed a problem where file size drastically increased when exporting to dwg paper space.
=====API=====
PR 2060032: Added two new API ApprenticeMode and ShowStartupScreen on the Application object
PR 1481190: Fixed a problem where API method CreateReference creates a reference to the wrong sketch
PR 1479222: Fixed a problem with API: SEPartX.OCX
PR 5329905: Added API ModelMember.ShowEdgesHiddenByOtherParts.
=====Insight=====
PR 5389021: Fixed a problem that caused an aborts when opening this file with Solid Edge or RevMan.
PR 5332365: Fixed a problem where STL & JT files are deleted after they are opened in view &markup
PR 5385685: Fixed a problem where Replace with different family member sets action to unchanged
PR 5388175: Fixed a problem where the Add to Library process is not completing when defining a folder contents
PR 5393644: Fixed a problem where the Author Field is getting set back to login name when Auto-save is on.
PR 1495972: Fixed a problem where Draft status is not automatically matching the attached part's status
PR 1499355: Fixed a problem with Where Used not working
PR 5397191: Fixed a problem where you are Unable to Save or use Add to Library for a particular part file
PR 5401669: Fixed a problem where Solid Edge search is crashing the w3wp.exe (SharePoint) process.
PR 5404652: Fixed a problem revising a part
---
End
---