--------------
Legal Notices
--------------
© 2006,
UGS Corp.
All Rights Reserved
Software, file formats, and audiovisual displays may be used pursuant to the
applicable Software License Agreement and contain confidential and proprietary
information of UGS Corp.; which is protected by
copyright and trade secret law. Such materials may not be reproduced or
transferred to other documents or used or disclosed to others for manufacturing
or for any other purpose except as specifically authorized within the terms of
the Software License Agreement, or as specifically authorized in writing by
UGS Corp.
UGS Corp.
5800 Granite Parkway
Suite 600
Plano, TX. 75024
--------------------
End of Legal Notices
--------------------
--------------
Release Notes:
--------------
Product: Solid Edge
Version: 18.00.04.07
Date: 31-Mar-2006
This release of Solid Edge has been certified to run on the following:
• Windows XP Professional® operating system (32-bit) running Service Pack 2
• Windows XP Professional® operating system (64-bit) running on EM64T hardware
• Windows 2000 Professional® operating system running Service Pack 4
• Internet Explorer 6.0 or higher
This Update can be instaled installed on top of Version: 18.00.00.69, 18.00.01.08,
18.00.02.04, or 18.00.03.04.
Note: Updates are all inclusive and can be installed on top of the base release
or any released UPdate.
Note: PR#5434509 was uncovered while preparing to release / post Update 4. A decision
was made to release Update 4 with this known issue. - - PR#5434509: When Hide Previous
Level is enabled, parts cannot be graphically (geometry in the screen) located in a
subassy that has been in-place activated. Workaround: You can locate these parts by;
turning off Hide Previous Level, or locate them in path-finder, or by dragging the
cursor to create a small fence locate. This will be addressed in V18 Update 5.
--------------------
End of Release Notes
--------------------
------------------------------------
This Update addresses the following:
------------------------------------
=====Assembly=====
PR 1502640: Fixed a problem that caused an abort in FlashFit when hitting Flip after a circular dependency error.
PR 5371628: Fixed a problem that caused an abort when deleting a relationship from the ribbon bar.
PR 5407218: Fixed a problem where an assembly file fails to open.
PR 2060309: Fixed a problem where you are Unable to select parts from view
PR 2063432: Fixed a problem where you can't restore an autobackup file to network folder.
PR 5347858: Fixed a problem where part features are not reflected at the top-level
PR 5353329: Fixed a problem where Sketch is fully constrained while it shouldn't be.
PR 5373421: Fixed a problem where adding a horizontal alignment in hole 28 causes holes to fail.
PR 5392740: Fixed a problem where a part flagged not to include in interference checking is being included
PR 5398842: Fixed a problem where Measure Distance is not locating points on a flat pattern when IPA from assembly.
PR 1494392: Fixed a problem where a standard part had an English name in the German version
PR 1503322: Fixed a problem where Part modifications will revert when a display configuration is applied.
PR 2062548: Fixed a problem where in an assembly file would not open.
PR 5301348: Fixed a problem where Fasteners are not positioned relative to the member in the drawing views.
PR 5403234: Fixed a problem where Line segments and dimensions disappear.
PR 5408943: Fixed a problem with a wrapped image in Virtual Studio v18
PR 1507327: Added "Subject" to the list of properties available to display in Edgebar.
PR 5402086: Fixed a problem where Peer variables don't work for released parts.
PR 5422617: Fixed a problem where using SAVE AS from a READONLY file does work properly
=====Part=====
PR 1496205: Fixed a problem where you get a stack overflow when clicking on middle mouse button
PR 1471984: Fixed a problem where flat pattern fails when recomputing a V14 part
Jeff W - PR 5301382: Fixed a problem where an inserted part copy won't save
PR 5373855: Fixed a problem where the Weight is wrong in an HTML report from FEMAP Express
PR 5391641: Fixed a memory issue while loading Parasolid files using SolidEdge API
PR 5391891: Fixed a problem where Contour Curve is not accepting the selection changes
PR 1480280: Fixed a problem where a Swept Cutout failing with a wrapped sketch on a cone has been fixed.
PR 5384360: Fixed a problem where Flat Pattern fails if start point of flange is changed and a cutout is present.
PR 5414713: Fixed a problem where FOP members Material gets reset to parent material if populated
PR 2063942: Fixed a problem where Select step causes an abort editing a pattern
=====Draft=====
PR 5386121: Fixed a problem where Edge crashes after closing this drawing
PR 5402899: Fixed a problem where Solid Edge aborts when opening an AutoCAD file in draft
PR 5406560: Fixed a problem where SE crashes when updating an assembly in a draft
PR 5353407: Fixed a problem where you are unable to map Jpn fonts in ACAD Translation Wizard
PR 5367991: Fixed a problem where imbedded Word documents do not export to DWG
PR 5373067: Fixed a problem where a Draft view become Corrupt
PR 5373444: Fixed a problem where bend centerlines on cropped views disappear after update.
PR 5374191: Fixed a problem where Cutting planes which are turned off are still being located.
PR 5390692: Fixed a problem where Surface finish symbols do not export correctly to dwg from V18 draft.
PR 5391041: Fixed a problem where existing callout without leader change justification when edited.
PR 5394823: Fixed a problem where Balloon item number linked to the parts list is showing wrong item number.
PR 5400843: Fixed a problem where changes to style resets overrides on existing elements
PR 1494809: Fixed a problem where sketches from an assembly shown in a drawing view disappear on update.
PR 1505075: Fixed a problem where Draft cannot be translated to DXF
PR 2063758: Fixed a problem that caused some V16 files to fail to open in V17 or V18.
PR 5331934: Fixed a problem where Only part of fill is translating out to DXF
PR 5374713: Fixed a problem where threads do not show up in part that was once cut.
PR 5402235: Fixed a problem where you get incorrect VHL results on a drawing
PR 5405662: Fixed a problem where an arc from v17 incorrectly displays in v18
PR 5412003: Fixed a problem where show/hide edge changes don't work on segments.
PR 5414898: Fixed a problem where changing dimension style roundoff caused property text size changed
PR 5415760: Fixed a problem with DXF files created using V18 Update 3 are blank
PR 5417868: Fixed a problem that caused an Abort when autoballooning a view with an elliptical cropping boundary.
PR 5415676: Fixed a problem where Save as flag doesn't work correctly
PR 5416704: Fixed a problem where Draft files exported to DWG have a box around every view
PR 1496861: Changed the functionality associated with being able to drag an arrowhead away from its witness line.
PR 5390692: Fixed a problem where Surface finish symbols do not export correctly to dwg from V18 draft.
=====API=====
PR 2060417: Fixed a problem where Model does not show up
PR 2063313: Fixed a problem where FOA member custom properties are not accessible using propauto
PR 5402070: Fixed a problem where Replace link fails on managed family of assy through API
=====Insight=====
PR 2055062: Fixed a problem where VB encountered error viewing using SEPARTX and SEDRAFTX via web
PR 1503794: Fixed a problem where Solid edge files cannot be revised via Insight Connect
PR 5403688: Fixed a problem where Folder path with ' character no longer appears to be valid
PR 1500061: Fixed a problem with poor performance when copying with insight a big assembly.
PR 5415963: Fixed a problem where View & Markup closes while using "Compare to Original Document"
PR 5417876: Added more logging to Diagnose the where-used query problem.
---
End
---