--------------
Legal Notices
--------------
© 2006,
UGS Corp.
All Rights Reserved
Software, file formats, and audiovisual displays may be used pursuant to the
applicable Software License Agreement and contain confidential and proprietary
information of UGS Corp.; which is protected by
copyright and trade secret law. Such materials may not be reproduced or
transferred to other documents or used or disclosed to others for manufacturing
or for any other purpose except as specifically authorized within the terms of
the Software License Agreement, or as specifically authorized in writing by
UGS Corp.
UGS Corp.
5800 Granite Parkway
Suite 600
Plano, TX. 75024
--------------------
End of Legal Notices
--------------------
--------------
Release Notes:
--------------
Product: Solid Edge
Version: 18.00.07.04
Date: 19-Jul-2006
This release of Solid Edge has been certified to run on the following:
• Windows XP Professional® operating system (32-bit) running Service Pack 2
• Windows XP Professional® operating system (64-bit) running on EM64T hardware
• Windows 2000 Professional® operating system running Service Pack 4
• Internet Explorer 6.0 or higher
This Update can be instaled installed on top of Version: 18.00.00.69, 18.00.01.08,
18.00.02.04, 18.00.03.04, 18.00.04.07, 18.00.05.05, or 18.00.06.06.
Note: Updates are all inclusive and can be installed on top of the base release
or any released UPdate.
Note: PR#5434509 was uncovered while preparing to release / post Update 4. A decision
was made to release Update 4 with this known issue. - - PR#5434509: When Hide Previous
Level is enabled, parts cannot be graphically (geometry in the screen) located in a
subassy that has been in-place activated. Workaround: You can locate these parts by;
turning off Hide Previous Level, or locate them in path-finder, or by dragging the
cursor to create a small fence locate. This will be addressed in V18 Update 5.
--------------------
End of Release Notes
--------------------
------------------------------------
This Update addresses the following:
------------------------------------
=====Assembly=====
PR 1500611: Fixed a problem where the Move Part collision option is behaving incorrectly.
PR 1516387: Fixed a problem where paths in XpresRoute disappear
PR 1530538: Fixed a problem where reflections are not visible if using a reflection box without "use for background"
PR 5021760: Fixed a problem where it is difficult to locate sketch elements when over a reference plane
PR 5516161: Fixed a problem where you cannot mirror parts if assembly is managed and path is changed
PR 5529513: Fixed a problem where wire report is not available in XpresRoute through customize
PR 1529044: Fixed a problem where tube paths are no longer visible
PR 5521959: Fixed a problem where adding status to document name formula for released parts does not work
PR 5549358: Fixed a problem where SE to jt translator doesn't honor LinkMgmt.txt MAP settings.
PR 5552460: Fixed a problem where assembly weldment is not showing in summary of atomic parts list.
PR 1410066: Fixed a problem where it is impossible to programmatically get name of AssemblyFeaturesExtrudedCutout
PR 1533596: Fixed a problem where you get an incorrect Cut Length when the Apply Radius option is ON
PR 5523652: Fixed a problem where FOA will not update after being copied with Revision Manager
PR 5544345: Fixed a problem where [Rename] action is setting the file attribute to read-only
=====Part=====
PR 1482704: Fixed a problem where Insert > Partcopy (FOP) causes to insert wrong members
PR 2067011: Fixed a problem where Solid edge freezes when the cursor passes over the model.
PR 2067805: Fixed a problem where an Element highlighted incorrectly using the Include command.
PR 5398364: Fixed a problem where you cannot flatten a mirrored sheetmetal part
PR 2067655: Fixed a problem where a 2-Bend Closed Corner fails
PR 5530972: Fixed a problem where a Formula in suppression variable is going away
PR 5558508: Fixed a problem where you cannot flatten a specific sheetmetal model with flanges
=====Draft=====
PR 2067514: Fixed a problem where Solid Edge aborts when updating view in this file.
PR 5512481: Fixed a problem where Editing, Saving As Flat and returning to assembly various times causes aborts
PR 5400796: Fixed a problem where a rotated a detail view disappeared
PR 1507202: Fixed a problem where Points do not export do DXF
PR 1515139: Fixed a problem where V16 smartframe geometry is sized wrong in V18
PR 1519812: Fixed a problem where Dimensions detach after forcing an update
PR 1526471: Fixed a problem where thread dimension values do not display if link to assembly is broken
PR 1527185: Fixed a problem where changing a block property raises an error after undo.
PR 5527798: Fixed a problem where dims are becoming detached in psm files after changing the material thickness
PR 2065591: Fixed an abort that occurred when clicking Bring to Front/Send to Back on a cutting plane line.
PR 2068530: Fixed a problem with Solid Edge API "Callout Properties"
PR 1532632: Fixed a problem where Solid Edge aborts when editing feature control frame properties.
PR 2068664: Fixed a problem where Solid Edge aborts when updating hole table.
PR 1519659: Fixed a problem where Block style overrides are ignored when printing as black.
PR 1534053: Fixed a problem where Solid Edge aborts when updating hole table.
=====API=====
PR 5418443: Fixed a problem resetting the link resolution property in Revision Manager API.
PR 1533978: Fixed a problem where a Macro will not change the color of a cutting plane line.
PR 1507804: Fixed a problem where you are unable to create assembly features using the APIs
PR 5556450: Enabled Migration commands with a Solid Edge Foundation License
PR 2067772: Need API for "Subfix 2" of dimension Prefix, added function SubfixString2.
PR 2067773: Need API for "Subfix horizontal alignment" of dimension Prefix, Added function SubfixAlignment and SubfixAlignmentConstants - seSubfixAlignLeft and seSubfixAlignCenter
=====Insight=====
PR 1515237: Fixed a problem regarding SEStatus and a multinational Insight environment
PR 1525159: Fixed a problem where revise drawing with Family of Assembly doesn't work correctly
PR 1528447: Fixed a problem where an Assembly cannot be opened - Open window disappears
PR 1523765: Fixed a problem where Insight managed SE file Binder has links to office documents
PR 5554781: Added a registry switch to control LCA Obsolete status documents
PR 5553515: Fixed a problem where deleting the first/orig file attached to PCF View & Markup aborts
PR 1534489: Fixed a problem where a Cookie file of the config file is not deleted while moving assembly file.
---
End
---