Solid Edge ST7 SDK
Solid Edge V19 SP4 - Readme

--------------
Legal Notices
--------------
© 2007,
UGS Corp.

All Rights Reserved
Software, file formats, and audiovisual displays may be used pursuant to the
applicable Software License Agreement and contain confidential and proprietary
information of UGS Corp.; which is protected by
copyright and trade secret law.  Such materials may not be reproduced or
transferred to other documents or used or disclosed to others for manufacturing
or for any other purpose except as specifically authorized within the terms of
the Software License Agreement, or as specifically authorized in writing by
UGS Corp.

UGS Corp.
5800 Granite Parkway
Suite 600
Plano, TX. 75024

--------------------
End of Legal Notices
--------------------

--------------
Release Notes:
--------------

Product:        Solid Edge
Version:        19.00.04.06
Date:           22-Mar-2007


This release of Solid Edge has been certified to run on the following:
    • Windows XP Professional® operating system (32 bit or 64 bit)
    • Internet Explorer 6.0 or higher

This Update can be instaled installed on top of Version: 19.00.00.66, 19.00.01.06,
19.00.02.06, or 19.00.03.06.

Note: Updates are all inclusive and can be installed on top of the base release
or any released UPdate.

--------------------
End of Release Notes
--------------------

----------------------------------------------------------
This Update addresses the following Customer Reported PRs:
----------------------------------------------------------

=====Assembly=====

PR 1498424: Fixed a problem where LinkMgnt.txt Search Path will not be used to solve broken links to texture files
PR 1499959: Fixed a problem where Solid Edge takes a long time to update an assembly with several interpart variables.
PR 1520564: Fixed a problem where an assembly hole feature is not cutting all the holes shown in the profile.
PR 1559755: Fixed a problem where Piping Route/Library is enabled without sepipingcomponents feature in license
PR 1564210: Fixed a problem where you cannot place second dimension in XpresRoute
PR 1571825: Fixed a problem with pattern of occurrences in an alternate assembly
PR 1572365: Fixed a problem where you are not able to change part properties of a weldment assembly.
PR 2069332: Fixed a problem where a sketch is modified and some of the frames reset
PR 2070297: Fixed a problem where an assembly will not save to IDF (PCBto3D) file
PR 2074467: Fixed a problem where assembly feature performance of 100+ features.
PR 5125289: Fixed a problem where an assembly report from Windows Explorer returning the incorrect quantity
PR 5331886: Fixed a problem where assembly reference planes are always on when in-place activated from Draft
PR 5444563: Fixed a problem where replacing an adj part in an FOA member causes other members to be incorrect.
PR 5552702: Fixed a problem in which assembly fence select, selects parts it shouldn't while in a top view.
PR 5650024: Fixed a problem where you cannot change Mate offset values to less than .001 mm.
PR 5651720: Fixed a problem where performance is impacted while trimming profiles in this assembly
PR 5677914: Fixed a problem where the Tube.BendTable API doesn't produce the correct results.
PR 5688357: Fixed a problem where a SaveAs on an assembly file changes the timestamp on the original asm's config file
PR 5551783: Fixed a problem where selecting faces when placing subassemblies using the Place Part window.
PR 5693785: Fixed a problem where saving a simplified assembly part fails the first time.
PR 5694894: Fixed a problem where an adjustable part is not working correctly when its variable is changed.
PR 5696460: Fixed a problem where a Switch/Retry message is generated when creating a frame in a subassembly.
PR 1567740: Fixed a problem where plane dynamics is not working for Plane Normal to Curve in an assembly.
PR 1571986: Fixed a problem where Solid Edge is hanging when trying to place a part in some situations.
PR 1577703: Fixed a problem where Solid Edge crashed after updating physical properties.
PR 5696834: Fixed a problem where Solid Edge crashed when calling activate on a part
PR 1536546: Fixed a problem where piping is not placed correct - Multiple solutions
PR 1546915: Fixed a problem where no parts are available in the V19 Standard Part Delivery Database.
PR 1553986: Fixed a problem where a Subasssembly will be saved after placement in another assy
PR 5699692: Fixed a problem where failed weldment features was causing poor view performance
PR 1574891: Fixed a problem where Basic Rendering in SE Foundation issues "invalid license" dialog.
PR 1579298: Fixed a problem where there are pipe fittings present in the file that are not related to the Pipe object
PR 5577293: Fixed a problem where Save As Movie is not active if animation is created
PR 5657892: Fixed a problem where Simplified assemblies is giving wrong result.
PR 5708925: Fixed a problem where Assembly Pattern performance is bad when adding new pattern occurrences

=====Part=====

PR 1567518: Fixed a problem where a crash occurs while attempting to create a vent feature
PR 5689314: Fixed a problem where Solid Edge crashed while opening a part file.
PR 1548804: Fixed a problem where profile line colors inherits the background color.
PR 1564335: Fixed a problem where the menu window doesn't list the opened parts
PR 1569020: Fixed a problem where a pattern is failing after recompute
PR 1569582: Fixed a problem where a Duplicate Variable error displays when opening part
PR 2077594: Fixed a problem where a protrusion's extent does not stay associative to keypoint.
PR 5589842: Fixed a problem where thread bitmap/texture is changed to be non-directional (threads.jpg)
PR 5691149: Fixed a problem where Wrap Sketch is showing inconsistent behavior.
PR 5691808: Fixed a problem where opening a V16 file changed the variable force unit
PR 5593595: Fixed a problem where toolbar buttons getting stretched out
PR 2078039: Fixed a problem where you cannot create a new file nor open an existing one in "V18 Update 10" on 64Bit
PR 2075826: Fixed a problem where the license borrow utility will not allow more than 14 days regardless of license file
PR 5669432: Fixed a problem where Solid Edge aborts when opening Family of Parts edit table
PR 1554344: Fixed a problem where a Section view is incorrect

=====Draft=====

PR 1572129: Fixed a problem where blocks that are members of a group do not export to AutoCAD
PR 1564332: Fixed a problem where Clearing Dimension Tracker causes an abort
PR 1567469: Fixed a problem where tapered threads are not being generated when cone is chamfered.
PR 2076152: Fixed a problem where a custom property date/time in property text is incorrect.
PR 5684216: Fixed a problem where Fonts are not exported the correct size from V19
PR 1572773: Fixed a problem where you cannot open a V14 draft file
PR 1573138: Fixed a problem where edge painted lines for bends reverting to default style.
PR 5687419: Fixed a problem where weld symbol and hole data was lost when copying and pasting drawing views.
PR 1576052: Fixed a problem where Solid Edge crashed when updating section views
PR 1524420: Fixed a problem where incorrect thread depth graphics are created
PR 1574614: Fixed a problem where copy and paste results in tilted dimensions
PR 1476889: Fixed a problem where some parts were out of place in DQ views.
PR 5707430: Fixed a problem where moving a leader on a callout followed by Undo causes a crash.
PR 1574583: Fixed a problem where groups are loosing format after copy/paste
PR 5358243: Fixed a problem where mapping acad colors to Solid Edge widths does not work with import all colors as black
PR 5606475: Fixed a problem where elements are missing when a DWG file is imported

=====API=====

PR 5678787: Fixed a problem with API GetRedefineSectionDocument
PR 1573562: Custom window captions are now reset when performing a save as
PR 5652139: Added new API AddAutoConstraints

=====Insight=====

PR 1557711: Fixed a problem where Insight Connect crashed when text function is used.
PR 1568258: Fixed a problem where invoking Property Manager from an opened assembly takes approx. 25 minutes
PR 1569139: Fixed a problem where .cfg will be deleted after "Save As" of assembly
PR 1571757: Fixed a problem where the current cfg-file is not downloaded with the asm-file and overwritten by old version
PR 1574127: Fixed a problem where a Part file will be deleted from cache when drawing is opened
PR 5625044: Fixed a problem where as users work the counter for ASP.Net Applications/Requests Executing gets stuck
PR 5670057: Fixed a problem where 50 or so files are deleted from server and local cache
PR 1551714: Fixed a problem where performance of file open is very slow
PR 5660196: Fixed a problem where performance is slow when searching a large number of doclibs.
PR 5626934: Fixed a problem where View & Markup aborts accessing properties
PR 1573712: Fixed a problem where some Sub Assemblies are always checked out during Check in


---
End
---