Solid Edge ST7 SDK
Solid Edge V20 SP1 - Readme

--------------
Legal Notices
--------------
© 2007,
UGS Corp.

All Rights Reserved
Software, file formats, and audiovisual displays may be used pursuant to the
applicable Software License Agreement and contain confidential and proprietary
information of UGS Corp.; which is protected by
copyright and trade secret law.  Such materials may not be reproduced or
transferred to other documents or used or disclosed to others for manufacturing
or for any other purpose except as specifically authorized within the terms of
the Software License Agreement, or as specifically authorized in writing by
UGS Corp.

UGS Corp.
5800 Granite Parkway
Suite 600
Plano, TX. 75024

--------------------
End of Legal Notices
--------------------

--------------
Release Notes:
--------------

Product:        Solid Edge
Version:        20.00.01.08
Date:           11-Oct-2007

This release of Solid Edge has been certified to run on the following:
    • Windows XP Professional® operating system (32 bit or 64 bit)
    • Windows Vista Business® or Vista Enterprise® operating system (32 bit or 64 bit)
    • Internet Explorer 7.0 (IE 6.0 minimum)

This Update can be instaled installed on top of Version: 20.00.00.96.

Note: Updates are all inclusive and can be installed on top of the base release
      or any released UPdate.

--------------------
End of Release Notes
--------------------

-------------------
Installation Notes:
-------------------

After downloading the Update to your machine, dbl click the downloaded file
and the Update will install.

-------------------
End of Installation
-------------------

----------------------------------------------------------
This Update addresses the following Customer Reported PRs:
----------------------------------------------------------

=====Assembly=====

PR 5790158: Fixed a problem with assembly feature performance.
PR 1601204: Fixed a problem with file close.
PR 2085688: Fixed a problem where Pathfinder takes a long time to rebuild during Close & Return.
PR 5790265: Fixed a problem where Solid Edge hangs after viewing properties of a file in the Parts Library tab
PR 2085586: Fixed a problem where a preview is not generated in FOA SaveMemberAs operation.
PR 5779779: Fixed a problem that caused a crash in the Motion environment.
PR 5798459: Fixed a problem that caused a crash in assemblies that have section views or simplified assemblies.
PR 2085626: Fixed a problem that caused Solid Edge to crash.
PR 2084310: Fixed a problem where using linkmgmt.txt file causes delays in open ASM file.
PR 5569116: Fixed a problem where Save as Movie gives different results than from Solid Edge motor simulation.
PR 2085656: Fixed a problem that caused a crash based on submitted crashlogs
PR 5792725: Fixed a crash in the Assembly Pathfinder code.
PR 5791891: Fixed a problem where the document formula is losing its information after creating drawing
PR 5784302: Fixed a problem where parts uploaded, but assembly links are missing
PR 2084868: Fixed a problem with cursor trails and zingers
PR 5778020: Fixed a problem where xpk import needs to import multiple bodies of same file name into the same part
PR 5786782: Fixed a problem where Catia V5 bulk VB translator options were incorrect
PR 1614185: Fixed a problem where a CATIA V5 assembly does not import correctly
PR 2088783: Fixed a problem where Solid Edge crashed after fastener application
PR 5782261: Fixed a problem where parts were being inactivated after doing a show only on an zone definition

=====Part=====

PR 2086250: Fixed a problem where a shortcut menu takes too long to come up in large part files
PR 5783402: Fixed a problem where bend lines do not show up when part is modeled completely
PR 1599742: Fixed a problem where bend disappears after adding a new Tab
PR 1582245: Fixed a problem where flat pattern is not correct
PR 1586092: Fixed a problem where sweep merges faces when using more then one cross section.
PR 5802014: Fixed a problem with flat pattern
PR 2086252: Fixed a problem were hole feature's response time is too slow on large parts
PR 1595081: Fixed a problem where bend radius cannot be changed after a convert to sheet metal
PR 1597527: Fixed a problem where bend relief returns in the flatten model when using a move face
PR 5811217: Fixed a problem where resizing ref planes in child gives wrong member geometry
PR 2088098: Fixed a problem where executing "GO TO" causes Solid Edge to crash
PR 5798598: Fixed a problem where the Lightworks Framework Application Failed while launching Material Table
PR 1600030: Fixed a problem where Save As Flat command produces an empty DXF file
PR 5825162: Fixed a problem where Flange sizes do not match value entered by user.

=====Draft=====

PR 5790010: Fixed a problem where hidden edges toggles are not working for pictorial or ortho views in wizard.
PR 5727318: Fixed a problem that caused a crash when selecting callouts
PR 5773094: Fixed a problem where a symbol is clipped by a Drawing View
PR 5801445: Fixed a problem where annotations and geometry do not translate to Solid Edge
PR 5812763: Fixed a problem where Solid Edge aborts when invoking Property Manager
PR 2087835: Fixed a problem where AutoCAD file with Japanese characters do not open in Wizard
PR 5815198: Fixed a problem where a Drawing file can no longer be opened in V20
PR 5815982:  Fixed a problem where SE crashed when try to move views after unselecting excel table.
PR 1614861: Fixed a problem with Callout is not correct on countersink holes.

=====API=====

PR 5806718: Added an API from CADPartner to aid the Tc data prep tools with STD parts
PR 5803835: Added automation method to get "Created" & "Last Saved" versions
PR 1614401: Fixed a problem where Macros don't run under Vista
PR 2086297: Fixed a problem where the value of custom property is not displayed on assembly path finder.

=====Insight=====

PR 5795995: Fixed a problem where files should not be checked out
PR 5796968: Fixed a problem where FTP server links on the Tech Support Help menu pop up a Server Login dialog
PR 5800304: Fixed a problem where Web Parts can not find 'Edge.exe'
PR 5800204: Fixed a problem where Solid Edge aborts when opening subasm via web parts page
PR 5806293: Fixed a problem where RevMan deletes part file if files are renamed the same.
PR 2078513: Fixed a problem where Solid Edge can not create a new folder in Japanese OS
PR 1607695: Fixed a problem where Redefine links do not work
PR 2086755: Fixed a problem where Japanese file names are garbled in View & Markup
PR 2060477: Fixed a problem where Customers cannot save SE file using Japanese name as PCF.

---
End
---