PR |
Description |
1792114 |
NX Sheet Metal:Export Trump GEO file for Lofted Flanges is not correct |
1843481 |
Linked Body does not update until feature playback |
1877492 |
CMM Pro_E: no centerlines on migrated pro_e drawings |
1892158 |
Failed to load assembly drawing |
1896008 |
Stock Offset Port Problems |
1897779 |
Listing Window to File doesn't work properly |
1903841 |
Points not added correctly when editing spline path |
1904164 |
Create spline path with end point on second spline - not created tangent |
1904291 |
Create Spline Path, pick end point on other spline, tangency not created |
1909670 |
Arrow direction while creating a ribbon sheet |
1917008 |
NXOpen IsSheetmetalBody returns TRUE for unparameterized body |
1920719 |
Trimmed Sheet feature always fails when feature is replayed |
1923055 |
Timestamp on Linked Point is not correct |
1926703 |
Detail view: Incorrectly underlined label when using "text above stub" |
1927107 |
Inconsistency in color rendering of DWG exported section edges |
1928269 |
Converting Mating Conditions gives "An invalid tag was passed to the tag module" |
1933666 |
Letter j and l not accepted in SurfaceFinishSymbol under Linux (Suse11sp1) |
1935501 |
PMI Custom Symbols are not exported correctly to JT file |
1936844 |
UF_MODL_create_symb_thread fails with Datum CSYS plane as start face |
1937846 |
Area Fill is incorrectly converted to 2D layout for DWG_DXF format |
1939239 |
No replacement for NXOpen.PDM.SoaQuery.AddFieldDescription() |
1941222 |
Pattern is not correct, only available after node opening |
1942010 |
Specify location icon in 'note' flickers |
1945936 |
Inserting new points into existing spline can cause spline to twist_knot |
1947701 |
Line Font with User Defined Symbol doesn't use the original symbol factor |
1949246 |
Error message during deriving of a Model View to a drawing |
1953167 |
PS26.00.200: 4222-027-26050_Draft(92) fails in NX 8.5.2.3 MP1 on Playback |
1953245 |
Make unique leaves new drawing file (specification) checked out |
1953485 |
Copy_paste a sketch does not create new named expressions |
1953570 |
Normal Cutout Feature replay fails |
1953589 |
Make Unique will leave new drawing dataset checked out |
1953634 |
Flat Pattern missing features depending if features overlap |
1954052 |
Centerline Type From Curves - wrong position when generating |
1954163 |
NX crashes when attempting to Edit a Spring Connection in CAE Motion app |
1955157 |
Dimensions disappears when view break insert |
1956872 |
Creating Non-Orthogonal and Left Hand Coordinate Systems should not be Possible |
1958146 |
Error Importing Part Stored in Teamcenter into another Part |
1958529 |
Moldwizard cannot change parameters of moldbase components in next session |
1959786 |
Unable to change the number of dimension decimal places of sketch |
1961116 |
UFSession.Draw.SetViewLabelParms issues if View Scale is before or after Label |
1962132 |
Steelstock with Resuselib inserts a component instead of a stock |
1962772 |
NX unable to create radius dimension on some rounded slots |
1962916 |
Bead : offset and curve direction of the bead curve change |
1962959 |
Perpendicular dimensions are retained in NX when migrated from Ideas - CMM 8.5.2 |
1963273 |
Editing Hole Features shows wrong values |
1963408 |
Spline Path not correctly aligned to port, missing Parallel constraint |
1963524 |
Bead: Created Offset Curve is to wavy |
1963578 |
Cannot obtain parents of DraftingCuve objects anymore in NX 8.5 Exact views |
1963812 |
Crosshatch is retained after part modification |
1964180 |
Wrong position of dimension extension lines by the dimension |
1964376 |
Template with multiple item type isn't selecting first item type as default type |
1964498 |
Weld point command with option overlap calculates the reference sheet not always |
1964593 |
Java API accepts Datum letters not valid for DMIS in dialogs |
1964693 |
Copying Electrode by modeling causes wrong Z position in all instances |
1964736 |
Callout Dimensions for Threads are displayed wrong |
1964814 |
Feature Playback fails in NX 9.0.1 (part from NX 8.5.2 failure free) |
1965240 |
PMI linear dimension corrupt when changing model view |
1965420 |
Adding points to spline path moves components together unexpectedly |
1965793 |
Position column should show if component used to define axis is closed |
1965795 |
Position column should show if assembly having pattern is loaded structure |
1966365 |
Patterns containing User Defined Symbols give error |
1966427 |
Auto Balloon does not appear to work on a Revolved Section View in NX 9 |
1966631 |
Problem with threads in a Half Section View, missing thread end line |
1966820 |
Weld Point Guide curve offset not trimmed to all boundaries |
1967690 |
Electrical Routing: NoTangencyAtTakeout |
1967696 |
Electrical Routing: Missing Tangency created After Wrong Point Deletion |
1967704 |
Electrical Routing: Wrong (different) Spline Behaviour During Move Point |
1967705 |
Electrical Routing: Wrong Number Of RCPs At Takeout |
1968208 |
Shell expansion delivers not expected result |
1968213 |
Changing rectangular pattern leaves symbolic threads |
1968655 |
Formulas disappear in Spreadsheet |
1968939 |
GRIP command VDEDIT now fails to Modify Curve Segments with FONT 0 |
1969595 |
Load Option -Load interpart data- does not work as expected in NX 8 |
1969617 |
Surface Finish Symbol Dialog has a limitation under Linux |
1969763 |
NX Sheetmetal - Small Gusset dimensions |
1969785 |
Missing geometry in drafting view using "Render Sets" |
1970000 |
CAD: NX will crash when updating Fibersim ply book |
1970183 |
Import of STL Data Fails |
1970629 |
Part Family update failed in NX 9 |
1970698 |
Unpredictable wrong behavior when updating a view with some sections |
1970875 |
Wrong shaded view in PDF when using view break |
1971302 |
Numbering rule Save CAE datasets created with traditional CAE datamodel in NX 8.5 |
1972094 |
Some arcs from Flat Pattern are visible in modeling |
1972378 |
UDF regression between 75 and 85 for expression transfer |
1972920 |
NXMGR: Catching errors from TCIN SOA |
1973050 |
Problem with line below symbol i drafting Detail view and Label on Parent |
1973090 |
Issues plotting streamlines |
1973375 |
Memory access violation when modifying Array |
1973808 |
Mounting Method has no influence |
1973890 |
PMI Balloons smashing up if the balloon contain a angle different then zero |
1973916 |
Inconsistent behavior of Raster Image with dynamic positioning |
1974026 |
Unchanged assembly is marked as modified when working with part family members |
1974180 |
NX 8.5 is too slow updating Extracted Region feature |
1974283 |
UDF Regression NX 8.0.3.4 MP1->MP8: Linked UDEs are not referenced when instanced |
1974465 |
Deformable bodies created in NX 4 |
1974640 |
NX 9 crash using compress post-view option with nvidia graphic card |
1974997 |
PS26.01.214: Trim Body not possible |
1975036 |
UDF record in udf_database.txt and library_dir.txt is limited to 256 characters |
1975205 |
Pattern Component does not create all instances |
1975353 |
Insert detail view results in error "updating an object of type Exact Detailed" |
1975852 |
Mac OS: Dialog Error after run NXOpen .jar or .class file |
1976004 |
Performance from Wave Geometry Linker by changing the part are bad |
1976312 |
ASM fails to open: too many iterations |
1976653 |
NXBlech "Resize Bend Angle" arbeitet fehlerhaft bei bestimmten Biegewinkeln |
1976655 |
Resize Bend Angle failed by different angle |
1976658 |
Layer and Color filters do not work in Exact Views |
1976994 |
Detail view label are displayed with an extra line when using Above Stub |
1977036 |
Set work part fails on JT files with LayerFilter information |
1977044 |
Reverse Direction not available for linked interface curves in NX 9 |
1977293 |
Tabular note completely loses its format when editing_moving origin |
1977308 |
Electrode Design Blank doesn't find matching size with multiple MATERIAL option |
1977769 |
Daimler Multi CAD: Replace transient Components |
1977900 |
Expressions loose their references when instantiating an UDF |
1978191 |
Null tag error in assembly drawing |
1978287 |
The UFSession.Draw.SetViewLabelParms() fails when setting True Boundary Label |
1978293 |
View label changes after the use of theUFSession.Draw.SetViewLabelParms() |
1978346 |
Missing UF_terminate() in Debug mode causes Sig11 on later part operations |
1978489 |
Wrong dimension values on Centerline based dimensions |
1978561 |
Changed character font size in Tabular Note after "Specify Location" |
1978621 |
Section view capping display missing from lightweight JT files |
1978630 |
PS26.01.214: Trim Body failed |
1978644 |
Invalid bend angle in .geo file |
1978706 |
NX: the underscored text is in the detail label |
1978966 |
Adopting NX 9 Drafting Dimension now requires a "nx_ship_drafting" license |
1979103 |
REGR:Clone issue with non geometric and reference only components |
1979168 |
It can take a long time to perform Open Component from the Assembly Navigator |
1979318 |
User Defined Symbol on Pattern is not displayed anymore |
1979398 |
Move Part Module in other Part Module via Nest Module NX hung |
1979399 |
Capture Arrangement Error |
1979501 |
Formatting and dimensions will be lost by update the drawing - break view |
1979591 |
New Drawing - Internal error: memory access violation |
1979691 |
Cant open file - get error "splines with bad data detected" |
1979751 |
OPEL: NX 9 - Variant Configuration Is Missing From The Assembly Menu |
1979756 |
OPEL: NX 9 - Suppressed Sub Assemblies |
1979795 |
Customized "ugii_env.dat" file is not loaded |
1979811 |
NX Relations Browser : Relations are no longer shown |
1979825 |
Critical performance problems when adding or removing "Boundary Faces" |
1979904 |
Copy paste features NX 8.5 and expressions |
1979957 |
Part Module: Different selection order in feature paste |
1979958 |
Part Module: Different selection order in feature paste |
1979965 |
Part Module: Different selection order in feature paste |
1980026 |
MCD : Export to Sizer used a wrong signed DLL internally |
1980079 |
Application crashes when shading in high quality image |
1980291 |
Saving mirrored Electrode in TC fails with 'Could not find file for component' |
1980352 |
Unable to open some NX parts in TC managed mode, give "Internal Error Memory..." |
1980377 |
Adopting NX 9 PMI Dimension now requires a "nx_ship_drafting" license |
1980423 |
Shell Expansion delivers unexpected result |
1980424 |
Easy Fill NX - Run Flow Analysis does not work with license file |
1980425 |
PS26.01.216: performance problem with Trimming Body |
1980469 |
Move Table Note gives Error after Adopting Object in KF |
1980498 |
Incorrect Callouts Symbol after updating Parts List settings using UF |
1980786 |
Loading assembly in NX with modular options |
1980798 |
Problems changing size of UDF (threaded hole) in pattern |
1980926 |
Rapid Dimension is not so rapid in context of assembly |
1980959 |
Broken Links after Component Replace |
1981011 |
Not possible to edit plates in mold base library after closing and reopen project |
1981087 |
Multiple SWEEPS (Stocks) on Routing Path |
1981139 |
Can't import part with tabular note (+symbol inside) twice |
1981263 |
Datum Feature Symbol non si aggiorna |
1981368 |
Silhouette curves do not display for lightweight spherical component |
1981377 |
Layer visible in view not working properly for sketch curves (in assy context) |
1981388 |
Are not able to select a baseline on name for Cylindrical Dimension in NX 9 |
1981463 |
Selecting geometry in Examine Geometry Crashes NX on Linux |
1981503 |
PSv26.1.215 Edit Feature Playback failed NX 9.0.1.3 D1, for A2386460500 |
1981505 |
Edit Feature Playback failed in higher version |
1981546 |
Wrong spelling _ letters missing in the result of some check mate checks |
1981559 |
Edit Feature Playback failed in higher version |
1981563 |
Edit Feature Playback failed in higher version NX 9.0.1.3 D1, for A2388852300_2 |
1981622 |
PS26.01.220- Playback failed in higher version NX 9.0.1.3 D1 for A2386373100 |
1981628 |
Edit Feature Playback failed in higher version NX 9.0.1.3 D1 for A2386364700 |
1981668 |
AskOpenPartFilename using C# crashes |
1981915 |
View Break with the View Style set to Fully Shaded results in incorrect PDF_Plot |
1981934 |
KF top instance is not deleted when child rule is deleted |
1981961 |
Internal Error when de-select face in Bridge Curve dialog |
1982023 |
Balloons removed deleting Parts List only if it's set as Customer Defaults |
1982064 |
Retained dimension when reference Object deleted |
1982099 |
Plate Preparation command creates unexpected result |
1982117 |
Make Unique inherits assembly attributes to its underlying component |
1982262 |
Surface Finish symbol does not move when view break applied to view |
1982282 |
Performance issue to save jt files in NX |
1982478 |
SB Resize Bend Angle does not work for specific values |
1982586 |
PS26.01.218 Fix: Subtract - Through face does not intersect path of the tool |
1982603 |
Welding: Connect Face Finder does not work in all cases |
1982671 |
RESIZE BEND ANGLE: Changing to some value ranges is not possible |
1982691 |
Angular dimensioning of a small angle fails |
1982706 |
NXOpen GetBendParameters returns wrong angle after Unbend _ Rebend |
1982730 |
Feature Playback Failure in NX 9. Same Model tested in NX 8.5.1.3 with Daim |
1982747 |
Export PDF file from shaded drawing is not shown correct |
1983053 |
Wrong result with import of NX 7.5 dpv settings to NX 9 |
1983164 |
Assy level Facet Representation color does not match color of component in assy |
1983195 |
Resize Bend Radius fails |
1983241 |
Add component using assembly constraints slow when lots of deformable parts |
1983271 |
Assembly navigator does not remove the asserted weight and status |
1983308 |
KF: creating multiple new parts with seed part and ug_mirror_body fails |
1983329 |
KF %ui_comp_selection doesn't keep objects reliably using OnInitialize callback |
1983376 |
Problem mit Teilefamilie und Teamcenter |
1983386 |
View break - not able to add an angular dimension |
1983390 |
002-7005793-Workaround doesn't work-View Break will result in Hidden Annotations |
1983456 |
PDF is missing parts of a shaded view |
1983502 |
TCUA : Interpart Link Browser takes around 15 min to open |
1983557 |
Remove Overlapping Entities Checkbox |
1983582 |
DOF of multipoint constraint cannot be permanently set blank |
1983591 |
Vehicle Design_Eyellipse: Memory Access Violation when applying changes |
1983707 |
Shaded View containing View Break will not plot or export to PDF correctly |
1983721 |
Executing DLL twice with UF_SF_ function fails with code 750002 |
1983723 |
dxf export mit Komma |
1983731 |
Editing plate with "cutout" does not work as expected |
1983764 |
Plate feature is very slow on startup and when editing a plate |
1983796 |
Warning message reports parts modified not reported in Assembly Navigator |
1983801 |
Creating plate with boundary object body faces gives error |
1983860 |
NX 8.5.3.3 not changing item type any more with Cadenas Partsolutions |
1983861 |
NX crash when import merge of HRN file into electrical connection navigator |
1983874 |
Can't open parts "The record area asked for does not exist in this object" |
1983879 |
Descriptive file name doesn't update properly in windows list |
1983972 |
Using UF_UGMGR_new_part_from_template() results in a part tag of 0 |
1984006 |
%nx_application icon wrong in drawing when master model JT saved |
1984278 |
NX 9 - Deformable Part Reference Names not change correctly |
1984447 |
Dimensions incorrect |
1984525 |
Moldbase parts can not changed, The selected component is not in current library |
1984583 |
Save As Operation copies CGM named reference to new item revision |
1984620 |
Wrong JT LayerFilter assignments from NX lightweight bodies |
1984629 |
NX 304449: Feature Playback failed in NX 9 for MFA_RB@0000001077_1 |
1984636 |
Unable to open part - Memory Access Violation. No error in NX 6 and NX 7.5 |
1984642 |
PSv27.00.165 Feature Playback failed in NX9 for MFA_RB@0000000958_1.prt |
1984646 |
PSv27.0.152 Feature Playback failed in NX9 for MFA_RB@0000002349_1.prt |
1984695 |
All features updated OK in NX8 & NX 8.5 & NX 9 D3 |
1984697 |
Error in NX 9 D3 |
1984707 |
Same errors in NX 8.5 & NX 9 D3 |
1984719 |
PS27.01.041Feature Update does not work in NX 9 fine in NX 8 |
1984726 |
PS27.01.041 fix. Feature Playback failed in NX 9 |
1984727 |
PS27.01.041 WA.Feature Update fin in NX 8 stops in NX 9 |
1984732 |
Feature Playback failed in NX9 for MFA_RB@0000000825_1.prt |
1984748 |
Same problem as described in Master PR1970875 (Shaded View Break) |
1984756 |
PS27.01.050 WA Feature Playback failed in NX9 for MFA_RB@TUERBEPLFA_1.prt |
1984811 |
NXOpen::Die::DrawBeadBuilder::StartPoint::SetPlane needs ug_die_design license |
1984921 |
JT_ASSOCIATIVE_BODY break associativity after "Update Part File" in NX 8.5 or NX 9 |
1985134 |
Part updates during loading |
1985151 |
Can not add a single load case on geometry |
1985178 |
Problem with Surface Finish symbol in View-Break View |
1985259 |
Internal error during loading part bc.003.751mod000_0500 |
1985395 |
Updating linked geometry causes all sections (from ship application) to disappear |
1985613 |
Associating table position to sheet size using KF gives signal 11 error |
1985663 |
Converting to reference_active curves doesn't throw an "out-of-date" status |
1985685 |
NX 8.5 fails to open an asm, with components with tc references, where NX 7.5 does |
1985702 |
Change in sheet size causes a change to the ordinate dimension text preference |
1985835 |
Problem beim Speichern einer Teilefamilie |
1985921 |
Problem with Surface Finish symbol in View-Break View |
1985924 |
WAVE geometry linker does not list product interfaces in component |
1985952 |
Convert Routing Splines fails |
1985985 |
Unable to import STEP214 file into NX |
1986189 |
Warning while opening - in Motion Simulation |
1986203 |
Problem open assembly in NX from Resource Manager and Structure Manager |
1986218 |
Importing a global ply definition '.layup' file - resultant mapping is poor... |
1986255 |
Error when saving drawings with Russian item_id |
1986315 |
Closing only the assembly part results in grayed out Window->More menu option |
1986426 |
Orientation of a Linked curve ( produced interface link ) |
1986483 |
Too many RCPs after deleting a segment of a path |
1986595 |
Change of layer for lightweight body reverts back upon save |
1986714 |
Suppressed Composite Curve prevents Product Interface conversion |
1986749 |
ReUse Library will no longer show up mulit-cad items |
1986918 |
Edit settings for Hole Callout using Inherit "Customer defaults" doesn't work |
1986950 |
Attaching a component as a Problem Item using Attach work part gives error |
1987159 |
NX 9 unable to 'save as' a part with LW automatic generation set to None |
1987307 |
Load Interpart Data not work in NX 8.5 as in NX 7.5 |
1987328 |
Can't select a named centerline when creating a cylindrical dimension |
1987445 |
Cannot edit bracket after editing profile |
1987735 |
Failed to create quick access named reference file when cyrillic item_id: |
1987781 |
Join Curve creates the wrong type due to Modeling preferences |
1987930 |
Checking failed for this part, please report an IR |
1987974 |
CGM Data for compare drawing is incomplete |
1988062 |
NX session crashed while postprocessing |
1988128 |
NX materials management unable to retain the units applied |
1988149 |
New face ID when using 'SB Resize Bend Radius' |
1988242 |
Error - The same title cannot be used on two different attributes |
1988301 |
Missing Geometry in View using "Render Sets" ("Extracted Edges - enabled") |
1988559 |
NX 9 hangs when trying to open an NX 7.5 sheet metal part file |
1988699 |
Dimensions in drafting didn't update after model modification |
1988820 |
ugtopv does not translate all coordinate systems into JT |
1989093 |
Replace component with maintain option fails on multi-cad item revision |
1989094 |
Mold Wizard Initialize Project fails on Linux with IE_MAV and terminates session |
1989491 |
Pattern Feature (Circular) does not work as expected in NX 8.5.3.3MP4 |
1989519 |
Attribute "DESCRIPTION" is not created |
1989577 |
Inconsistent units after un-setting attribute from or not from template |
1989607 |
Creation of UGALTREP changes Item Name in TC |
1989647 |
Part Attributes are no longer exported to JT file from NX |
1989684 |
KF edit sketch crash changing angular dimension |
1989718 |
Profile cutout parameters fail to update to different profile sizes in Ship appl |
1989775 |
Bracket fails when target stiffener edited |
1989914 |
The record area asked for does not exist in this object, cannot open part |
1990053 |
Crosshatching disappears in Revolved Section View after placing Detailed View |
1990161 |
Crosshatch disappearing in either parent or detail view and internal errors |
1990213 |
MaterialMissingAssignements has the wrong value |
1990219 |
Unable to open part => invalid or unsuitable OM object |
1990327 |
Long selection Time using Rapid Dimension in Sketch |
1990767 |
Sketch doesn't maintain consistent geometry during edit |
1990811 |
Broken associatively after Import Mechanism - 2 |
1990818 |
UF_DRF_set_line_arrow_preferences set an invalid preference value |
1990825 |
Checking failed for this part, please report an IR |
1991366 |
Checkmate check G-SO-EM gives incomprehensible error message |
1991655 |
File_Open : stp - HK004__FIX_M12_140624.stp - Error number: 1 |
1992103 |
FGA KBE Linked Csys doesn't update position after General Relink |
1992104 |
Modifying Sketch Reference causes sketch problem |
1992421 |
Electrical Routing:LostConstraintDuringRCP-Movement |
1992551 |
NX crashes when creating custom made cutout with collar plate in NX |
1993240 |
Saving problem assembly |
2146397 |
Drawing view become out of date after component is opened |
2164397 |
HNS-TWS2: Replace 2 occurrence of a component raises an Internal Error |
2191276 |
CPJ:When it is set as "Referenced Edges Only", a reference element is displayed |
2197431 |
CPJ:If a Spline Path is edited, "Lock Length" will turn off |
2201455 |
Cannot create branch Path with existing spline path |
2201460 |
REGRESSION -Cannot create additional RCP to existing Spline Path point on curve |
2201834 |
Underlined Parent label note appears when edit a label of style view |
2209633 |
View update causes display of erased curves |
2212197 |
When the [Assign Corner] is executed, debug messages is displayed |
2212732 |
Display out of date after update drawing |
2214679 |
The result of export to DXF is wrong |
2215010 |
'Sequence method:1,2,3' does not work when a prefix_suffix is entered |
2215098 |
Solid of a cross-section view is also exported to JT |
2215419 |
When I exported a solid body into JT file, JT has two solid bodies |
2216543 |
View Dependent Edit hidden lines are missing after view update |
2218405 |
C1 Error Recovery with Undo mark missing |
2221699 |
An extra underline is added, when edit the Character height factor |
2222556 |
CPJ: Datum feature symbol created on dimension line bend |
2222601 |
ISZ_VUP:Loading of altrep from which revision differs fails |
2223526 |
Cannot change the selected path point to another |
2223719 |
Customer would like to edit Jog by using shift key when editing the Ordinate dim |
2223802 |
By updating model from Exp. Editor, EDU does not pop-up, and unable to operate |
2224040 |
About the label of [Section View] which uses [View Break] |
2225972 |
A view dependent edit is not remembered for a specific solid silhouette curve |
2226872 |
About assignment of the expression by changing the expression |
2227761 |
Error occurs when translating NX data which contain [Sheet Emboss] to JT |
2228483 |
Missing Geometry line in NX8 drafting [Silhouettes Curves] |
2228650 |
The extra 6 edge lines are displayed on NX 7.5.2 upwards by View Update |
2228935 |
Contour disappears when use the "compress" of post view |
2229032 |
CPJ-VUP: UAF (NX 9.0.1.1) Feature update error occurs in Flat Solid(105) |
2229034 |
CPJ-VUP: UAF (NX 9.0.1.1) Feature update SB_FLAT_SOLID |
2229410 |
Not available to create branch path with tangency |
2229494 |
When update drawing, hidden silhouette curve is displayed in the view |
2229811 |
[NX 9.0] About label on parent of the drafting detai view |
2230739 |
Two underlines of a view label are displayed if text factor Greater than 1.0 |
2230859 |
Can't obtain parents of drafting curve objects in NX 8.5 Exact views |
2231522 |
The arrows created in expand mode is displayed distorted in NX 9 |
2231855 |
Even though we set detail view label off the label is consumed by detail view |
2232015 |
Journal replay fails to set drafting preference 'Lightweight Drawing Views' |
2232409 |
The translator is not able to connect to Tc in 4-tier but it works in 2-tier |
2232421 |
NX 310864: Error message is not displayed in spite of inaccurate model |
2232542 |
Make unique leaves new drawing file (specification) checked out |
2232962 |
In [Edit Entire Objects] command, the line erased is displayed |
2232963 |
If the width of the line is changed, type of line will also be changed |
2233321 |
There are NX 7.5 part files failed to be open on NX 8.5 |
2233473 |
CPJ: A perpendicular dimension moves by feature updating |
2233575 |
When I add a material, material names of additional materials are changed |
2233788 |
After loading the Interpart data, files are not fully loaded |
2233892 |
[Problem]The unnecessary alert is displayed on Unite feature |
2233992 |
Invisible cell border is displayed by editing origin |
2234188 |
Break-out Section with Render sets: Part of Visible lines become fixed width |
2234367 |
We cannot change the jog setting from the on-screen list |
2234420 |
Hide original while extracting composite curve does not hide the original curve |
2234860 |
A line is displayed under a parent label of a detail view |
2234902 |
PS26.01.212: UF_MODL_ask_curve_points() returns wrong error code 820120 |
2235004 |
Lock status is changed to Unlock once Form is displayed by NXOpen. UI.LockAccess |
2235046 |
Warning message displayed below the already existing dialog |
2235175 |
CPJ : "Out of Date" status is not display in Part Navigator |
2235437 |
Extension of NX 8's dimension will be moved on NX 9.0 |
2235899 |
Reg_NX 7.5.4 - ISZ_VUP: The correct end gaps are lost by view update |
2235976 |
Splice and Other component type get changed after export and import |
2236057 |
NX 900_SZK_UAD Crosshatch failed when "update" or "version up" drawing in NX 9 |
2236058 |
NX 900_SZK_UAD Crosshatch is different in NX 7.5 and NX 9 |
2236084 |
The dwg nav not updated after the component is loaded |
2236135 |
Copy&Paste the Feature problem |
2236140 |
Information message is not displayed in Japanese |
2236193 |
View Rotate performance is bad in NX 9 than NX 7.5 |
2236242 |
The model cannot be closed with an error in drafting application |
2236265 |
NX 900_SZK_OD Angular dimension is change while open drawing in NX 9 |
2236269 |
NX 900_SZK_OD Extension line of the Dimension can't display correctly in NX 9 |
2236377 |
Unable to edit decimal place of multiple stocks size |
2236441 |
The row of hole name does not remove when de-select all holes |
2236492 |
[Problem]About correction of direction of datum CSYS |
2236737 |
ISZ_VUP:Date Released of Family Member is updated by "Update Parts" |
2236811 |
Exterior body color becomes the same color as internal cutout in "Flat Pattern" |
2236985 |
iTest: Solid Punch feature doesn't reflected when partmodule is active |
2237092 |
Please let me know about "Activate sketch" |
2237112 |
NX 9.0.0_SZK_UAD Ref OBJ of Diameter changes in NX 9 after view update (2) |
2237160 |
Extension line of dimensions are extended in NX 8.5 after updating view |
2237184 |
The lines edited by view dependent edit in NX 6 disappear\appear in NX 8.5.3 |
2237200 |
GDT symbol created in NX 6 moves after updating view in NX 8.5 |
2237213 |
The decimals is not displayed in Dimension set by [Display As PMI] command |
2237245 |
UAF: NX 9.0.1 Edge blend fails during feature playback |
2237248 |
In Lightweight Section View, "Dynamic Input Box" is always reset |
2237249 |
PS26.1..213::UAF:NX 9.0.1 Failed to construct draft surfaces |
2237251 |
UAF: NX 9.0.1 The regions to be kept are changed in Trimmed Sheet feature |
2237266 |
Internal error occurs when performing partial loading for component |
2237270 |
In WAVE Geometry Linker, Character displayed with vector is corrupted |
2237275 |
Error occurred during display of part, Display operation attempted on non-displa |
2237371 |
[Show Info View] is not visible in the [Requirements Validation] in Japanese env |
2237422 |
Default container does not become effective |
2237489 |
[Thread]In NX 9, Different method type is set |
2237615 |
[CAD] It is not possible to save the data |
2237714 |
Layer filters do not works in "view dependent edit" |
2237741 |
About "Embedded curves : G-CU-EM" [Check Mate] |
2237846 |
Cannot obtain parents of DraftingCuve(extracted ) objects in NX 8.5. Exact views |
2237914 |
<URG>Crosshatch pattern changes when I open the drawing in NX 9 |
2237977 |
Size reverts back if edit the "Lineup" feature |
2237995 |
The facet body which is copied by layer is not displayed in the PNT has a added |
2238094 |
Object ID is changed when we change the value of user expression |
2238224 |
[CAD]"Reflection Data" is not updated when parent feature is changed |
2238250 |
CPJ-VUP: UAF Failure(NX 9.0.2.2) update causing missing edges for Break Corner |
2238251 |
CPJ-VUP: UAF Failure(NX 9.0.2.2) Update error occurs in Break Corner(2) |
2238291 |
CPJ-VUP: UAF Failure(NX 9.0.2.2) Update error occurs in Secondary Contour Flange |
2238292 |
CPJ-VUP: UAF Failure(NX 9.0.2.2) Update error occurs in Break Corner(42) |
2238298 |
CPJ-VUP: UAF Failure(NX 9.0.2.2) Update error occurs in Mirror Feature(38)(39) |
2238300 |
CPJ-VUP: UAF Failure(NX 9.0.2.2) Update is changed geometry by Break Corner(123) |
2238302 |
CPJ-VUP: UAF Failure(NX 9.0.2.2) Update error occurs in Normal Cutout(11) |
2238333 |
CPJ-VUP: UAF Failure(NX 9.0.2.2) Update error occurs in Threaded Hole(5) |
2238337 |
CPJ-VUP: UAD Failure(NX 9.0.2.2) Linear Dim. is erased by Update Views. |
2238339 |
CPJ-VUP: UAD Failure(NX 9.0.2.2) Edges of Thread are disappeared by Update Views |
2238343 |
CPJ-VUP: UAF Failure(NX 9.0.2.2) Update error occurs in Flat Solid(114) |
2238346 |
CPJ-VUP: UAD Failure(NX 9.0.2.2) 2DCenterline moves to wrong pos. by Update Views |
2238350 |
CPJ-VUP: UAD Failure(NX 9.0.2.2) 2DCenterline moves to wrong pos. by Update Views |
2238355 |
CPJ-VUP: UAD Failure(NX 9.0.2.2) Thread hole silhouette are disappeared |
2238360 |
CPJ-VUP: UAF Failure(NX 9.0.2.2) Update error occurs in Break Corner(105) |
2238364 |
Detail View: Incorrectly underlined label when using 'text above stub' |
2238366 |
CPJ-VUP: UAD Failure(NX 9.0.2.2) 2DCenterline was moved & rotated by Update View |
2238371 |
CPJ-VUP: UAF Failure(NX 9.0.2.2) Update error occurs in Secondary Contour Flange |
2238379 |
CPJ-VUP: UAF Failure(NX 9.0.2.2) Update error occurs in Flange(7) |
2238387 |
CPJ-VUP: UAD Failure(NX 9.0.2.2) Unnecessary edges appeared by Update Views |
2238388 |
CPJ-VUP: UAD Failure(NX 9.0.2.2) Crosshatch is displayed partially by Update View |
2238400 |
CPJ-VUP: UAF Failure(NX 9.0.2.2) Update error occurs in Break Corner(52) |
2238402 |
CPJ-VUP: UAD Failure(NX 9.0.2.2) Position of Linear Dim. was moved by Update View |
2238462 |
CPJ-VUP: UAD Failure(NX 9.0.2.2) Crosshatch became partially by Update Views |
2238464 |
CPJ-VUP: UAD Failure(NX 9.0.2.2) Solid silhouette was erased by Update Views |
2238465 |
CPJ-VUP: UAD Failure(NX 9.0.2.2) Solid silhouettes were displayed by VW_UPDATE |
2238466 |
CPJ-VUP: UAD Failure(NX 9.0.2.2) Section line changed after VW_UPDATE |
2238468 |
CPJ-VUP: UAD Failure(NX 9.0.2.2) Position of a note was moved by VW_UPDATE |
2238469 |
CPJ-VUP: UAD Failure(NX 9.0.2.2) Extension line's position was moved by VW_UPDATE |
2238608 |
CPJ :Hidden Solid silhouette curves are displayed by Update |
2238633 |
CPJ : Result file of ExecuteCompareReport.exe is not created correctly |
2238657 |
CPJ-VUP: UAD Failure(NX 9.0.2.2) Loading of part causes movement of View Label |
2238659 |
CPJ-VUP: UAD Failure(NX 9.0.2.2) Crosshatch is erased by Update Views |
2238661 |
CPJ-VUP: UAD Failure(NX 9.0.2.2) Crosshatch jumped out a boundary by Update Views |
2238669 |
CPJ-VUP: UAD Failure(NX 9.0.2.2) Update views behaves different in NX 8 and NX 9 |
2238670 |
CPJ-VUP: UAD Failure(NX 9.0.2.2) 3 Crosshatch issues occurred by VW_UPDATE |
2238672 |
CPJ-VUP: UAD Failure(NX 9.0.2.2) Position of Crosshatch moves by Update Views |
2238673 |
CPJ-VUP: UAD Failure(NX 9.0.2.2) Crosshatch is removed by Update Views |
2238674 |
CPJ-VUP: UAD Failure(NX 9.0.2.2) Crosshatch became partially by Update Views |
2238675 |
CPJ-VUP: UAD Failure(NX 9.0.2.2) Crosshatch became Retained by VW_UPDATE |
2238677 |
CPJ-VUP: UAD Failure(NX 9.0.2.2)Crosshatch on TOP moves to wrong pos by WM_UPDATE |
2238678 |
CPJ-VUP: UAD Failure(NX 9.0.2.2) Linear Dimension disappears by WM_UPDATE |
2238694 |
V26.01.218 - CPJ-VUP: UAF Failure(NX 9.0.2.2) Edge Blend(812) |
2238711 |
PS26.1.221:CPJ-VUP: UAF Failure(NX 9.0.2.2) Update error occurs in Draft(69) |
2238787 |
CPJ-VUP: UAF Failure(NX 9.0.2.2) Update error occurs in Flat Solid(131) |
2238836 |
CPJ-VUP: UAF Failure(NX 9.0.2.2) Update error occurs in SB Break Corner(124),(128 |
2238846 |
CPJ-VUP:UAF Failure(NX 9.0.2.2) Update error occurs in Divide Face(10) |
2238855 |
CPJ-VUP: UAD Failure(NX 9.0.2.2) Dimension Extension Line appears |
2238871 |
The positions of a component differ between NX and JT2Go_TC vis |
2238919 |
Cannot update a drawing |
2239236 |
CPJ : Out-of-Date flag is displayed if exist the drawing view |
2239368 |
NX 901_SZK_MC_Shape of model changes in NX 9_model25 |
2239394 |
Datum Axis - Vector orientation is not correct |
2239501 |
Unable to create the point with specifying the angle |
2239513 |
Error occurs when save the part file |
2239680 |
NX 901_SZK_MC_Shape of model changes in NX 9_model62 |
2239704 |
The extension line of dimension will be displayed unintentionally |
2239847 |
CMM_Native of NX 9.0.1 can not be executed in error |
2240176 |
Cannot open_tranlsate CATIA V5 Translator using NX9.0.1.3 MP1 |
2240180 |
The color of piloting is wrong |
2240201 |
Define prebends give the wrong result in direct unfolding |
2240216 |
CPJ : Cannot load the JT file to Native NX |
2240419 |
When TabularNoteTemplate which added is moved, Style differs from a set value |
2240450 |
Unable to access the custom line width if the output is changed in print dialog |
2240535 |
NX 901_SZK_OD Note disappears in NX 9.0.1 |
2240608 |
[CAD]Move face feature is updated incorrectly in NX 9 |
2240633 |
NX 9.0.1 - Boring tool gouges in cycle Drill, Bore |
2240774 |
About label on parent of the drafting detail view:Unexpected line is shown |
2240836 |
The additional curves are not trimmed to the solid in flat pattern view |
2240933 |
Error encountered while converting preNX 9 spline to NX 9spline by convert splines |
2240974 |
Checking failed for this part please report an IR |
2241162 |
Unable to hide tabs in blockstyler through hide method |
2241333 |
The positions of a component differ between NX and JT2Go_TC vis |
2241337 |
Null tag error during extrude |
2241339 |
Not able to create the section view |
2241388 |
No Static API Available for textColorFontWidth Block in Block Styler |
2241432 |
NX displayed an error "Invalid or Corrupt Function Pointer" when switching from |
2241492 |
Disallow dimension text override for inherited pmi sketch dimension |
2241555 |
Extra bodies translated while exporting the JT file |
2241627 |
Angle on Arc _ Ellipse option does not work correctly |
2241710 |
'Run ID' attribute is not added to the parts added in the active Run |
2241788 |
Enforced Displacement constraints with SPC card in NX Topology Optimization |
2241965 |
Cannot open_translate catpart in NX |
2241975 |
Cylindrical coordinate system will increase on re-opening the file |
2242396 |
Checking failed for this part, please report an IR |
2242429 |
[CAD] The numerical value set by "Qualify Part - Multi" is cleared |
2242549 |
[TQ] Design Rules are unavailable in NX 9 |
2242613 |
Checking failed for this part please report an IR |
2242624 |
The creation steps of Dimension differ to the view which created View Break |
2243057 |
NX 9.0.2.5 Power drafting issues after import of AutoCAD file |
2243213 |
Not able to open catia V5 R23 part in NX 9.0 |
2243416 |
Edited Sub-assembly is not getting saved on saving top assembly |
2243702 |
Can the corrupt Global Shaping features be fixed |
2243778 |
Paste operation response time of feature(Body) is deteriorating |
2243849 |
Checking failed for this part please report an IR |
2808636 |
ug_expression_string value can only be changed from KF once |
2808652 |
Saving the part results in Internal error: invalid solid object tag |
6505295 |
NX crashes after defined Stock Offset Vector in Spline Path dialog |
6507049 |
Assign Discontinuity twists a rectangle space reservation |
6612662 |
Flat pattern annotation is lost if on a sheet other than sheet one |
6630885 |
After self intersection sweep alert message click tool icon gives Internal Error |
6631793 |
Linked ports created by filter setting Face_Two Lines are not have associativity |
6648606 |
Can't select subassembly for remembered constraints |
6696798 |
Unexpected deformed geometry display |
6713291 |
Show = False on a Tab Page hides container items rather than the Tab itself |
6716643 |
Stock cannot be recreated after removing parts of mirrored assembly |
6747086 |
NX 8.0.3.3 - Elec - Spline Path Editing insert point is not correct |
6764791 |
Legacy part family warns when populating members with material from Library |
6781649 |
Z-clipping is not correct in a legacy broken view |
6812874 |
Assembly opens modified |
6910662 |
Drag and drop adding stock like a part |
6924642 |
[v1] Deleting a component, a piece wiring is "deleted or hidden" and connection |
6934007 |
Select default part type on Import assembly into Teamcenter |
6937634 |
Error opening file Object supplied is of the wrong type |
6937825 |
Cannot select Path Segments for Members defining a Run in the context of 4GD |
6943140 |
Part is marked modified after reopen |
6945276 |
Radius dimension for arc to center does not pass thru center |
6945456 |
Send MultiCAD JT to NX fails to show Assembly Cut |
6947529 |
2D Centerline jumping to another hole of pattern array when created |
6950987 |
Appended text on hole dimensions causes dimension to disappear |
6955206 |
Rounded Corner stock inverts vs path when the Tangent Straight path is moved |
6956275 |
NX: Silhouette of the curved surface does not appear in the view |
6957145 |
Delete Routing Objects to delete a path does not delete RCP's. |
6959187 |
Load to NX from TC Not Respecting Overridden JT on Occurrence |
6960514 |
NX: Replacement of Datum Plane does not reparent reference vector dependency |
6964960 |
Load interpart data ON causes cyclical load_"update objects" when working on dwg |
6966979 |
PILO Points will not update to new inputs after relinking |
6969622 |
Component not displaying in drafting view |
6969727 |
Migrated assembly shows as modified when open in NX |
6972408 |
Cannot get angular dimension to show the smallest included angle |
6974714 |
Double underlines in Detail view and section view labels |
6975352 |
NX 9 Web Browser Home Page URL does not work like NX 8 & NX 8.5 |
6977180 |
Import Assembly Into Teamcenter - Default part type is not assigned |
6978336 |
NX 296459: Pattern Feature fails for a User Defined Feature |
6980255 |
Problem w_ setting W4 on Rotor Region to an expression |
6980602 |
Internal error replacing pattern with user defined symbol |
6985171 |
Patterns containing User Defined Symbols report error, can open 2nd attempt |
6986617 |
Angle dimension in Drafting Application, cannot get the acute angle |
6986715 |
Extracted Edges in Exact views cannot be mapped to the original modeling Edges |
6988352 |
Internal Structure of JT File Different Between NX 8.0.2 and NX 8.5.2 |
6989644 |
When opening a part file,the Patterns are not loading |
6990394 |
Modifying a part is not updating in NX.8.5 and in NX 6 |
6990741 |
Errors saving assembly with PMI attached to components containing JT Override |
6990966 |
Thicken feature produces different results after playback |
6992657 |
Position of linked sketch geometry doesn't update - Drawing dimensions incorrect |
6996501 |
View dependent edit works differently in NX 9.0 then in NX 7.5 |
6998253 |
Problem with AssociativeText.GetObjectPropertyText |
6998912 |
SubsetRecipe iterator throws a Java Runtime Environment Exception |
6999252 |
View will not update - modeler error |
6999850 |
3601 Edit RUN In 4GD environment, cannot select stock to add or remove from run |
6999932 |
PMI Cut Arrows Rotate beyond 90 Degrees Appear Improperly in Vis |
6999933 |
PMI Cut Arrows do not display properly in Vis Using Reorient Text |
7000242 |
NX CAM, Simulate Machine, the IPW is continually disappearing and returning |
7000626 |
Multi-cad JT incorrect behavior when partial loading on or use custom seed part |
7100262 |
Radial PMI dimension dialog has overlapping tabs |
7102547 |
Unable to open a drawing sheet. Cannot move view off of the drawing |
7107738 |
NX: Calculate Penetration is giving extreme measurements instead of interference |
7107857 |
Object has no valid file root |
7108504 |
Sum, and hence the average, reported by the 'Identify' command is not accurate |
7109653 |
NX: STEP imports PMI and will not fit to screen |
7110491 |
How to set Component as a Splice using CMP_HRN format netlists in Routing |
7111244 |
Checkmate "GDDQS-BQS Profile" Crashes NX |
7111714 |
MW:Custom metric lifter auto engraving curves show up in NX 7.5 but not in NX 8.5 |
7111922 |
Error in syslog setting UGII_ENV_FILE |
7112097 |
Wire EDM path generation is inconsistent |
7112738 |
Unable to load parts "The record area asked for does not exist in this object" |
7113932 |
NX should block the saving of DE which have newer version in Teamcenter |
7114199 |
Variable Axis-Operation will not generate after re-selecting part geometry |
7115060 |
Maco changing ribbon to classic fails to change |
7117153 |
4GD:Attributes from Design Features do NOT sync in a new NX session |
7117380 |
Assembly drawing is out of date after update and save |
7118071 |
Can't replace component in drawing Internal Error : Memory Access Violation |
7118724 |
Save As Dialog takes very long time in Tc10.1.1 _ NX 9.0.1.3 |
7119098 |
NX: Replace reference sets taking too long |
7119584 |
Routing PTS part, smart initialization needs to work from port attributes |
7120134 |
Fastener Assembies in NX 8.5 are not working as they did in NX 7.5 |
7120325 |
Cut Level changed when copying operation from NX 7554MP10 to NX 9013 |
7120753 |
Electrode Properties do not update after pattern component is deleted |
7120791 |
Prog Die wizard BOM issue |
7121365 |
Removed command_functionality "Variant Configuration" from NX 9.0.1 |
7121774 |
Pattern Feature removes part of two instances of a blend Feature |
7123257 |
Exact representation does not show sketches on visible layers |
7124053 |
Change Positive Direction settings does not change dimension to Negative |
7124164 |
Selection of multiple solids creates one wave link feature |
7124362 |
Smart Lightweight view performance issues |
7124364 |
Routing Mechanical - Delete Routing Objects Leaves RCPs |
7124410 |
Routing Mechanical - Parallel Offset Paths Always generates Associativity |
7124482 |
3D Swept mesh is mismatched between 2 meshes with glue coincident MMC |
7124552 |
Routing Mechancial Checker reports 2 different warning for same radius |
7124701 |
Enlarge Surface Patch Trim Body and Trim Part commands not working NX 8.5.3 |
7125384 |
NX part family spreadsheet does not get dismissed |
7125521 |
UF_WAVE_load_parents no longer returns failure information |
7126163 |
Retaining Datum Feature Symbol attached relationship to a Feature Control Frame |
7126274 |
NX - sections stay in clipboard |
7126379 |
Toroidal Faces Silhouettes Error Display (Inch units model in MM units drawing) |
7126828 |
FBM fails to update flag for part with a preceding drill operation |
7127120 |
NX - Local Untrim and Extend issue |
7127797 |
Bridge curve UI dialog: needs to show section pick point position |
7127815 |
NX to TcVis Interop causes multiple login prompts to appear |
7128012 |
DXF_DWG: NX filename with comas cannot be translated interactively |
7128778 |
Assembly clearance analysis produces very wrong results |
7128791 |
Assy Clearance Analysis penetration very wrong with lightweight analysis |
7129211 |
PDW Component Drawing doesn't follow View Scale as in template |
7129326 |
Weld Issue - Edit Fillet weld-cause Refresh problem |
7129334 |
Display.RasterImageBuilder Width and Height properties do nothing |
7129543 |
LineWidth enum names do not align with True Type font menu options |
7130658 |
Extra JT dataset on revise from NX |
7130738 |
Error editing a GD & T object |
7131431 |
3d hex mesh mesh is creating Abaqus elements inside out |
7131681 |
Can no longer map from an Exact extracted edge curve back to the model mode edge |
7133671 |
Corner Smoothing is inconsistent in newer versions of NX |
7133936 |
UF_SHOPDOC_generate_doc throws memory access violation |
7134429 |
Add Reusable Component and Add Component orient parts differently |
7134842 |
Nominal and deviation values not showing on CMM report |
7135008 |
MW DME moldbase - no way to specifiy plate thickness in dialog |
7135558 |
PMIs created on the JT-Override data go retained when reopened |
7135888 |
Split Profile_Plate:Unable to perform split on the highlighted solid bodies |
7136499 |
CycleObjsInComp does not progress to the next Tag when remoting |
7137396 |
DME Type Moldbases questions - cannot specify plate height |
7137497 |
Engage and Traverse vectors changed when regenerated in newer version of NX |
7137498 |
Engage Vector changed when generated in newer version of NX |
7137510 |
FEDRAT statements added and deleted |
7138672 |
Extra Attribute added to top part in assembly |
7138775 |
Unexpected value error when unsuppressing adopted Linked Body feature |
7139476 |
Update Shared Body in Part Module hangs NX |
7140726 |
Arabic fonts created in reverse order after Pasted in AE or Curve Text |
7141299 |
An RM object had an unsuitable OM class for this situation, NX 6.0.5 MP12 |
7141618 |
UF_ATTR_assign returns 512054 |
7141740 |
PLMXML Export Topology Omits Connector When a Built in Path is Used |
7141817 |
Rule Based Structure Weld LAP Weld to use different values Near & Far Side |
7141956 |
RBSW Weld Joint - Using INFERRED for a corner results in a LAP Joint Type weld |
7142346 |
After updating a view, Bad Pointer error during a save |
7142405 |
Tc 4GD - Checkout of DCE's in NX is inconsistent |
7142569 |
Grouping issues |
7142596 |
4GD Partitions without "AddContent_Remove Content" don't display Names in NX |
7142603 |
Cannot safely get geometry using nxopen.RuleManager.evaluate( referenceChain ) |
7142967 |
RBWS Edit Joint Definition - CORNER Preview image is open vs closed |
7143001 |
RBSW Create Joint; T weld manual multiple build data that cannot be created |
7143762 |
Detail view label underline has double lines |
7144102 |
ERROR 1250 :Serious error (code [903]: [Out of memory]) encountered during trans |
7144850 |
Clearance Management highlights the same Clearance Feature |
7145325 |
Laminate Post Report Spreadsheet -- Wrong Cell Highlighting |
7147204 |
LMA PMI:Severe Error open assembly if all JT Override Occurrences configured out |
7147289 |
Stock becoming segmented after assign corner |
7147545 |
Compliment Angle is being created after placing the dimension created |
7148221 |
NXMGR: Item Name is not correct when saving to a new Item |
7149077 |
FEM materials don't update when material library is edited |
7149486 |
Not able to select POINT when Qualifying a PORT |
7149592 |
Upon open - Internal Error: Memory Access Violation |
7149598 |
Can't modify extension length on Port in Qualify Part |
7149686 |
Surface Moved Outside Control Surface |
7149690 |
Surfaces moved outside the control surface |
7149698 |
Surfaces moved outside the control surface |
7149722 |
Global Shaping Results Sewing Issue |
7149726 |
Global Shaping Results Sewing Issue |
7150286 |
PM request across chamfer with adjacent structure of different thicknesses provide |
7151058 |
Regression in Save All |
7151618 |
Miter fails in projected curves |
7153820 |
Sheet template attribute won't update |
7154664 |
Hole table issue thread depth not displayed correctly and in two groups |
7157553 |
NX: file export IGES crashes NX |
7157604 |
Setting units to lbm-ft results in incorrect Longitudinal Y-Frames and Z-Frames |
7158034 |
Internal error: memory access violation; Tabular Note cell Edit Settings |
7159960 |
B AXIS rotation issue |
7160758 |
Cannot edit invisible expressions error while editing UDF parameters |
7164182 |
Issue regarding TC classification fixed in NX 9.0.2 |
7165470 |
Penetration Management: PAX file issue for cutout object |
7166108 |
Rapid dimensioning in assembly context gives wrong result |
7166248 |
Assembly fails to load due to linear dimension - Objects do not intersect |
7167149 |
Unable to specify lesser than 103.622222K for initial condition BC |
7171582 |
DisplayObjectsDetails writes attributes to Info window not selected device |