PR # |
Description |
1507698 |
CAM: Drill - the Parameters from Tool-Edit does not match the correct Values |
1559541 |
Display of group name in NX Manager |
1620108 |
CAD: SMD - resize bend angle does not work |
1652542 |
The "exec" Command from TCL let UG hangs on High Speed Machines |
1691930 |
Neutral Fact or error raised with custom Bend Formula |
1693114 |
NXOpen > Curve > GetLength method returns inch values in batch mode |
1698480 |
Flat Pattern view, curves display Disoriented (circles) |
1701274 |
PRO: NXOpen method GetBendParameters returns wrong angle values |
1706449 |
MP - An attempt was made to create a link between objects in different parts |
1714588 |
Mark Sharple's - team - 'single math' operator 'square of magnitude' wrong... |
1718464 |
Preview of selected polygon face lost when switching display or sectioning |
1735115 |
Assemblies can not be opened with NX 6 |
1736814 |
Unable to load the customer defaults for flat pattern |
1744169 |
Replaced component is replaced in two assemblies with no warning |
1744306 |
Customer Color palette cannot be loaded when using an Environment Variable |
1745627 |
The type of this document is not managed by the CATIA Teamcenter integration |
1746059 |
NC: Part does not fit properly when immediate view animation speed is set |
1747032 |
Mirror body linked to later split body |
1747547 |
Gouge Check reports erroneous gouges with negative Part Safe Clearance value |
1751040 |
Fix for PR1735115 does not fix all cases |
1763817 |
Playback fails in NX 6 with error "Failed to construct draft surfaces..." |
1770635 |
Open part already open in session: "Failed to load part" rather than "Reopen" |
1773402 |
TRA: DXFDWG: non-expandable blocks do not import to NX |
1774752 |
50% of all Ventilation holes Marking Sketches are Wrong |
1774756 |
The Top-values of the frames should be the same of the base |
1776544 |
Steel Distribution profiles jumping around |
1777061 |
PRO: wrong property recorded for RelativeConvergenceCriteria in Optimization UI |
1777403 |
CAE: Automatic Coupling shows wrong direction for dof |
1778947 |
File recovery from Internal error: memory access violation |
1779143 |
BETA: Missing leader for balloon and coordinate note |
1779151 |
BETA: Custom symbol frame out of position |
1779159 |
NX 5 JT compared with NX 7.5 ph32 JT are different |
1780744 |
Unable to add components when in a manifestation part |
1781295 |
Move/copy component results in random db_part_no |
1782633 |
Assembly Add Component Button Not Working |
1782885 |
TC_CAD: PR 1= 780744 Unable to open "add component" menu |
1782959 |
NXManager: Add Component does not work for specifications since NX 6.0.5 |
1783558 |
Unable to open "add component" menu in specification |
1783923 |
IPW is wrong after a Tool collision was detected |
1783997 |
NX Ship: Stop at intersection does not work |
1784150 |
Clearance analysis problem on Linux (French only) |
1784559 |
RMU does not show the same result as toolpath cuts - incorrect remaining blank |
1786568 |
NX Ship: problem with manufacturing xml output |
1786838 |
NX Ship: Feature Migration from NX 5 to NX 7.5 |
1787581 |
Unable to add components when in a manifestation part |
1787720 |
Contact Data ON produced "Corner Endpoint Failure" on Machine controller |
1787835 |
Unable to add components when in a manifestation part |
1787958 |
Linked body not updated correctly applying part family values with assem.constr |
1788039 |
Die Flange Steel re-strike with cam direction not parallel to Z absolute |
1788875 |
CAM Templates fails to load carrier, pockets and tools under the unused group |
1789155 |
MP - Clearance analysis problem on Linux O_S (French only) |
1789752 |
Keep Selected Flips the Start and End, and the Guide Offset Direction |
1789755 |
Keep Selected Selects All Sketch Curves instead of those only intended |
1789807 |
TRA: Dimensions associated to intersection points are notes and lines after ugto |
1791387 |
PRO: ExtractFaceBuilder.GetCommittedObjects() returns first feature only |
1791874 |
ROU: Length of routing object does not update in top assembly part |
1792079 |
Internal error while converting mating to constrains |
1792528 |
Mesh not generated after FEM update |
1794221 |
Unable to import dwg file in NX on Linux |
1794226 |
FACE_MILLING operation creates a wavy toolpath which gouges the part geometry |
1794430 |
CAD: Copy_Paste of sketch curve into modeling crashes NX |
1794711 |
MW Part naming rule numbers different as of NX 6 |
1795238 |
Problem with Step 203_214 export get an IM0522 error |
1795287 |
TRA: Step214 Import- arcs generate to "GENERATED CIRCLE" |
1795416 |
Part Family Member cannot not be opened in NX 6 or newer |
1795659 |
NX 4 Drawing will open as modified in NX 6 after refile_part -cleanup |
1795872 |
Face Milling takes almost 20 times longer to generate in NX 7.5 compared to NX 5 |
1796723 |
Import part in NX manager with "create named group" produces a wrong group name |
1797130 |
CAD: NX 6 Feature Control Frame with Leader Type Datum: Internal Error when edit |
1798546 |
Saving imported Part Family Member over Reuse Library returns Err-64 bit only |
1798712 |
GTBC - Assembly constraints out of date after edits (help points) |
1798856 |
NXOpen > Curve > GetLength method reports inch values in batch mode |
1798908 |
Strange behaviour in copying spline paths in Electrical routing in NX 7.5 |
1798990 |
Changing SB Resize Bend Angle causes an unexpected rotation |
1799072 |
Problems with using Reuse Library Modeling Data inside NX |
1799450 |
KF: ug_body.dfa calls a non existing function ug_sheet_askBoundaryEdges() |
1799469 |
CAD: convert to sheet metal fails with a neutral factor error |
1800316 |
CAD: Instanced threaded hole cannot edit by MB3(make sketch external) |
1801221 |
Cutter corner radius changes while copying operations from one part to another |
1801234 |
NX 4 Drawing will open as modified in NX 6 after refile_part -cleanup in NXMgr |
1801377 |
MP - After TCEng 2005SR1 patch MP9 and NX 6.0.5 SOA object property error |
1802546 |
mom_fixture_offset_value not generated for LATHE_CONTROL. Fixed in V8 |
1802773 |
GRIP -Transfer_Rapid template setting not maintained - OPER_NEW |
1802976 |
Check-out policy for remote items ignored |
1802986 |
Cannot select geometry in replacement assistant if loaded lightweight |
1803319 |
Unable to create Ramp in NX 7.5.1.5 PDW for Punch |
1804169 |
NX SHIP: Distribution doesn't work with Teamcenter and 64 bit NX 5 |
1804372 |
Error when open a file with NX 7.5 |
1804415 |
PTS UI lost after saving part with a syntax error in KF function |
1804460 |
Problem with string expressions from PTS containing German special characters |
1804466 |
CAM: PR - cannot execute the function MOM_abort (PR-06197540 ) |
1804643 |
Project initialize regression with suppressed components in NX 7.5 |
1805038 |
Deforming Cable assy explodes the assembly |
1805444 |
Screw gets wrong orientation when positioned on Washer |
1805787 |
Unexpected tool moves in "Contour Profile" operation |
1806001 |
After open assembly state is modified |
1806098 |
PLANAR MILL- Floorplane in boundary not associative with model |
1806346 |
Error when verifying and simulating turning toolpaths generated in UGV18 |
1806732 |
New UDE TYPE l and TYPE g cause UF_UDE_ask_integer to fail |
1806758 |
KF Class '%ug_comp_select_file' fails on Linux |
1806908 |
Cannot export to XML with "Manufacturing XML Output" |
1807007 |
Hole with depth limit "Until next" fails update if parent is deleted |
1807031 |
Planar Mill: Floor-Plane is not associative when selected inside Component Part |
1807083 |
Part family removes "User defined" flag from expressions |
1807138 |
Custom Symbol raises warning when adding a new library |
1807410 |
Unable to use formula in Weld Point dialog |
1807563 |
Error message "NULL TAG not allowed" occurs during View update |
1807642 |
MP: Check-Mate Check Dimension Tolerances results in a internal error |
1807732 |
NX-MAC: NX 7.5 .reg unable to save in OOTB install after read in new Palette |
1807760 |
Component with empty named reference leads to fail to open assy |
1807804 |
Failed to Save with code 580134 "Attempt to save bad pointer, save abort" |
1807955 |
Mark Sharple's - team - 2d mapped meshing gives poor resultant mesh... |
1807965 |
Pocket not created on promoted body in assembly |
1808101 |
Assembly contains unexplained references to old part when importing into TC |
1808126 |
Regression in pattern face |
1808141 |
Could not open part containing routing objects in NX 7.5 but no problem in NX 3 |
1808159 |
Part does not open in NX 7.5.1 due to data error |
1808177 |
Open part already open in session: "Failed to load part |
1808179 |
Open part already open in session: "Failed to load part |
1808180 |
Open part already open in session: "Failed to load part |
1808202 |
Modeler error: non-manifold body or boundary |
1808240 |
Wrong pattern when placing bolts in the opposite direction of holes |
1808248 |
Toolpath changed from arc movement to lineal after regenerating from NX 4 to NX 6 |
1808273 |
Placing View (Faceted Representation) takes 4 times longer |
1808323 |
File size increase dramatically after saving NX 4 drawing in NX 7.5 |
1808456 |
Manual update from material library issue |
1808515 |
Problem with manufacturing xml output, marked circles are not exported correct |
1808518 |
Problem with manufacturing xml output, marked circles are not exported correct |
1808521 |
Problem with manufacturing xml output, marked circles are not exported correct |
1808581 |
Ship Design: Problem Steel distribution, unsuitable OM object |
1808788 |
XML file handling in CSE driver fails |
1808790 |
Face Mill Area ignores Cut Region Start Point in NX 7.5. Was correct in NX 5 |
1808888 |
Load Options with Symbol "$" in the path didn't work in NX 7.5 |
1808933 |
Unable to save an assembly in NX, if it created in TC (StructureManager) |
1808976 |
Tool-axis flips after copy operation |
1808982 |
Translating ProE Wildfire 4 M120 files to NX fails |
1808994 |
Blank Layout does not find UP_DATUM_FACE if the Stationary Face |
1809103 |
Crash NX selecting Part Navigator or Internal Error Part Cleanup or Playback |
1809126 |
Tag 0 resolves to NULL, Incorrect object for this operation |
1809173 |
Cut region in UGNX 6 different than UGNX 4 |
1809205 |
Failed to load part when trying to load object on demand |
1809378 |
File can not be loaded: Internal error |
1809432 |
Error removing retained handle while editing full bolt circle associativity |
1809550 |
ug_face_askEdges - hostpointers to non-work part objects without part_name |
1809755 |
Incorrect error message if required step file is not available |
1809762 |
Create or update part family member goes to update loop |
1809877 |
NX 7.5 complement arc su sketch |
1810131 |
Unable to reposition NX 5 hole in NX 6 |
1810146 |
CAM: PR - post-processor does not realize a GOTO with only a Wireangle change |
1810571 |
Missing text if importing IGES File from CATIA 5 in NX |
1810687 |
NX Ship MP9 - XML-Output: Missing Text Information for MarkingLineSymbl in XML |
1810724 |
Cannot open assembly with empty components in NX from Structure Manager |
1810768 |
Fail to load part in NX 7.5.1 due to invalid solid object tag (820022) |
1810806 |
Unable to o en assembly in NX 7.5.1, get "Feature is created without partition ma |
1810933 |
Specification always being marked "Modified" |
1810936 |
PRO: NXOpen method "GetBendParameters" returns incorrect angle value |
1810974 |
Every time user creates a new part he gets information window |
1811111 |
Mark Sharple's - team - re-sizing geometry corrupts mapped & swept meshes... |
1811121 |
Spanish language issue |
1811350 |
Not possible to add component to altrep - similar to PR 1803640 |
1811426 |
Copy and Paste CAM Operation Causes Tool Axis To Change |
1811718 |
MP Tabular Label works in single level model only, not in assembly |
1811961 |
Using Quickpick in Find Selected Component shows blank entries |
1812115 |
KDA: StepSt tus ignored in %ui_comp_point as of NX 7.5 |
1812120 |
Strange behaviour for Section view update |
1812216 |
Fastener Assembly creates wrong thread depth |
1812410 |
Empty tool-path after transform operation via Grip |
1812502 |
Cannot Open a Part in NX 7.5-invalid solid object tag |
1812532 |
Engage change direction after transform operation via Grip |
1812613 |
Pre-load problem using nx flow results |
1812718 |
CAM: 3D Prile operation with extend at edges mills the contour not complete |
1812760 |
KF: ui_comp instance updates UI in all open parts with apply_state3Dedit |
1812773 |
CAD: Bend is divided into two bend areas when using 'SB Resize Bend Angle' |
1812829 |
Transform operation via GRIP change clearance plane |
1812951 |
Automatic edge-edge stitch not successful |
1813074 |
NX 4 to NX 6 - same safe distance parameter results in different tool path |
1813120 |
Part is not a valid version of component part |
1813141 |
MP: "Invalid Object" message if loading assembly in TC Integration NX 6 |
1813337 |
MP: Cannot retain the Replace Component: Component Name dialog setting |
1813628 |
Internal Error while opening assembly top level part |
1813887 |
Export Turning Grooving Tool into Library returns Error "dbc_tool_left |
1813969 |
ERROR "can't read dbc_tool_left_tracking_point " after export Tool |
1814149 |
Reverse toolpath problem NX 6.0.2.8 ( CAM) |
1814304 |
'undo' does not (only) undo 'node drag' operations... |
1814620 |
Turning cut region in NX 6 different than NX 4 |
1814852 |
UDE problem with NX 7.5 |
1814885 |
Problems loading assemblies with altreps-> invalid object messages |
1815084 |
CAM: PR - Error: can't read "dbc_tool_left_tracking_point" comes during Library |
1815096 |
CAD: Updating a drawing hangs the system |
1815200 |
UFDraw.AskBoundaryCurves returns error |
1815218 |
Post-processing to the MILLTURN post locks NX |
1815286 |
Open assembly the altrep is replaced by the 3D-Master |
1815383 |
Blend centerline fails on edge blend and face blend |
1815525 |
Create Component Pattern fails from reuse library part |
1815901 |
KF - dialog based on %ui_comp class doesn't maintain input on opening |
1816064 |
Cannot disable the background on some section views |
1816126 |
Sheet2 on specific drawing is not possible to open in NX 7.5.x on Win 32-bit |
1816200 |
UGMGR: Some parts are new in the session. If you select OK it will save all new |
1816211 |
Can't set default ItemType with .pax file |
1816254 |
Order of Reference Sets while loading an assembly is not used as expected |
1816539 |
KF: Multiple 'Evaluate Temporary Rule' UI's throws internal error |
1816561 |
PR\ container and sims BCs not synchronized: red bullet not filled |
1816579 |
Update detail view "Bad number of dimension subscripts given for attribute" |
1816653 |
Replace Component, Properties -> old part name as the new component name |
1816695 |
NXSM: 'Resize Bend Angle' causes an unwanted rotation of part |
1816999 |
Object names are lost when using associative copy |
1817062 |
Inconsistencies on the user interface for Human Modeling |
1817114 |
Revision rule not honored after adding component to specification |
1817184 |
Placing part family from reuse library takes a long time |
1817336 |
Profiles have wrong length after being updated |
1817686 |
MP: please Backport fix for PR 1781295 to NX 6.0.5 |
1817791 |
Automatic stitch not fully successful and manual stitch result in crash |
1818092 |
Add Reuse Library fails - The library name or library path is already existing |
1818129 |
NX Structure does not update Teamcenter CadBom when using custom item types |
1818158 |
Internal Error message when activate display label |
1818205 |
Is not possible to edit positioning of a pre-nx5 hole |
1818298 |
Place Part, PFmember selected but the PFtemplate is placed |
1818470 |
Internal error when deleting unused expressions |
1818489 |
Z-Level Profile operation generates incomplete toolpath |
1818530 |
CAM: unexpected tool flipping in "Zlevel Profile" operation |
1818551 |
CAD: Custom Symbols (Reuse Lib) in NX 7.5 reports loading before and after insert |
1818890 |
PS23.01.149 - Edge Blend overflow settings does not keep shape from NX 5 |
1818893 |
UGto2D breaks down with unknown exception |
1818934 |
Curve projection not completed - same projection correct in previous versions |
1818972 |
Simulation incorrectly Displays an Operation when using CSYS Rotation |
1819020 |
Selecting an Operation using MB1 crashes NX_CAM |
1819154 |
Auto Balloon Performance is not acceptable |
1819189 |
Import of I-DEAS symbols will crash after returning an internal error |
1819335 |
Reclassify Feature Group ignores classification criteria - now fails in NX 7.5 |
1819352 |
MP : Save operation fails with internal error - same issue as PR6412690 |
1819558 |
Beam Section Manager displays incorrect geometry in Cross Section Preview |
1819670 |
PRO: &VWDEP grip call fails in NX 7.5.x with Internal Error |
1819759 |
Problems with expressions in PTS using German characters in expression name |
1819793 |
Custom weld points have the same marker_symbol in NX 7.5 |
1819810 |
NX Sheet Metal Flat Pattern Orientation vector flips |
1820056 |
Regression in CATProduct translation, signal 11 |
1820081 |
Adaptivity setup does not work with this model |
1820142 |
CAM: Open CAM assy fails with "no such parent" caused by ONT MCS column |
1820167 |
MW Edge Patch does not work in assembly context |
1820258 |
Copy EXTERNAL_TRIM and Paste Inside - throws internal error and exits out of CAM |
1820292 |
Update detail view "Bad number of dimension subscripts given for attribute" |
1820307 |
Export_Import from User Defined Tools over Library gets error on retrieve |
1820353 |
TCUA: SYS: TC8.3_ NX 6 Access Delay |
1820540 |
Revision increments in NX even when Save As error occurs |
1820643 |
Severe performance problems for File-> Save as of a part file derived from a JT |
1820778 |
MP - Cannot add MW standard part in NX 7.5.2.5 with Legacy Method |
1821073 |
NX Shape Search window is not sizeable |
1821093 |
Export -->JT from Unigraphics Not working with UGII_GENERATE_MULTI_CAD_JT=3D1 |
1821095 |
Newly created_qualified stock cannot be assigned using Detailed_Simple style |
1821137 |
Save fails with Internal Error after break Wave links in assembly context |
1821185 |
Russian Language Category description is displayed in wrong encoding |
1821251 |
Hole feature reports syslog error "Do Not call UICOMP::refresh_dialog()" |
1821344 |
Different Prt Name Management Dialog in PDW |
1821409 |
CAM: Zlevel Profile tool axis flips 90 degrees |
1821454 |
NX 7.5.2 behave differently than NX 5.0.6 with mirror feature |
1821483 |
Analyze measurement and expressions shows different result |
1821509 |
AppendBndFromCurve fails for NOCORE CamBlank geometry in NX 7.5 |
1821662 |
Update detail view 'Bad number of dimension subscripts given for attribute' |
1821742 |
2D NX Symbol library problem |
1821778 |
MP: Ship Mfg. XML output MP7 vs MP9 is different |
1821907 |
PRO: NXOpen routine "GetInnerBendFaces" returns incorrect faces |
1821946 |
PRO: NXOpen method "GetBendParameters" returns wrong angle values |
1822002 |
CAD: Base lofted flage shows incorrect result |
1822069 |
Customer Defaults must accept variables for ShapeSearchWorkDirectory |
1822077 |
ugcheckmate.dat no longer works when referenced in UGCHECKMATE_CONFIG |
1822111 |
CAM: unexpected tool flipping in "Zlevel Profile" operation |
1822209 |
The command Flat pattern fails on simple un-parametrized |
1822226 |
Tool axis change after making a copy of an existing operation |
1822276 |
Blank Layout ends in Incorrect object for this operation |
1822506 |
The CSYS appears and cannot be deleted |
1822665 |
MP - Routing Bill of Materials does not list Stock in non master part |
1822704 |
TRA: Missing Surface Finish Symbols after translating with ugto2d |
1822783 |
Assembly exported from NX into CATIA has changed structurally |
1822786 |
Exploded Assembly after export to CATIA |
1822814 |
UGII_LANG =3D Italian - Internal Error, Memory Access Violation returned in Runne |
1822992 |
Update of TAB feature fails |
1822996 |
While update sim file NX deletes some objects (constaints,...) |
1823418 |
PRO: Error for invalid layer value of internal sketch plane |
1823536 |
Update detail view "bad number of dimension subscripts given for attribute" |
1823621 |
Different information about density of linked body |
1823623 |
CAE: memory access violation while identify |
1823666 |
Check-mate with save to Teamcenter doesn't update the image_preview.qaf |
1823759 |
Error for invalid layer value for internal sketch points (layer 271) |
1823780 |
Problems using %ui_comp_selection with multiple objects |
1823836 |
Disparition des groupes CAD. - Advanced Simulation removes display of groups |
1823935 |
Ramp on Part option for ZLevel function causes wrong toolpath |
1823966 |
Saving an IPW over "Workpiece - Save as" does not allow to change Item type |
1824131 |
Interpart Expression update failure : no such interpart expression |
1824255 |
Internal Error when reposition Text |
1824263 |
API call UF_SKET_create_dimension behaves differently in NX 6.0.5 and NX 7.5.2 |
1824305 |
Error in post-processor using templates and new Top+Bottom functionality |
1824434 |
Sketch NX 4 fully constraint NX 7.5 over constraint |
1824655 |
Some IPE fail to update |
1824707 |
CAD:- Section view update on drawing takes to long |
1824709 |
Interpart Expression update failure : no such interpart expression |
1824900 |
Move to layer seems not to move all PMI Custom Symbol entities |
1824960 |
Update Assembly constraints |
1825084 |
Deformation does not seem synchronized to local CSYS |
1825534 |
Cannot read WEDM MultipleStepoverBuilder and StockPerPassBuilder values |
1825705 |
Strange x-form behaviour in NX 7.5 |
1825913 |
Edit Interpart Expression changed between NX 4.5 and NX 7.5 |
1826003 |
NX 6 part open fails in NX 7.5 with partition error |
1826004 |
NX 6 part open fails in NX 7.5.2 with partition error |
1826074 |
Error "Bad number of dimension subscripts..." updating detail view |
1826113 |
CAM: OF-PR - the Generation of the internal Toolpath hangs with NX 7.5 |
1826119 |
Bitmap path not displayed using "getenv" path function in PTS in NX 7.5.2 |
1826160 |
Parts using ug_extract_body and ug_udfs in NX 6 don't open in NX 7.5 |
1826357 |
Display by Time' and 'Maximum Angular Increment' missing from simulation options |
1826363 |
CAM: PR - Missing Preferences inside Simulation Options from Synchronize |
1826379 |
Instanced operations are shown as generated but aren't the same as the original |
1826563 |
Part with ug_component, ug_udfs fails to open in NX 7.5.2 |
1826572 |
CAM: PR - Feature Process does not recognize a valid Geometry-Group for creation |
1826682 |
Fit is incorrect depending on Animation Speed if constraints not displayed |
1826814 |
Dimension does not reassociate, if moving a section line and move it back |
1826850 |
Feed Rate Column is empty inside Teach Mode Operation |
1826852 |
CAM: PR - Additional Insert is shown when Tool Display is set to "Assembly" |
1826882 |
Making floor plane creates unwanted broken link body |
1827162 |
Fatal error in turning toolpath |
1827247 |
File > Open (assembly) leads to memory access violation |
1827344 |
KF: selected instance in %ui_comp_selection not highlighted correctly |
1827348 |
KF: %ui_comp_selection upgrade issue from NX 5 to NX 7.5 |
1827485 |
Exploded View not correctly translated in """Managed Mode""", like expected |
1827524 |
UG-CAM: NX 7.5, Part disappears after display |
1827534 |
URGENT: Section View not correctly translated in Managed Mode, like expected |
1827785 |
Z_Level gouges the part geometry in NX 7.5 with Ramp on Part-Level to Level |
1827850 |
Send part to NX via router that is already open in session gives Open error |
1827872 |
Laminate Modeler, Analyze Laminate Strength, Allowable Loads on Laminate wrong |
1827938 |
Create new component does not show the default RefSet |
1827960 |
NX Sheet Metal part continually marked "Modified" after inserting Flat Pattern |
1828089 |
Results can not be opened in NX but Nastran solves without warning |
1828097 |
Highlight of mesh is resulting in time being lost |
1828104 |
TC2007.1.7b and 6.0.5 MP3 reporting the wrong revision |
1828569 |
In Post-processing using Identify command repeatedly then NX will hang |
1828951 |
Replace Component, Properties -> old part name as the new component name |
1829014 |
Part file sizes grow vastly when saved having used Projected Area in Moldwizard |
1829181 |
Distributed mass information reports incorrect information |
1829185 |
" Cut angle vector must not = be parallel to tool axis " error on Cavity mill op |
1829215 |
Error " Bad number of dimension subscripts when updating detail view |
1829235 |
Mark Sharples - team - no 'update fem' icon available after 'offset region' used |
1829487 |
CAM: PR - Using the "User Defined "Holder in Turning Tools return TCL Error |
1829632 |
CAD: Internal Error while creating detail view |
1830008 |
CAM: GRIP TOOL command "out of memory" |
1830659 |
NX Human Active Reach works in NX 6 but not functioning in NX 7.5 |
1830997 |
Custom Symbols (Reuse Lib) in NX 7.5 reports |
1831063 |
UDF replacement overwrites existing parameters, regression to NX 4 |
1831102 |
Open of newly created UGpart data fails to open in NX |
1831519 |
Conversion Nastran from Ansys |
1832104 |
CAD: Unable to open Part file |
1832165 |
Tool axis changes if 'Level to Level' option is set to 'Ramp on Part' |
1832594 |
Assembly fails to load with message "Attribute already exists" |
1832678 |
The roller-ball is meshed incorrectly |
1832737 |
An Invalid Tag was passed to the tag module |
1832841 |
Automatic edge-face stitch stops at 95% in the process |
1832858 |
Copy Electrode fails with internal error when not saving file with head_blank |
1833299 |
NX Open problem on W7 - NX 7.5.2 mp2 (spline slack) |
1833300 |
Formboard is not created if all wires aren't routed |
1833901 |
Unable to Update Finite Element Model |
1834117 |
Checkmate: TC Validation result shows wrong icon, a pass it should be failed |
2079779 |
Analysis-Mass Properties does not reflect the correct Density after model change |
2080819 |
Make the setting 'Element Normals' the default setting and remember it |
2084935 |
Rigid link elements of edge-face connection look weird |
2087403 |
Combine Tris should not allow to select many elements in 1st_2nd selection step |
2087412 |
In Combine Tris dlg, all highlighted elements are cleared by Refresh operation |
2092078 |
Update error after recording when using an external sketch |
2105010 |
CTEST-CPJ:Copy and paste of bead causes displacement |
2105740 |
Can't import Sim file as a part of assembly to NX integrated TC |
2106630 |
Part Navigator hide when switching to History-Free Mode |
2106936 |
The View Borders are disappeared in "View->Layout->Synchronize" |
2110548 |
Save As on component in assy context does not cause all parents to be modified |
2114353 |
An Unknown error is displayed when I change Tool ID and Material Selection |
2118979 |
Syntax check can not work |
2122882 |
i-TEST: DXF of Weld symbol(JIS:"Spot") fails in export |
2129047 |
i-TEST: Cannot Unbend convert to sheetmetal body |
2130740 |
Opening a component from the ANT after Structure Only returns Error Recovery |
2135108 |
As opening assembly fem after saving it twice, error occurs |
2136973 |
i-TEST: Feature Control Frame will not be exported correctly |
2139182 |
CSW:"Stationary Face" of "Resize Bend Angle" will move |
2139790 |
Question about IGES Conversion |
2140249 |
Specified Revision Rule does not work when selecting on Item |
2141651 |
NX 7.5: Modeling :The setting of [Customer Defaults] doesn't become effective |
2141940 |
CPJ: NX data loading behavior is different between TcEng2005 and Tc2007.1 |
2144083 |
Flow cut pa h with Reference Tool has missing areas in toolpath |
2144466 |
CPJ: The second argument of for.NET(C#) API:AskNodeDelta must be an array |
2145528 |
CPJ: AskFcfParms crashes NX session |
2145792 |
PS22.01.247 - CSW:Section view cannot be made due to EB |
2146156 |
CPJ: Rectangle selection cannot do cylinder solid form |
2146261 |
CPJ: AskDirectedDimension crashes NX session |
2146567 |
UFModl.CreateProjCurves wrapped incorrectly |
2146795 |
CSW Cannot edit after Flatting Solid |
2147589 |
The feature error occurs if "Convert Mating Conditions" is executed |
2147776 |
MP: export drawing to part and get 'Internal error |
2147990 |
The Simulation can't open and edit when the Measure object which was created |
2148098 |
The Simulation can't solve in RecurDyn solver with ADAMS function |
2148187 |
NX7513MT-UAF=-041:NX 5 part fails at feature playback in NX 7.5 |
2148350 |
NX7513MT-UAF -098: NX 5 part fails at feature playback in NX 7.5 |
2148506 |
NX7513MT-UAF 64bit-011: Error occurs by executing "Playback" |
2148771 |
NX7513MT-DWG -019: ViewUP The drawing changes after view updated |
2148791 |
NX7513MT-DWG -024: ViewUP: View label moved when updating NX 5 drawing in NX 7.5 |
2148808 |
NX7513MT-DWG -038: ViewUP The drawing changes, when the view was updated |
2148825 |
NX7513MT-DWG -014: Annotation "Note" moved when opening NX5 drawing in NX 7.5 |
2148840 |
Reverse function of the toolpath editor hangs NX |
2148866 |
CPJ-VUP: UAF_UAD Failure(NX 7.5.1 ip3) - NX 6 SB Drawn Cutout fails update NX 7.5 |
2148868 |
CPJ-VUP: UAF_UAD Failure(NX 7.5.1 ip3) - SB Normal Cutout is failed to update |
2148870 |
CPJ-VUP: UAF_UAD Failure(NX 7.5.1 ip3) - SB Break Corner is fails update in NX 7.5 |
2148871 |
CPJ-VUP SB Break Corner(27) and (28) fails in Playback |
2148873 |
CPJ-VUP: SB Break Corner(21) is failed on edge created by Contour Flange |
2149661 |
Flowcut generates improper cut order tool-paths |
2149833 |
Mouse Wheel 2 Zoom fails after pressing MB2 to close line sketch dialog NX 7.5 |
2150555 |
An internal error occurred when doing to close the part file |
2150824 |
[NX_Open] Error occur when creating a curve using with UF_CURVE_create_int_object |
2150859 |
[CAD] Translucency setting is lacked when using light weight loading |
2151658 |
CPJ: Clearance analysis object list contains invalid objects |
2151898 |
Section view update on drawing take approx. 20 minutes |
2152258 |
CPJ: Returning to history-mode "No Target solid defined" |
2152431 |
[CAD] Preview of draft feature and indicator direction are opposites |
2152484 |
Flowcut - Tool path is not generated on top of a rib - NX 7 to NX 7.5 regression |
2152771 |
Part list problem with the Qty filed |
2152909 |
Flowcut Toolpath has irregular moves |
2152915 |
Component group strings in render set dialog is displayed as garbled Japanese |
2152991 |
CPJ: Undock of PNT is reset by changing work part. in ANT |
2153438 |
About the element that cannot be deleted |
2153652 |
Edit model parametric line parameter in drafting |
2153742 |
Projected curves on plane(s) are still displayed with None option |
2153765 |
CPJ: Automatic Override is applied when using "Move Part" command |
2153768 |
CPJ: An over ridden component unexpectedly move |
2154126 |
[Detail View] cannot be created to [Drawing View] |
2154130 |
PS22.01.254: A sheet body can't be split |
2154132 |
2-D Distance of information window on XY plane is incorrect |
2154248 |
Get an internal error caused |
2154334 |
The threshold that is set on this signal chart is different from the one actually |
2154470 |
I cannot edit the text of the ID symbol Internal Error |
2154495 |
LocateNodesOnMesh() always returns Zero count in .AFM |
2154536 |
TSW: when the User uses Update command to the Section View, NX cannot be operated |
2154626 |
CPJ: incorrect results to export "radius of curvature" for curve analysis graph |
2154712 |
CSW : DB_PART_NO and DB_PART_REV are mismatch when copy and paste by ANT |
2154734 |
CPJ: Ordinate Dimension position is not correct |
2154735 |
Cancel Block Styler dialog causes internal error |
2154844 |
CPJ: Component fails to open - "A deleted or invalid class id was used" |
2154855 |
Calling SetWorkComponent() many times causes an error - no GDI resources left |
2154895 |
CPJ: Arc center cannot be chosen using [Move Component] |
2154896 |
CPJ: Component fails to move |
2154921 |
CPJ: Rotating component raises Internal Error |
2154960 |
PointSubfunctionReturn returns 0 in all cases |
2154991 |
Not getting specified radius for Corners --> Smoothing |
2155072 |
CPJ: Memory usage grows when adding Existing Curves to a sketch |
2155221 |
CPJ: Move Part reports overriden after Back then Back or Cancel used |
2155354 |
CSW: File cannot be saved after running Playback |
2155397 |
CAM: cutting order is unusual in turning(Bi-directional) |
2155398 |
CAM: cutting order is unusual in turning(Altemate) |
2155446 |
The revision increments in NX even when Save As error occurs |
2155496 |
CSW: Adding new sketch curves raises Out Of Memory error |
2155551 |
CPJ: Unsupported topology change; Deleting History Free United Solid Fails |
2155643 |
Could not assign stock with internal error on Teamcenter mode |
2155721 |
CPJ: Can not create normal cutout |
2155834 |
Condition of optional "Radius restraint" of bridge curve |
2155871 |
UF_SKET_create_dimension throws internal error |
2155965 |
Block Styler- problem with Specify Plane block |
2155974 |
Setting up of Customer Default settings do not reflect in NX session start |
2155979 |
CAM: It is an error happen when a tool query option is used |
2156046 |
CAM: It does not stop by IPW collision in ISV |
2156074 |
CSW : Error "A deleted or invalid class id was used" when comp selected in ANT |
2156161 |
NX 7.5: Note with 2bytes characters is garbled when importing IGES file |
2156293 |
CAM&Drive displacement during Moldwizard Simulation |
2156339 |
When we create sim and fem without restarting NX, the mesh is different |
2156347 |
NX 7.5 Moldwizard - Adjust Baffle Length does not adjust the length |
2156354 |
If we close winform dialog while quickpick is being displayed, NX crashes |
2156387 |
NX7524MT-UAF-005 Error occurs by executing "Playback" |
2156408 |
[TQ] How is the stress calculated in the case with strain gauge |
2156568 |
CPJ-VUP: UAF_UAD Failure(NX 7.5.2 ip4) - Resize face fails to update |
2156571 |
CPJ-VUP: UAF_UAD Failure(NX 7.5.2 ip4) - SB Normal Cutout is failed to update |
2156575 |
CPJ-VUP: UAF_UAD Failure(NX 7.5.2 ip4) - SB Break Corner fails update. |
2156644 |
CPJ-VUP: UAF_UAD Failure(NX 7.5.2 ip4) - Trim and Extend is failed to update |
2156726 |
PS23.01.152 - CPJ-VUP: UAF_UAD Failure(NX 7.5.2 ip4) - Edge Blend is failed |
2156733 |
CPJ-VUP: UAF_UAD Failure(NX 7.5.2 ip4) - EB failed to update |
2156847 |
Auto chain selector during 1-d mesh causes internal error |
2156901 |
When I create MMC on polygon bodies, the Polygon face is transformed |
2156919 |
Null tag not allowed error appearing for unknown reason |
2157085 |
Suppressed mating conditions are unsuppressed on conversion |
2157086 |
Suppressed mating conditions in assembly unsuppressed on conversion |
2157369 |
NX 7.5: Note with 2bytes characters is garbled when importing IGES file |
2157399 |
Internal Error occurs when updating view |
2157421 |
An unnatural square is displayed when I am using Assembly Navigator |
2157571 |
Idealize Geometry, Automatic Feature Removal, Holes cannot Deselect |
2157604 |
Internal Error when selecting "Region Boundary Curves" without finishing Sketch |
2157616 |
Character corrupts in "Track Drawing Changes" |
2157864 |
zlelvel; pre-drill point eliminates engage from arc center |
2157867 |
When axisymmetric element is copied then get an internal error |
2157890 |
i-TEST: switch to "History-Free Mode", Internal error if suppressed features |
2157902 |
i-TEST: "Mirror Feature" works in NX 7.0.1 but fails in NX 7.5.1 for SM features |
2157937 |
Internal Error appears when opening a part exported from Part Export |
2158063 |
Unable to select Sphere Center for a Weld Point |
2158114 |
The category name and Datum CSYS are added IGES is importing done to NX 7.5 |
2158156 |
Face Collector Block shows some blue curves on blend faces |
2158167 |
PLANAR MILL- Operation status is incorrect after changing floor plane |
2158199 |
Edit Chamfer feature fails with memory access violation error |
2158260 |
Convert Mating Conditions changes the lengths of the wring |
2158295 |
NX 7.5.1 crashed by the command "View Laminate" at Windows7 |
2158508 |
The display of the status of "Constraint Container" is wrong |
2158510 |
Wrong nodes are marked and there appear InternalError when making Candidate DOF |
2158706 |
[CAD] Translucency setting is lacked when using light weight loading |
2158740 |
Internal Error occurs in "Idealize Geometry" for history free mode_promotion |
2158766 |
Chinese characters display as squares after the text is applied |
2158879 |
Face collector block finds lines and arcs |
2158914 |
Internal Error occur by [Circular Blend Curve] |
2158973 |
I can not create fem and sim file by a particular method |
2158989 |
i-TEST: An error occurs in "Find Object" and causing undo last operation |
2159005 |
Add Reusable Component: Use Inferred Constraints is missing from dialog |
2159108 |
Enlarged text of PMI symbol after copying to another model view |
2159111 |
CPJ: Cannotobtain Poisson's ratio or Young's modulus with UF_SF_ask_material |
2159325 |
HNS-TWS1: Cannot use "Move Part" on a part which has "Stock Offset Point" |
2159537 |
[QA] About a behavior of normal cutout of history free |
2159539 |
[NXCMM] Safe Plane specified by path creation is not displayed |
2159540 |
[NXCMM] Exit Point does not update |
2159542 |
Renaming tolerance in Navigator does not update DMIS |
2159554 |
File -> Export -> Parasolid -> "21.0 - NX7.0" is not available |
2159559 |
NX Motion RecurDyn output Incorrect Results |
2159625 |
Japanese language HD3D report imported with ugmgr_vpximport has error |
2159631 |
CAM: It is corner smoothing and NX forces to terminate |
2159744 |
i-TEST: In Japanese environment, Japanese translation of "stock" is wrong |
2159751 |
i-TEST: DB_PART_NO changes after copy_paste of packed components in ANT |
2159830 |
CPJ: NX crashes when you replace a connector in Teamcenter |
2159880 |
NX 4 & NX 7.5 - Open by proximity not displaying components |
2159898 |
An internal error occurs with the Units converter |
2159942 |
DXF and DWG :The character cannot be exported by NX 7.5.2 |
2159965 |
All Free or "All Fixed" command in constraint dialog does not sometimes work |
2160012 |
CPJ: Internal error is raised commenting DIE DESIGN in the license file |
2160018 |
Changing floor plane does not cause operation to be flagged as "Regenerate" |
2160165 |
Measurements are not correct when editing |
2160181 |
Part of the component is not displayed in section views |
2160232 |
[Routing] The attribute of DB_PART_NAME isn't listed correctly |
2160362 |
Could not assign stock with internal error on Teamcenter mode |
2160463 |
DB_PART_NAME attribute value is garbled in Japanese byte character set |
2160500 |
In TcVis, NX Locator PMI via JT is wrong when you flip the model |
2160507 |
CPJ: Internal error occurs using Extrude with " Region Boundary Curve" |
2160510 |
There are two problems in Preview animation of response contour result |
2160525 |
Associative option does not work correctly |
2160625 |
Routing: Overstock information and properties are wrong |
2160636 |
Unable to create Intersection Curve by 2 datum planes |
2160793 |
Zlevel Profile gouges thru the part with Level to Level set to 'Ramp on Part' |
2160899 |
HNS-TWS1: Internal error happens using Transform Path |
2160900 |
HNS-TWS1: Internal error happens when we edit Spline Path in Space Reservation |
2161172 |
Regarding "Clone" using the User Number option |
2161176 |
HNS-TWS1: Editing a fold angle (extension vector), an internal error occurs. |
2161181 |
HNS-TWS1: 'Unknown Error' is displayed deselecting segments in Orient Branch |
2161184 |
HNS-TWS1: In drafting, can not select a single segment for Orient Branch |
2161186 |
HNS-TWS1:Internal Error when placing a deformable part on spline path control pt |
2161306 |
CPJ: Average Temperature is higher than Max Temperature in Report |
2161335 |
Failed to open the part and get error: "View type is invalid or unknown" |
2161493 |
CPJ: Editing a routing path raises a Tag error |
2161728 |
CPJ: Query of overstock information returns invalid information |
2161851 |
Pinned constraints are removed when i-part is modified |
2161913 |
Some of the joint information doesn't display in List Measurements |
2161984 |
Incorrect object for this operation during Move Component |
2161986 |
[DE] The system can not create correct the addendum section of the system type |
2162002 |
Original section disappears after editing the feature to add additional section |
2162005 |
Internal Error in expanded drawing view editting spline pole to block |
2162015 |
NXOpen.UF.UF Sf.AskMeshDimension() throws a NXException |
2162108 |
Rotating part with MB2 after creating WireEDM process gives Internal error |
2162287 |
No JT file is created when loading this specific assembly |
2162293 |
Object Dependency does not highlight children sketch faces |
2162328 |
DXF and DWG :Some dimensions cannot be exported by NX 7.5.2 |
2162329 |
DXF and DWG :[Weld Symbol] cannot be exported by NX 7.5.2_64bit |
2162350 |
Drag the studio spline in expand view get the internal error |
2162434 |
Cut angle vector must not be the parallel tool axis - error |
2162444 |
CAM: Even if it changes Cut Direction by Thread Milling,a picture doesn't change |
2162466 |
The strain result is strange with work coordinate system |
2162825 |
Canceling "Show Thickness by Color" UI throws Internal error |
2163078 |
Create element command is not registered with Undo lists |
2163086 |
Create element command causes Internal Error: Memory Access Violation |
2163497 |
RMB in Fastener Assembly Configuration terminates session or internal error |
2163780 |
CPJ: A revision flag stands by the placement from a reuse library |
5811001 |
CDF path defined in Customer Defaults using vars containing spaces can't be |
5887417 |
k-factor doesn't accept values <0 and >1 |
5915826 |
Linked body does not reposition to new position of mated parent |
5925090 |
PS22.01.247 - Face appears to be 'missing' after creating a edge blend |
5962755 |
Ghost image while doing the sew operation in the idealized part |
6016555 |
The result o f Resize blend is wrong |
6129312 |
Part navigate or flyout |
6152621 |
NX License not releasing through API |
6175381 |
Launch NX from TC takes 35 minutes when display update Report enabled |
6221041 |
Trim Extend command has an error |
6226898 |
Subdivide segment point cube location is wrong |
6249617 |
Draft display indicators |
6255883 |
NX 7.5_BETA: Gateway: CDF not loaded if path contains blanks |
6286993 |
NX 7.5 UAF Testing - Part fails to update in NX57.5 but updates with no issues in |
6288663 |
NX 7.5 Legacy Lathe Tools display incorrectly for Horz flip part |
6288671 |
NX 7.5 Legacy Lathe Tools display incorrectly for Vert flip part |
6288676 |
NX 7.5 Legacy Lathe Tools display incorrectly for Vert upside down part |
6293673 |
Sending a part already open in an NX session raises an UGINTEROP error |
6294854 |
NX 7.5 Legacy Lathe Tools display incorrectly for Vert flip part, 2nd example |
6303607 |
MP Unable to Retain when cloning in TC and Native OS |
6304084 |
File opens modified after saved and re-opened |
6304639 |
In History Free Mode, Edit pole is gray out in Match Edge |
6306654 |
Replace Component is taking a very long time to process compared to NX 4 |
6307645 |
Add lines to replace points in TRIM ANGLE CHECK |
6311882 |
Leader not staying where placed |
6322690 |
mqc_validate HiddenLineSetup does not check ALL views |
6324906 |
mqc_validate ShadingType does not work as documented |
6329917 |
WCS handle is displaying(preview) wrong display when creating Direct Sketch |
6330436 |
Can not create stock between folded stocks |
6332778 |
Distance Measurement not Updating |
6333288 |
Export PDF with shaded view results in white solid body as grey in output |
6333447 |
Replace Part Fails |
6334505 |
Have to make Harness assembly the work part every time |
6334513 |
Adding more then one wire tie causes formboard failure |
6336050 |
Distance measurement does not update |
6337264 |
Failure to update links when Unfreezing Components |
6337718 |
64-bit; create tool dialog is corrupt if template part has no tools |
6340060 |
Every Surface orientation being inverted when using CATIAV5-NX translator |
6340131 |
GM VersUp: Update undo happened. - error 670024 at line 1082 in o:\ugnx751\ip1\s |
6344315 |
A part with the same name is already loaded when open it in TC |
6345563 |
Edit and go to corner all pass and OK the system crash |
6346944 |
Inconsistent feature update when Delay Interpart is ON_OFF |
6347366 |
Unable to copy-paste feature group, cancel results in fatal error |
6348300 |
Error while converting to DXF using 2D Exchange Option |
6358967 |
'Auto Save Cleanup' option does not work. No boundaries created |
6361677 |
Cannot add a component to a specification |
6365474 |
Thread Mill operation with Cutcom does not output Non Cutting Moves |
6368579 |
Invalid Tag NULLTAG (in isValid (2)) when working with Variants in NX |
6368972 |
Unable to t rn off section view background |
6369793 |
Center drill crash into part |
6370762 |
Edit-> Move Object-> Point to Point raises Internal Error in custom application |
6371358 |
Flat pattern note doesn't show up if SB Normal Cutout exists |
6373381 |
Import Assy: Import Number set to Auto Translate, but behaves like Number Rule |
6374754 |
Un-necessary faces added to Copy & Paste - Mapping |
6377126 |
Dynamic Deviation Analysis object is always the top of selection priority |
6377155 |
Measure distance performance is very slow |
6377222 |
Make Current + Extract Body causes un-related Law Extension to fail |
6377751 |
Canceling Wave link information dialog is causing OM Object error |
6377809 |
Spline path not updated after transform path |
6378366 |
PS22.1.252 Cannot get desired Radius in Face Blend Feature |
6378399 |
Could not create subdivide segment after transform path |
6378513 |
Cannot add existing part by Place Part in routing application |
6378527 |
Copy spline and re-associate RCP to linked port is causing an error |
6378645 |
When a component is renamed using Save As, the constraints reflect the old comp |
6379122 |
Place Part Lock Rotation is enabled even though there is no rotation vector |
6379246 |
Modify spline point of rectangular stock spline path is causing error |
6379257 |
Edit circular stock to rectangular stock and drag handle for width is causing IE |
6379935 |
Edit-Stock Offset point result is different depends on offset vector selection |
6379938 |
We want to translate into Japanese again |
6379945 |
Edit Stock Offset point added loop in the spline path |
6379960 |
It takes long time to start X-Form and Match Edge command in History Free mode |
6380353 |
NX 7.5.1 Issue: Fatal error during copy-paste |
6380581 |
View operation by MB2 roll not work after completing command with MB2 |
6380593 |
Edit Overstock length or its position continuously, NX session crashed |
6380609 |
Update formboard Length from Exact to Up to Nearest became overstock strange |
6380613 |
Replace Part does not work if use "Routing Transform" |
6380671 |
Sketch Orientation is not inferred when creating Sketch on Datum Plane |
6383191 |
User Defined not display in expression dialog after being used in PF spreadsheet |
6385344 |
PS23.01.142 - Missing face in edgeblend causes "hole" in final part |
6385811 |
PS22.1.254 Unexpected result using face blend |
6387864 |
Insert a note on a hole - anchor on opposite side of arc causes leader to jump |
6389151 |
Unable to open top-level assembly more than once |
6389358 |
Unexpected update upon loading assembly |
6390026 |
Unable to create intersection point between two joined curve |
6390116 |
PS22.01.254 - Unable to execute (constant radius) edgeblend |
6391914 |
Many ContourProfile Parameters are not exposed to MKE |
6392951 |
Unable to delete CSYS entities unless CAM setup is deleted |
6394185 |
Cannot enter drafting. Cannot extract the curve from edge |
6394287 |
Measurement expression is not updated after linked body was edited |
6395166 |
Leader end-point snaps to the opposite side of the edge of a hole |
6395442 |
EdgeTraceRemoval MKE Flag is not working correctly |
6396316 |
NX 7.5.1 crashes when attempting to performing split body on part |
6396692 |
Cavity mill with reference tool gets different results with cut area |
6397132 |
Drafting exited automatically - CRASH - "Cannot extract the curve from edge" |
6397134 |
PS22.1.244 Unable to execute faceblend. Result previews but will not compute |
6398048 |
Label and PM INote text not exporting to DXF file using 2D Exchange |
6398190 |
Edge Blend fails after a 0.1 mm shift in an upstream surface |
6398600 |
NXOpen > NXObject > Name returns null_Nothing rather than "" |
6398821 |
Intersection Curve inverts following replace of parent features |
6399813 |
Crash in "Model Cleanup_ Face Repair" |
6399876 |
Between Regions --> Departure keeps resetting back to 'Use Common' |
6399894 |
Unable to execute Trim And Extend - Make Corner |
6400356 |
Geometry Linking Failure |
6400425 |
Place Part from the Routing Run Navigator is broken |
6400637 |
Internal error opening parts |
6400655 |
Incorrect Parent_Child relationship after Copy-Paste |
6400677 |
Cannot edit REFERENCE_COMPONENT in NX 7.0 - deleted in NX 7.5 |
6400917 |
Isoparametric Divide make an odd face if use point constructor |
6401322 |
Hang after Update to End or Make Current Feature |
6402685 |
Issue with display of certain views |
6403350 |
Exporting csys' doesn't export the absolute csys |
6403405 |
Die Eng - Trim line development does not create geometry |
6403886 |
Cannot recreate feature because a parent has been deleted |
6405023 |
File - New does not work in Japanese Environment |
6405091 |
Can not change the result of measure components to approximate_exact |
6405358 |
Rapid surfacing: surface boundaries change when feature is changed |
6405424 |
Problem with Arrowheads Translating NX 6 -->JT |
6406295 |
SOA error while opening assemblies with part family members |
6406424 |
Zero Stress in "TOP" results |
6406855 |
Unexpected Failure On Trim Body. Unable To recreate Trim Body |
6407029 |
PS23.01.132 - Unable to execute (constant radius) edgeblend |
6407943 |
Ship Design "Edit Section" UI Incorrect in managed mode |
6408711 |
Java external app fails at startup with java UDO library |
6408856 |
Cast does not work from inside NX after 7.5.1 upgrade |
6409161 |
Check-Mate takes 10 times longer now to display results in HD3D window |
6410710 |
NX 7.5.2.3 - Export - Heal Geometry hangs at 30 percent - errors reported in logfile |
6411381 |
Internal Hook up error - object does not exist opening a file |
6411968 |
Replace does not properly map geometry leading to edgeblend failure during update |
6412067 |
Ghost children exist. Dependencies shows no children but info states otherwise |
6412598 |
When replacing a Plane with another, an incomplete dependency transfer resulted |
6412690 |
Internal error: memory access violation failed to save |
6412720 |
HD3D Check-Mate taking long time to display results for large drawings |
6412963 |
Die Eng module - Draw Bead does not work without a reverse normal |
6414671 |
Resetting blocks using properties doesn't work in Apply callback |
6416444 |
Measure Distance does not work between Faceted Body and Solid Body |
6416607 |
UDF from Swept with Angular Law does not include expressions |
6417185 |
Representation Column does not change after execute Show Lightweight command |
6417285 |
Received internal error after using Pocket function for multiple tools |
6417873 |
UFUi > PointSubfunction and PointConstruct fail on drawing with no views |
6418163 |
Import of Ansys 12.1 INP file causes un-handled exception error |
6418476 |
New segments will sometimes not respect the hide_show status |
6418557 |
LPR Plotting on Windows 7 OS does not function |
6418608 |
Problem with components moving in assemblies |
6418856 |
Filter, body edges selects incorrect |
6419155 |
PTS activation causes internal error |
6419165 |
Error editing crosshatching, valid NX 5.0.4 boundary is self intersecting in NX |
6419180 |
Difficult to map mesh triangular regions |
6419196 |
NX string expression not matching type with design logic function string arg |
6419197 |
2D mapped mesh using curved mid-side option on multiple surfaces doesn't work |
6419684 |
NX 3 UF ported to NX 4 cannot find bodies from mesh nodes on Vertex |
6419769 |
NX Manager creates a new IR when saving an unreleased IR |
6419887 |
WIRE EDM- Open Profile violating the boundary when ON condition boundary |
6421641 |
GOTO point coordinates reflect ABS not WCS or MCS location |
6421921 |
mom_pos_arc center is incorrect when mom_kin_read_ahead_next_motion is true |
6422006 |
Custom Spot weld does not treat as "Weld Object" in Japanese mode |
6422019 |
Edit Mesh does not understand Design Sim when sim is the display part |
6422049 |
Unable to edit a spline path |
6422077 |
Editing Form board spline with shape segment gives wrong result |
6422088 |
VisualC++RuntimeError while creating formboard |
6422092 |
Internal error while updating formboard |
6422108 |
Cannot rotate Flat Oval space reservation by editing spline path |
6422143 |
Internal Error occurred when editing a path with over stock |
6422442 |
Link Issue between files within assy leads to "interrupt " Error |
6422579 |
The highlighted entities are different in formboard with Native NX and TC environment |
6422590 |
When remove connector with "Remove Part", NX cause error and can not remove it |
6422605 |
Part gets "modified" without modification when data has Datum Feature Symbol |
6422675 |
Runtime Error - R6025 pure virtual function call occur with Fluid Body |
6422686 |
Apply Fix Constraint option of Subdivide Segment does not show the simple solid |
6422699 |
During point definition, Method is changed unexpectedly by dragging mouse |
6422703 |
Stock Offset path is moved which has a constraint |
6422762 |
Transform Path & Remove Part does not work with Pre-selection (MB3) |
6422804 |
Force Save All breaks absolute matrix information |
6422818 |
A newer version of this component has been loaded |
6422863 |
Cannot Link a "multi-bodied" SHEET BODY even though all requirements are met (NX) |
6423040 |
Parents of a measurement in the "Dependencies" window disappears |
6423155 |
Internal error when opening a file in NX 7.5 - opens in NX 6 and NX 7 |
6423377 |
Some of connectors are not aligned to the base plan in formboard |
6423386 |
Element size in dialogue doesn't reflect Undo |
6423429 |
Formboard layout makes to change the orientation for some connectors |
6423441 |
Connector is tilted when Path has changed using "Orient Branch" |
6423450 |
NX crashed while editing copied spline from other component. |
6423461 |
Unable to infer offset direction from surface without [Create Interpart Link] |
6423488 |
Cannot select edges to redefine 2 lines Fitting Port |
6423532 |
Bend Radius cannot be edited in [Stock Fold] of Rectangle Stock |
6423552 |
NX Crash during Fold creation for Rectangular Stock of Linear Path |
6423577 |
[Linked Composite Curve] with [Fix At Current Timestamp] OFF is not updated |
6423635 |
Internal error raised opening a partfile in Teamcenter only |
6423665 |
Internal memory error |
6423869 |
PS23.1.147 7 .5.1 face blend fails in NX 7.5.2 |
6423948 |
SDI Plot (lp r) of NX 6 on Windows 7 64-bit never reaches printer |
6424052 |
Error occurred when dragging pivot points of Radial Bend |
6424071 |
Internal error while adding Stock Transition |
6424110 |
DBALL and MASTER files are not removed after R-flex simulation |
6424135 |
MMC_OVERLAP_ CHECK_TIMING_debug.txt causes warning message in TC env |
6424137 |
Removing 2D mesh which created by "Face from Mesh" has performances issue |
6424142 |
Unable to open assembly file |
6424163 |
Unable to create Fold Stock after deleting assembly constraints |
6424178 |
Internal Error during edit spline path with Rectangle space reservation |
6424185 |
Unable to create path with "Canon not find NX object from Parasolid tag" |
6424190 |
In an assembly context, Error occurred when move a connector of Deformable part |
6424195 |
Internal Error in Updating Form Board |
6424449 |
General Relinker not Relinking Interpart Expressions |
6424689 |
Unable to add curves in an Internal Sketch with RegionBoundarCurves S.I. |
6424730 |
Weld object is not created with correct direction |
6424766 |
Cannot Zoom In_Out by MB2 scroll after completing an action by MB2 |
6424782 |
Create PMI dimension between WCS plane and solid body edge is causing IE |
6424814 |
Find PMI Associated Geometry on PMI Center Mark display result in all Views |
6424822 |
CenterMark referencing ThreadCircleSymbol will be retained in update |
6425052 |
Weld points renamed if origin moved |
6425341 |
Save from checkmate does not create preview image |
6425358 |
Error recovery failure while editing Component Array |
6425359 |
Folder Name created in Save As dialog is always displayed as "New Folder" |
6425434 |
Unable to edit [SB Bead] with error "A required parameter was not supplied" |
6425962 |
Cannot Zoom In_Out by MB2 scroll after execute Examine Geometry |
6425983 |
NX takes more time to select features from PNT for Feature Group |
6426033 |
Item and corrupted Dataset is created even save failed |
6426539 |
FASC transfer move changes tool vector if generated in operation |
6426624 |
Cannot export to STEP or IGES from Teamcenter using Single Sign-on |
6426740 |
Moving Ordinate dimension set mess-up the order |
6426746 |
Change view style to invisible circle center Mark associativity is missing |
6426765 |
Switch between Work part; Representations is not changed to Lightweight sometime |
6426807 |
Internal Error occurred at Sheet Metal Reform |
6427033 |
CSYS creating themselves, cannot be deleted |
6427190 |
Double-click previously loaded part doesn't provide Reopen option as like in V9 |
6427300 |
Component remains highlighted and will not update - HD3D Check-mate results |
6427327 |
Cannot select components to add to BOM after a component set has been hidden |
6427363 |
If sheetmetal has unbend feature, SB Gusset feature cannot be created |
6427401 |
Delete folder from reuse library and do part Save As is causing TC error |
6427415 |
Copy solid body from body view is causing an Internal Error |
6427442 |
Apply Area Fill in selected Point in Region cannot be created by Internal Error |
6427879 |
Publishing Fillet Weld into TcAE Does not work |
6427895 |
Publish of Sealer to TcAE does not work |
6428446 |
Errors when trying to edit solid body for fem |
6429024 |
Attempting a Swept feature fails with the error "Reference Coordinate System Unde |
6429402 |
Part files always open as modified that contain drawing with tabular notes |
6429618 |
Curve become auto selection candidate for Match Edge reference |
6430092 |
NX 7.5.1 Ship Design Section SOA Error |
6430678 |
MP: Turning Post is not using the Secondary Turret offset for a drill cycle |
6430684 |
Component Name for assembly constraints doesn't replace correctly |
6431310 |
NX 4 file hangs opening drafting in NX 7.5 |
6431377 |
Section View Foreground option raising update failure in 64-Bit Windows |
6431828 |
Simulation navigator "inactive" indicator appears to have a bug |
6432183 |
The bearing load vector gives an error |
6432260 |
New folder created by Save As does not show correct folder name |
6432405 |
Routing Mechanical: Run Navigator no longer cares about Reference ID's |
6432535 |
Circular event problem |
6432662 |
Spring "moment" spelled wrong...shows up as "momement" |
6433023 |
Thread milling; problem with engage and retract motion when using cutcom |
6433261 |
Sorting result columns doesn't sort numerically |
6433375 |
Customer defaults does not read environment variables with spaces in the path |
6433654 |
Align Datum to Dimension Leader |
6434284 |
Improper cast installation |
6434493 |
Edit VSWEEP losses start_end formulas (expressions) |
6435182 |
Setting the Global OFF in the Sheet Metal Preferences is not taking effect as ex |
6435482 |
Turning Teach Mode Operation shows error about not having required csys matrix |
6435603 |
TOOL PATH VERIFY- tool orientation is incorrect when in pocket |
6435704 |
The constraint is not active |
6435829 |
Unable to change tool in operation copied from another part |
6435835 |
Can not open part file, evcrvu.c: Unknown curve type |
6436090 |
Distance Measurement Feature is not updated correctly. Regression in NX 7.5.2HF1 |
6437679 |
Using ug_convert_part -mm not all non-cut and boundary data converted |
6437757 |
Wants to get CAST installed |
6437827 |
Promote body causes record does not exist error |
6438036 |
Boolean fails with tool and target do not form complete intersection |
6438404 |
Material density is overwriting to default when reparenting linked solid body |
6438552 |
Routing attributes not assigned to port when using Stock As Component |
6438664 |
Post-processing strains in NX 6 |
6438666 |
Replace causes non-associative body to swap position in part navigator |
6439274 |
Unable to open an assembly in NX 7.5 |
6439291 |
Output Request Element Temperatures for ABAQUS preferences gives wrong result |
6439322 |
ZLEVEL- Tool changes tool axis when verifying |
6439592 |
Blanking Stock |
6440005 |
Tab thickness defaults to Global Value |
6440078 |
MR: Posting to an XZC mill using a Right Angle Head |
6440230 |
Operation creating revolved solid when UGII_CAM_GC_USE_HYBRID is active |
6440260 |
Z-level profile tool path is missing areas of cut |
6440349 |
Replacement Assistant Mapping is Unreliable |
6440710 |
Custom symbol in JT is corrupted in ugtopv |
6440932 |
Same issue as PR 1813120 |
6440984 |
NC: Inconsistent "File -> Open" results: NX may or may not report Internal error |
6441453 |
Mirrored welding symbols does not show correctly |
6441536 |
Rough Turning Tool Path does not show correct cut time in ONT |
6441650 |
Custom Symbols in TC 8.3 have performance problem versus native NX 7.5.2 |
6442363 |
Get "Sketch Name Not Found" error when selecting base edge for Flange |
6443117 |
Mirror feature fails in NX 7.5.2 and works in NX 5.0.4-0.6 |
6444227 |
Cannot select solid body of work part to trim to another assembly component |
6445621 |
Replace Part for Part Family Member does not work on TCE |
6445625 |
Associative maximum distance measure incorrectly reports zero distance |
6446240 |
Unable to save top assy when placing parts from reuse library in 64bit |
6446449 |
Orient Branch does not work |
6446697 |
Moving a tool to another pocket will flag all operations for regeneration |
6446771 |
CAE Report fails if used multiple times after the first write report call |
6446861 |
NX takes a long time to switch from manufacturing to design |
6446869 |
Changing cut com register number forces user to generate operations |
6448237 |
Turning Teach Mode op Maximum Spindle RPM not output in Standard CLSF output |
6448404 |
'Internal error: memory access violation' - 2D map mesh |
6448433 |
&VWDEP grip call fails in NX 7.5.2 with Internal Error |
6448589 |
ui_comp on_ok on_apply not evaluated when modifying |
6448973 |
Cannot extra ct the curve from edge |
6449021 |
NXOpen > Body > GetFaces method is VERY Slow in NX 7.5 |
6449610 |
Floorplane got broken link and not associate to model in an assembly |
6449977 |
Problems with assembly fems and groups |
6450194 |
The component with spline path does not move |
6450815 |
Out of date information is not set properly to Frozen Parts |
6450960 |
No valid MKE license error message when starting MKE after installing NX 7.5.1 |
6450971 |
Internal error opening nx assembly with component no read access_DUP of 6440984 |
6450990 |
Copy operation from one prt to another & change tool but got a new oper. created |
6451197 |
MaxAllowedWorkRevs is not working in NX 7.5.2.5 |
6451204 |
One working revision for item types, nx manager displays the wrong error |
64=1364 |
MW: Inserting ejector pin reports: "Part is not currently loaded" |
6451389 |
Analysis -> Measure Distance causes tool display to disappear when editing tool |
6451854 |
NXOpen.UF.UF Session.UI.PointSubfunction causes error 3520002 |
6451865 |
Cannot Publish Clinch weld data to Teamcenter |
6452386 |
Copy operation from part to part does not work correctly |
6452650 |
Mold Slide assembly is not updating as expected |
6452667 |
Tool axis changes when verifying toolpath |
6453274 |
Tool axis flips 90 degrees on NCM |
6453529 |
Tool axis is being reset to a random orientation when copying operation |
6453599 |
Unnecessary message is appeared when Information of Stock Browser is used |
6453818 |
Replace Component, Properties -> old part name as the new component name |
6453883 |
Getting an invalid tag trying to save as |
6453929 |
Increase the default height of the "Create Interpart Reference" dialog |
6455385 |
Internal memory access with error code 580039 |
6455439 |
De-selecting a Turning Teachmode Linear_Move Sub Operation Curve |
6455930 |
Unable to use new routing stock in NX 7.5.2 |
6455955 |
Quick trim on this arc produces Internal Error |
6456228 |
Part File created in NX 6.0.4 can't be opened on NX 7.5.2 |
6456257 |
The characters in the menu are garbled |
6456278 |
An error massage is appeared when edit diameter of Space Reservation |
6456750 |
MP Attempting to change the WCS while in the MW BOM, Component is changed to Top |
6456784 |
Broken view can't be select to ed= it view boundary |
6456851 |
It is not possible to project a point to a view in Drafting |
6457150 |
Label parameter no longer works for %ui_comp_vector blocks |
6457549 |
Cannot update Family Members |
6457793 |
Bitmap information is not displayed in PTS |
6458193 |
Allow free mapped mesh not working for a parallelogram |
6459319 |
ugmanager_import uses existing BOM structure |
6459774 |
Info alert - should not show when sequence has gaps |
6459781 |
Unexpected Info Alert With Embedded Feature Group |
6459785 |
Timestamp reorder error should ref parent not feature group |
6459789 |
Unexpected behavior when dragging features into and embedded feature group |
6460046 |
Information alert showing on sequential features |
6460176 |
Lost Children on Make Current Feature |
6460195 |
Replace Feature Breaks Linked Composite Curve |
6460435 |
Fit to view does not center subassembly |
6460463 |
Internal Error While Using Replacement Assistant Through Synch Links |
6460745 |
Performance issue loading features in Feature Browser |
6461072 |
Sorting of Out-of-date features is not maintained in Synchronize Links |
6461091 |
Unexpected Reason in Synch Links - Single Segment Composite Curve |
6461224 |
Failure to Execute Synchronize Linked Features within Synch Links |
6461891 |
JA function Features.ConvertToSequentialFeatureGroups causes unexpected reorder |
6461938 |
MB3 browse not available on non-history points and curves |
6462281 |
Opening empty MENCMachining operation from NX now results in error |
6463014 |
Opening Error - related to PR 6439274 |
6463203 |
Can't import expression file |
6463305 |
&VWDEP grip call fails in NX 7.5.2 with Internal Error |
6465234 |
Cannot import correctly CSV file when the spot matrix is in specific direction |
6465378 |
Replaced component is replaced in two assemblies with no warning |
6466179 |
Cut angle vector must not be parallel to tool axis error |
6466738 |
Feature Browser not showing timestamp view of datum plane |
6467081 |
Memory Access Violation opening .sim model |
6468490 |
Linked points not working correctly using PTS |
6468628 |
Using Identify get popup Attempt to free already free memory in Storage Manager |
6469382 |
NX Visual Issues fails with "Cannot Access Server" error |
6469887 |
Heal Path retaining prior extension lengths |
6469888 |
Heal Path does not follow segment of Start Point |
6469950 |
Internal Error converting Mating conditions |
6470793 |
Pure virtual function call error |
6470850 |
Failed to import .afu data when importing Dataset 58 .unv file |
6471907 |
Edit Stock does not update display |
6472032 |
Center marks become retained after updating view |
6472103 |
Split Body edit delete parent does not provide delete notification |
6472131 |
Import a deck, run SOL 111, create XY graphs, runs out of memory |
6472316 |
Internal error importing assembly which has a comp with no write access in db |
6473827 |
No Delete warning for Overstock |
6474000 |
Converting file creates a large spike in harness |
6474087 |
Parting tools no longer available "memory access violation errors" |
6474159 |
Routing Ports NOT ALWAYS Showing |
6474210 |
Overstock not remembering changes to number of pieces |
6474273 |
Psuedo Port not removed |
6474315 |
Route B_Curve changing lengths after conversion |
6475558 |
An unexpected stub reference error when loading assembly structure only |
6475799 |
NX 7.5 - RAPID statement removed from clsf in Point to Point Break Chip cycle |
6475802 |
FEDRATE_IPM statement added to CLS |
6475803 |
CLS listing adds a FEDRATE_1.100 statement in this release |
6475804 |
FEDRATE statement removed to CLS |
6476078 |
ugtopv fails in spot weld data including out-of-date geometry in latest baseline |
6477396 |
Mating conversion internal error |
6478919 |
Can not apply bend to space reservation pipe after patch |
6480230 |
Exporting groove tool with "User Defined" insert corrupts library file |
6480460 |
Show light weight loading does not update while in session |
6480523 |
Feedrate misapplied on retract motion for drilling operations |
6481873 |
NX 7.5 export JT - PMI basic dimension boxes off plane |
6481925 |
CAVITY MILL- warning -Cut angle vector must not be parallel to tool axis |
6481958 |
Memory Access Violation opening .sim |
6487092 |
NX 7.5.2MP2 - Check-Mate "ug_check_part.exe" - read_result option not working |