· How can I get the latest information on the NX plotting system?
· Why does NX 3 provide a new plotting system?
· Why does the new plotting system use commercial printing software provided by SDI?
· Can I still use the legacy plotting system?
· Plotting fails on windows with “Can not access plot server.”
· How can I use I-DEAS and NX on the same system?
· How can I setup NX software to work with PrintMaster software from SDI?
· Why aren’t my output files appearing?
· How can I get more debugging information?
· The pm_bps_executor.exe hangs on Windows. How do I fix this?
· How do I output in Gerber format?
· How do I set up a PCL-3 plotter?
· How has banner functionality changed in the new plotting system?
· How are colors and widths used in the new plotting system?
Features of the NX Plotting System
· What are key enhancements in the new plotting system introduced in NX 3?
· How can I convert legacy NX Open API programs for the new plotting system?
· How can I convert legacy NX Open GRIP programs for the new plotting system?
· How can I combine multiple plots in one plot file?
· How can I plot just an area of the screen?
· How can I save plot output to disk in the new system?
Printer Queues and Printer Groups
· Is there a way to automatically convert legacy plot queues for use with the new plotting system?
· In the new plotting system, how can I obtain the behaviors produced by legacy plot queue switches?
· Can all users at my site share the same printer definitions?
· What are some reasons for using multiple printer groups?
· How can I produce plot output in HP-GL/2 format?
· How can I set up a printer queue to work with Acrobat Distiller?
· Where are printer profiles saved to?
· How can I set up multiple system profiles for a plotter?
· Can I plot on Windows to a printer not defined on my local workstation?
· How can I eliminate the "jaggies" to make plotted lines appear smooth?
· Why is my HP printer so slow?
· Why are my lines so wide, my dashed lines solid or my lines so light?
· Why is my OCE plotter is cutting the paper incorrectly?
· Why is my custom sheet size clipping plots?
The latest information on the NX plotting system is available at the UGS Tech Support page (http://support.ugs.com). Search the UGSolutions Database for the exact phrase “NX Plotting System Information.”
A new NX plotting system was needed because legacy plotting functionality was outdated and inadequate. The legacy system was designed more than a decade ago, and it had not been updated to support newer printers or contemporary printing concepts or an easy-to-use graphical user interface. NX users had requested many enhancements that could not be effectively implemented in the context of the legacy plotting system.
It was essential to replace the legacy system with a new plotting system that provides modern printing features commonly available with other applications. The powerful features of the new system can significantly enhance the effectiveness and productivity of NX users.
The new plotting system is based on powerful commercial printing software developed by SDI (www.sdicgm.com), a UGS strategic partner. Basing the new system on commercial printing software provides NX users with capable, flexible, and up-to-date printing functionality.
SDI is in the business of and plotting, and also has extensive expertise in CGM (Computer Graphics Metafile), a graphics file format that NX produces for the new plotting system. Major NX customers already use SDI products, and SDI provides the printing/plotting capability in I-DEAS.
The UGS partnership with SDI means that NX customers can install other useful SDI products to obtain optional enhancements to printing and CGM functionality.
No. The new plotting system replaces the legacy plotting system. Legacy NX plotting functionality is not supported by NX 3 or later NX releases. You cannot use legacy plot queues with these releases.
If you run NX 2 or an earlier NX release concurrently with NX 3 or a later NX release, then two different plotting systems are in use. The earlier release uses the legacy plotting system, and the later release uses the new plotting system. The two plotting systems are independent and do not interact with one another.
On Windows the SDI software will use the registry variables in HKEY_LOCAL_MACHINE\Software\SDI if they exist. This will conflict with the settings that NX is trying to use. Delete or rename this registry hive and retry the operation.
Since you have already configured I-DEAS printing on your system, you can simply share the pm_server directory that contains your I-DEAS printer setup. All user profiles and system profiles will work for both NX and I-DEAS. In NX simply set UGII_SDI_SERVER_CFG_DIR to point to your I-DEAS pm_server directory, and the printers will be usable from both I-DEAS and NX. You will see both I-DEAS and NX jobs on the QUEUE page.
If you want to have multiple printer groups set up in NX, then you could have one printer group which pointed to your I-DEAS pm_server directory, and other printer groups set up with NX only plotters. In this case you would not see the I-DEAS jobs on the QUEUE page, because part of an NX printer group changes the HOME directory where these files are kept. In using a printer group you separated the NX HOME directory and the I-DEAS HOME directory.
In order to communicate with PrintMaster, you must create a file called “servers” and place this file in the $UGII_SDI_BASE/config/pm_submit directory (on Windows you will need to create the directory). This file should have a line like:
Name~hostname~6050
Where Name is the user displayed name that will appear on the SDI Print Submit dialog, hostname is the hostname of the machine running the PrintMaster server software, and 6050 is the listening port. Once this file is in place, you must either change UGII_SDI_SERVER_TYPE to WORKGROUP, or if you are using Printer Groups, modify your Printer Group list file and add a “SERVER” keyword.
The SDI software had a problem where the cleanup process would leave a lock file out of sync. This caused job retrieval to fail to process jobs. The most common symptom would be that you would plot to a TIFF or other image file, the job would seem to complete but no output file would appear. There are two ways to resolve this:
1. Turn off the job cleanup process. This is done from the Print Administrator on the BPS executor tab. Uncheck the Clean done jobs toggle. Doing this means that the jobs directories will build up and waste space, so if you do this, you must clean up the jobs directories manually.
2. Delete the file
print_submit\<nodename>\submitted_jobs
This should be done when no jobs are running on the system. This file is in the My_Documents folder on Windows and in the ~ directory on Unix.
This problem has been fixed by SDI and the code has been integrated into NX 3.0.4 and NX 4.0.1.
If you need to try and figure out why some jobs are failing, you can set the environment variable SDI_SERVER_CLEAN_DIR=0. Note that this must be set in the environment, you can not just enter this in the ugii_env.dat file. This will cause the SDI software to keep the temporary jobs files that get created in the jobs directory. The jobs directory is located in $UGII_TMP_DIR/bps, unless you are using printer groups. If you are using printer groups, then the jobs directory is whatever you entered under the JOBS_DIR keyword.
This process is used by SDI to create temporary files. Depending on the permissions at your site, these variables may not work to UNC drives. The symptom is that the process hangs, so the plot jobs never finish. In order to fix this, it is recommended that you change your environment so that these temporary files are created on a local drive:
If you are using Printer Groups, edit your printer_group_list_file.txt file and make sure your JOBS_DIR and HOME_DIR for all your printer groups point to a local disk directory, such as c:\temp.
If you are not using Printer Groups, set the environment variables UGII_SDI_OVERRIDE_HOME and UGII_SDI_BPS_JOBS_DIR to point to a local directory, such as c:\temp.
Gerber output is supported through an NX provided program gerber.exe (simply gerber on Unix). In order to set up Gerber output, you must first specify the directory that you want the output .grb files to go to. You do this by setting an environment variable, UGII_SDI_OUTPUT_DIR. All gerber output will be placed in this directory. Then startup the Print Administrator and add a new plotter. Give it a name, and select any model other than PDF. Select the option “Execute program on Input File”, and for the full executable enter gerber.exe (windows) or gerber (Unix).
The most recent plotting has limited support for PCL3
compatible devices. The first requirement is the following binaries:
win_band.dll
14.1.24
win_mft.dll
8.2.41
sdi_hppl.dll
3.1.1
These are available in NX 4.0.2, NX 3.0.5, NX 3.0.4
MP3, NX 3.0.3 MP8 and NX 3.0.2 MP13. To
add a PCL-3 model start the Printer Administrator
(File->Utilities->Printer Administration.
1. Select the
models tab, and then Add… at the bottom.
2. Name the model, you may want to use pcl3 in the name to remind you
what it is later.
3. Set Color to
Both and
4. Add a
resolution of 600 Both.
5. Add the paper
sizes needed for your printer.
6. Set the HPPL
Model to PCL3-GUI
7. Save the
model
Now that the model is created, you need to configure a
printer. Click Add to add a printer, and
then select the PCL-3 model that you just created in the model drop down list. Select the NT queue that is appropriate, and
then click on advanced options. In the
advanced options dialog enter:
For
Rendering:
+PCL3GUI +RGB
For Post
Processing
+RGB
The
plotter should now work using PCL-3.
In the new plotting system, plot banner functionality (appends an informative text block to plots) is enhanced to support additional content elements, including elements to display the full path of the part, the Team Center revision of the part, whether the drawing sheet is out of date, etc.
Plot banner functionality is also enhanced to permit the location of the banner text block to be defined relative to the bounds of the plot, so it is no longer necessary to specify the location in absolute plot coordinates. For example, the banner location might be specified relative to the lower-right corner of the plot.
In addition, for printers that use RTL printer models, you can set header and trailer options to display an alternate form of banner. If enabled, the header is printed on the leading edge of the output, and the trailer is printed on the trailing edge of the output. The content of the header and trailer are the same: date and time, user account name, CGM file name, SDI job number (a number referenced on the Queue page of the NX Print dialog), and an optional text message that you are prompted to enter when you click Print.
· You can enable headers or trailers for individual plot jobs on an RTL printer. Click Advanced Settings on the Print Setup tab of the NX Print dialog. When the Advanced Settings dialog is displayed turn on Headers or Trailers as desired.
· You can enable headers or trailers by default for all plot jobs printed on an RTL printer. Select the printer on the Printers tab of the Printer Administrator dialog, and click System Profile. When the System Profile dialog is displayed, click Advanced Settings on the Printer Setup tab. When the Advanced Settings dialog is displayed turn on Headers or Trailers as desired.
The new plotting system supports easy specification of colors for plotting, including use of as-displayed (WYSIWYG) colors, part colors, custom color palettes, and black-on-white. All 216 object colors can be used. Custom color palettes are easy to create and edit, and can be readily stored and shared via color definition files (CDFs).
The new plotting system also supports easy specification of widths for plotting, including use of standard widths, an arbitrary single width, custom widths assigned according to object width index, and custom widths assigned according to object color index. Custom widths are easy to create and edit, and can be readily stored and shared via width definition files (WDFs).
Color customizations are independent of width customizations, and can be used in mix and match fashion. You can save custom color and width settings with an individual drawing sheet, so the same colors and widths can be used each time you plot the sheet.
· The new system uses standard plot file formats (CGM and TIFF) that are supported by a wide variety of commercial applications, so the new plotting system can be readily extended and integrated with other customer processes.
· All aspects of the new plotting system are controlled by intuitive, easy to use graphical user interfaces.
· It is much easier to control printer settings than in the legacy system. Many settings can be easily set by an NX user in the NX Print dialog instead of by a system administrator in a plot queue definition.
· It is much easier to define printer queues. An ordinary user can readily define printers and profiles for the plotter devices and plotting tasks that are most important to him. Easy printer definition means greater productivity for both end users and system administrators.
· The new system permits system administrators and ordinary users to define "profiles" to encapsulate commonly used printer option settings (scale, portrait/landscape, color/monochrome) for fast and easy preparation of plot jobs.
· CGM files produced for plotting support a generous variety of color and width settings. It is much easier to set color and width attributes than in the legacy system.
· The NX Print dialog displays a preview of the plot layout on paper, and also provides a CGM Viewer function that displays the contents of the CGM file to be printed. The CGM Viewer function can also be used to select a rectangular subregion of the plot for printing.
· The new system permits the user to save print-ready CGM files on disk that can be directed to any plotter at a later time without starting NX or loading a part.
· The new system permits the user to convert wireframe CGM output to raster images (e.g. JPEG) of arbitrary resolution.
· The new system provides an easy-to-use visual interface for arranging plots on a layout.
· The new system provides effective user interfaces for operating on multiple drawing sheets at once, both for plotting and CGM export.
· The new system provides powerful programmability, and the nxplot command-line program provides some programming options even to customers without GRIP and UFUN licenses.
· The new plotting system supports plotting of raster image annotations on drawing sheets.
An extensive collection of NX Open API functions provides comprehensive access to NX plotting functionality introduced in NX 3.
For an example of how to plot all drawing sheets in the current part, refer to sample program ufd_plot_drawings.c in the NX Open kit.
For an example of how to create HP-GL/2 output files for all drawing sheets in the current part, perhaps for purposes of comparing plots in HP-GL/2 format, refer to sample program ufd_plot_drawings_hpgl.c and script move_hpgl.pl in the NX Open kit.
· Command-line program nxplot provides programmatic access to some plotting functionality without using an NX Open license. You can automate common plotting tasks by implementing scripts or programs that invoke nxplot.
Beginning with NX 3, GRIP plotting statements are redefined to utilize the many features of the new plotting system. Plotting statements PLOT, PLTSAV, PLTSUB, and PLTDEL have new parameters and new behaviors. Also, statement PLTUPD and plotting-related parameters of statement DRAWV are now obsolete and have no effect.
If you have legacy GRIP plotting programs written for releases before NX 3, you can modify them to use the redefined statements with their new parameters. If you do not modify or recompile your legacy GRIP plotting programs, you can continue to use them with the new plotting system, provided you create a mapping file that maps legacy statement parameters to values that are meaningful in the new system.
· Only limited features of the new plotting system are available with this mapping technique. To fully exploit the capabilities of the new system, you must modify GRIP plotting programs to use the updated statement parameters.
You can find instructions for using the mapping technique in a sample mapping file provided with NX. The sample file is ${UGII_BASE_DIR}/nxplot/sample_plotter_mapping.txt.
The new plotting system provides Plot Layout functionality for arranging multiple plots in one plot file for printing or for saving to disk in CGM format. This functionality permits you to layout multiple plots for efficient printing on roll-feed paper, or to overlay plot jobs so they are printed on top of one another, or to collect plots in a single file for publishing.
Plot Layout functionality includes an intuitive, easy to use, graphical user interface that permits you to see the current arrangement of plots and to manipulate each new plot as it is added to the layout. Optionally, the functionality can compute a default, initial location for each new plot in a manner designed to conserve roll-feed media.
You can add any number of plots to the plot layout over the course of the session, but you can still plot individual jobs at any time without disturbing the contents of the layout.
To add a plot to the plot layout, click Add to Plot Layout in the File-->Plot dialog.
Although NX does not allow selecting an area to plot, the SDI software does. Generate your plot normally. When you get to the SDI NX Print dialog, bring up the CGM viewer. On the CGM Viewer, right mouse button will bring up a context menu that allows you to select a viewport. Select the viewport, and then cancel the CGM Viewer. When you then plot, only the viewport area will plot.
The NX plotting system supports various strategies for saving plot files on disk. Choosing an approach depends on how you intend to use the files.
You can save plot files on disk in printer-independent CGM format by selecting Save CGM File in the File-->Plot dialog. You can later use the NX Print dialog to print the saved CGM files on any printer, or you can use various applications to import or otherwise process the files. For example, Microsoft Office applications support importing of CGM files. Note that you can view any CGM file with the CGM Viewer function of the NX Print dialog, but you can also install a CGM viewer application or browser plug-in so that you can easily view the CGM files you save on disk.
You also can save plot files on disk in the printer output format (e.g. RTL, PostScript, HP-GL/2). If you save a plot output file on disk only occasionally, then use the Output Options setting in the NX Print dialog.
1. In the File-->Plot dialog, click Plot to display the NX Print dialog.
2. Choose a printer and then set Output Options to Print to File or "Print to File and Printer".
3. When you click Print, the system prompts you to specify a path for the plot output file.
If you routinely save plot output files as part of some defined process, then you might prefer to invoke the process automatically whenever a plot output file is produced. To accomplish this, you can use the Printer Administrator dialog to set the Render File then Execute Program option for your printer.
1. Select File-->Utilities-->Printer Administration.
2. Specify the printer group for the printer of interest.
3. When you click OK, the Printer Administrator dialog displays. In the Printer Administrator dialog, select your printer.
4. Click Setup.
5. Turn on the Render File then Execute Program option.
6. Enter the full path of a command (including switches) to invoke your process. After SDI software generates each plot output file, it automatically invokes your command, specifying the plot file name as the last parameter. In a simple case, your command might simply copy the plot output file to a particular directory. On windows an example would be:
copy %1 d:\printer_group\in\*.*
A more elaborate example, which looks for the cgm filename, so it can preserve the jobname on the output file would be:
for /F %%K in ('dir /b *.cgm') do set FILENAME=%%~nK
copy %1 C:\TEMP\plots\%FILENAME%.hpp
Note, this example works around a problem in NX 3 and NX 3.0.1
in which the output filename does not carry the jobname
as entered by the user. This problem is
scheduled to be fixed in NX 3.0.2. Note
that in 3.0.1 you can set an environment variable SDI_FORCE_OPNAME=1 which will
cause the SDI software to preserve the jobname on the
output file.
You can also generally retain plot output files so you can later access them on disk. In the Printer Administrator dialog, click the BPS Settings tab, and turn on the Save Input/Output Files option. The setting affects all plot jobs printed on all printers in the printer group.
You can find retained files under the "jobs" directory. (Search for UGII_SDI_BPS_JOBS_DIR in the ugii_env file.) By default, the jobs directory is ${UGII_TMP_DIR}/bps, and you can find all files for a particular plot job in one of the subdirectories of ${UGII_TMP_DIR}/bps/user_name/node_name, , where user_name represents the user account name, and node_name represents the system node name.
Retained input/output files can consume large amounts of disk space, so delete the files promptly when they are no longer needed.
No. You must manually define new printers for the new plotting system, but defining a printer in the new system is generally easier than defining a queue in the legacy system. The process of defining a printer is similar to using the Add Printer function on Windows systems. It can be as simple as entering a name for the printer, and then using the mouse to choose the operating system print queue from one list and the printer model from another list.
You might define fewer printers for the new plotting system because the new system permits you to directly control more options than did the legacy system. For example, some options controlled by plot queue switches in the legacy system (switches /AS (auto-scale), /D (DPI), /SP (set palette), etc.) can be conveniently controlled by the NX user in the new system. Therefore, you might prefer not to define extra printers to handle the various option choices.
· Printer definitions are platform-specific, so if you use both Windows and UNIX workstations, you will create a printer group with printer definitions for Windows and a printer group with printer definitions for UNIX.
Use File-->Utilities-->Printer Administration to define printers.
In the legacy plotting system, you set plotting options by
specifying switches (codes) in plot queue definitions. The new plotting system
supports comparable features, but you enable the features in other ways. For
some common legacy plot queue switches, the following table indicates how to
produce comparable results in the new plotting system.
/2
(HP-GL/2 switch) |
When using the Printer Administrator dialog to create the printer, choose an HP-GL/2 printer model. (See also "How can I produce plot output in HP-GL/2 format?") |
||||||||||||||||||
/AR (Auto-run switch) |
You need not perform any steps to obtain this behavior. The new plotting system automatically processes all ready plot jobs. |
||||||||||||||||||
/AS (Auto-scaling switch) |
In the new plotting system, you can obtain auto-scaling behavior by enabling the Best Fit to Page option as follows. · You can enable Best Fit to Page for an individual plot job, or you can save the setting in a user profile. Set the Scaling option to Best Fit to Page on the Print Layout tab of the NX Print dialog. Click Save Profile As in the NX Print dialog to save the setting in a user profile. · You can enable Best Fit to Page as the default scaling setting for a printer. Select the printer on the Printers tab of the Printer Administrator dialog, and click System Profile. When the System Profile dialog is displayed, click the Print Layout tab, and turn on Best Fit to Page. |
||||||||||||||||||
/DJ (DesignJet switch) /LJ (LaserJet switch) |
When using the Printer Administrator dialog to create the printer, choose the appropriate DesignJet or LaserJet model from the list of printer models. |
||||||||||||||||||
/D (DPI or dots-per-inch switch) |
In the new plotting system, you can set the DPI or resolution as follows. · You can choose the resolution for an individual plot job, or you can save the resolution in a user profile. Set the Resolution option to the desired value on the Print Setup tab of the NX Print dialog. Click Save Profile As in the NX Print dialog to save the setting in a user profile. · You can set the default resolution for a printer. Select the printer on the Printers tab of the Printer Administrator dialog, and click System Profile. When the System Profile dialog is displayed, choose the default resolution on the Print Setup tab. · You can set the resolutions supported by a custom printer model. Select a custom printer model on the Models tab of the Printer Administrator dialog, and click Properties. When the Properties - Printer Model dialog is displayed, use the Resolutions option to customize resolutions supported by the printer model. Note that you cannot modify the properties of a predefined printer model. First use Save As to save a custom copy of a predefined printer model, and then modify the properties of the custom copy. |
||||||||||||||||||
/MO (Monochrome switch) |
In the new plotting system, you can enable monochrome output in the following ways. · You can enable monochrome output for individual plot jobs. In the File-->Plot dialog, set the Colors option to Black on White, or instead, set the Colors option to Monochrome on the Print Setup tab of the NX Print dialog. Click Save Profile As in the NX Print dialog to save the NX Print Monochrome setting in a user profile. · You can choose monochrome as the default color setting for a printer. Select the printer on the Printers tab of the Printer Administrator dialog, and click System Profile. When the System Profile dialog is displayed, set the Colors option to Monochrome on the Print Setup tab. · You can specify whether a printer model supports color or monochrome output. Select a custom printer model on the Models tab of the Printer Administrator dialog, and click Properties. When the Properties - Printer Model dialog is displayed, set the Colors option to Color, Monochrome, or Both. Note that you cannot modify the properties of a predefined printer model. First use Save As to save a custom copy of a predefined printer model, and then modify the properties of the custom copy. |
||||||||||||||||||
/SP (Set palette switch) |
In the new plotting system, you can set the Colors and Widths options in the File-->Plot dialog to reproduce the behavior of any of the many possible settings of the legacy /SP switch. You can set the Colors option to any of the following
values.
You can set the Widths option to any of the following values.
|
||||||||||||||||||
/11 /14 /17 /A3 /A4 (Tray
selection switches) /PG (Page size switch) |
In the new plotting system, you can select a paper tray or size by using an initialization file containing tray selection or paper size commands that are inserted at the beginning of each output file dispatched to the printer. When you define a printer, you can specify an initialization file to be used for all jobs printed on this printer. 1. On the Printers tab of the Printer Administration dialog, select the printer of interest. 2. Click Setup. 3. When the Printer Setup dialog displays, enter the path of an initialization file in the Initialization File entry field or click the Browse button to search for the file. When you define a paper size for a custom printer model, you can specify an initialization file to be used for all jobs printed on paper of this size by all printers that share the custom printer model. Use this second approach if you wish to define a printer that supports printing to multiple paper trays. 1. On the Models tab of the Printer Administration dialog, select the custom model of interest. 2. Click Properties. 3. When the Properties - Printer Model Dialog displays, select the paper size of interest. 4. Click Edit Paper Size. 5. When the Paper Size Properties dialog displays, enter the path of an initialization file in the Initialization File entry field, or click the Browse button to search for the file. |
Yes. Printer definitions are stored in a directory called a printer group directory, and any NX user who can access the directory (i.e. who has "read permissions" for the directory) can use the printers in the printer group.
· Printer definitions are platform-specific, so if both Windows and UNIX workstations are used at the site, you must create a printer group with printer definitions for Windows and a printer group with printer definitions for UNIX.
Also, any printer devices or files specified by printer definitions must be visible to the operating system of each user workstation. When defining a printer for Windows, for example, the printer must have been added on each user workstation (via Add Printer), or you can use the LPR/Queue option or device option to identify the printer in Uniform Naming Convention (UNC) format: \\server_name\share_name to permit access by all user nodes. To use the LPR option requires that optional software be installed on your system to support the LPR command, then on the Printers tab of the Printer Administration dialog, select the printer of interest, and click Setup. When the Printer Setup dialog is displayed, set the Printer option to LPR/Queue and enter the UNC name of the printer. If the remote queue is on a Windows server, then you can use the device option. To use the device option on the Printers tab of the Print Administration dialog, select the printer of interest, and click Setup. When the Printer Setup dialog is displayed, set the Printer option to Device and enter the UNC name of the printer.
If all users at the site share only a single printer group per UNIX or Windows platform, then the system administrator sets environment variable UGII_SDI_SERVER_CFG_DIR in the ugii_env file to identify the printer group directory.
Users also can share multiple printer groups per platform. In this case, the system administrator enumerates the printer groups in a printer group list file, and he sets a customer default to identify this file.
You can create multiple printer groups as a strategy for organizing printers, so that an individual printer group might represent just the printers at a particular location or just the printers belonging to a particular department or work group. This provides the following benefits:
· When you invoke the File-->Plot dialog to prepare a plot job, it is easy to choose the appropriate printer group by its descriptive name, and the NX Print dialog lists only the printers in this printer group. This approach can make it easier for you to select the printers you use most often, because printer lists are uncluttered by printers you rarely use.
· Use of multiple printer groups means that printer definition can be a distributed responsibility. The system administrator might create a printer group to represent printers that are shared by all users at the site. Others might create printer groups for printers used only by users in a particular workgroup at a particular location. An individual NX user might create a printer group to manage printers and printing options that he uses most often.
· Because it is easy to define printers in the NX plotting system, each individual NX user can readily define printers for his particular printing needs in his own printer group. (Defining a printer is similar to using Add Printer on Windows.)
To use multiple printer groups:
1. List the printer groups of interest in a printer group list file.
2. Set a customer default to identify the file. NX reads the printer group list file to display an option menu of printer groups in the File-->Plot dialog and other plotting dialogs.
3. Specify a special entry in a printer group list file to automatically include the contents of some other printer group list file, so an individual user can create a file that includes the contents of the printer group list file defined by a system administrator for the site or workgroup.
A template version of the printer group list file is provided with NX. The template file contains instructions and samples to explain file syntax. When creating a printer group list file, you can copy this template file and add your printer group information to the copied file. The template file is ${UGII_BASE_DIR}/nxplot/printer_group_list_file.txt.
To produce plot output in HP-GL/2 format, plot the job on a printer defined to use an HP-GL/2 printer model.
First you must define a printer that uses an HP-GL/2 printer model. By default, the SDI plotting software integrated with NX uses RTL (HP Raster Transfer Language, a subset of HP PCL) for many printer models. To produce HP-GL/2 output, you can choose an existing printer model that uses HP-GL/2, or you can create a new printer model that uses HP-GL/2. In either case, use the Printer Administrator dialog to define printers and printer models.
1. Select File-->Utilities-->Printer Administration.
2. Specify the printer group for the new printer.
3. When you click OK, the Printer Administrator dialog displays.
4. To use an existing printer model, add a new printer and choose printer model "GEN:Generic HPGL/2". Or, if you have an actual printer device in mind (e.g. HP DesignJet), then you can create a HP-GL/2 model for this printer by copying an existing model. Follow these steps to create the model.
1. In the Printer Administrator dialog, click the Models tab and select the model of interest.
2. Click Save As, and specify a unique name for your new model, possibly including some reference to HP-GL/2.
3. Then click Properties, set the Class to "HPGL/2", and click OK.
4. Then return to the Printers tab and add a new printer using your new model.
5. After you add the new printer on the Printers tab, click System Profile and specify default options for the new printer.
6. Click Cancel or Close to dismiss the Printer Administrator program. You will be able use your new printer the next time you invoke File-->Plot.
If you wish to save HP-GL/2 plot output files on disk, see question "How can I save plot files on disk?"
An
integrated PDF export capability is available within NX-3 plotting. This feature is licensed separately by SDI
who can be contacted at sales@sdicgm.com.
If
you want to work with acrobat distiller, you must create a new printer model
that has the sheet sizes that you need, and specifies postscript initialization
files for those sheets. The postscript
initialization files will be what tell Distiller the size of the output PDF
file that is needed. Here are the
specific steps to follow:
1. In the Printer Administration tool create a new plotter model. Do this by going to the model tab and selecting HP:HP Postscript Multi-Bin Generic, and then save as to a new model name.
2. Edit your new model by selecting it and pressing properties.
3. Add/Delete paper sizes as required. The paper sizes should all be specific sized sheets.
4. Delete the 600 resolution and add a single 3200 resolution.
5. For each paper size, select it and the edit paper size.
6. Change the printable width and height to match the width and height.
7. Add an initialization file for each sheet. The initialization file is what is going to tell Distiller the size of the postscript file it is receiving. You will want a separate one for each sheet that you set up. The postscript file will be 72 dots per inch. There are ps initialization files ps*_init in the printer group directory for a3, a4, A and B size sheets. You will want to create initialization for any other sheet sizes that you need. The important thing is to add an initialization file for each sheet. In the initialization file field you want to specify the simple name of the initialization file. The software will then find the file in the printer group directory. That way the printer would not depend on a path, e.g. specify “ps_letter_init” and not “d:\printer_group\group1\ps_letter_init”.
8. Once the model is set up, then add a plotter that uses this model. You can either print directly to the virtual queue set up by Distiller, or you can set it up as a “render file and execute program” plotter, and then set it up to execute a script that copies the file to the distiller watched input directory. The first argument to this script will be the filename of the postscript output file. The script can be as simple as:
copy %1 d:\distiller\in\*.*
You may want to set the default system profile to landscape, as that is how the sheets come out.
Users can now plot.
They will have to select the right sheet size for their drawing, in order for
the right initialization file to be used.
Plotter profiles are tied to a
particular user. If you are not using Printer Groups, and are just
specifying your printers using UGII_SDI_SERVER_CFG_DIR, then the profiles will
be located in the file:
c:\Documents and Settings\<user
name>\My Documents\print_submit\<nodename>\userprofiles (Windows)
~/.print_submit/<nodename>/userprofiles (unix)
If you are using Printer Groups,
then the profiles are saved under the HOME_DIR specified in the Printer
Group List file. The file will be:
$HOME_DIR\print_submit\<nodename>\userprofiles
First set up and test the profiles
for an individual user. Once you are
happy with the profiles, copy the userprofiles file
from the users directory to a temporary location that is easy to access. See Where are printer profiles saved
to? to locate the
file. Now go into your Printer
Group directory, which contains the definitions for your plotters. Make a backup copy of defaultprofiles. Then edit defaultprofiles,
and read in your saved userprofiles file. Copy the profiles for each printer to follow
directly after the <System Profile> for that particular printer. Delete the text “Basic Plotting System~0~”
from the user profiles that you are putting into the system profiles. You should be able to tell that the new
profiles match the <System Profile> for the plotter. Save this file, and
all users should now be able to access the multiple system profiles per user.
Yes, you can set up to plot to a device not setup on your local workstations, as long as you have TCP/IP installed on the system. You can use the remote printing support that is built into TCP/IP. When you set up your printer in the Print Administrator, on the Print Setup page, select LPR Queue for the printer. In the LPR queue name field, enter in the name of the remote system and the printer queue on that system in UNC format. Use quotes around the name, e.g. “\\hostname\printer name”.
The problem of "jaggies", also known as aliasing, occurs when diagonal lines are rasterized for output on raster printers and plotters. In the rasterization process, a line is rendered using a pattern of dots. The print resolution or dots-per-inch (DPI) setting determines the number and size of dots in the pattern. If the resolution is low, the pattern contains fewer dots and larger dots, so jaggies can result, and the line does not appear smooth.
To address jaggies, you can increase the Resolution setting specified on the Print Setup tab of the NX Print dialog. You can specify resolution for RTL and PostScript printers you have defined, and you can save the preferred resolution in the system profile for the printer or in a user profile. You cannot specify resolution for HP-GL/2 printers, because the printer itself controls the resolution.
Note that increasing the resolution can increase printing time. Also, for RTL printers, it can significantly increase the size of plot files delivered to the printer.
Supported resolutions depend on the capabilities of the printer device, and also on the printer model definition managed by the Printer Administrator dialog. In some cases, different resolutions are supported for color and monochrome output.
If you set the Color option to Grayscale in the NX Print dialog, then patterns of black dots are used to represent the various shades of gray. For lighter shades, the pattern of dots is sparse, and curves and dashes can appear irregular or broken where no dots are printed.
You can use any of the following strategies to improve the appearance of curves on plotted output.
· Avoid using Grayscale. You can set the Colors option to Monochrome on the Print Setup tab of the NX Print dialog, or you can set the Colors option to Black on White in the File->Plot dialog.
· Use Grayscale, but increase the Resolution setting specified on the Print Setup tab of the NX Print dialog. (Note that you cannot specify the resolution for HP-GL/2 printers.)
· Use Grayscale, but set the Widths option to Custom 3 Widths in the File->Plot dialog, and increase each of the line width values in the Custom Widths dialog.
When you increase resolution or line widths for Grayscale output, the system uses more dots for each curve, giving the curve a more regular appearance.
Many of the HP printer models are set up by default to use RTL which has a default output setting of High Quality. While this generates the best plot, the speed of the output is very slow. There are two choices for a solution. You can switch your output to a HPGL-2 format if the plotter supports it (most will support it). In this case, just select the Generic HPGL-2 model. The second option is to bring up the Print Administrator and go to the Setup page for the printer queue, and then select advanced options. Enter in either +QDRAFT or +FAST755 as the rendering option for the printer. +FAST755 should only be used when you will only be plotting line drawings. Using +FAST755 for Solid fill drawings (like raster images or High Quality Visualization) will cause the ink flow to exceed what the print head is capable of. Using a sample C size drawing the performance was:
RTL by default 11 minutes 13 seconds
+QDRAFT 4 minutes 35 seconds
+FAST755 1 minute 33 seconds
When NX creates a CGM file for plotting, it creates it at full scale. The line width that was specified (using customer defaults or custom widths) are applied to the lines in the CGM file. Similarly the dash size and space size specified in customer defaults for Visualization are used to generate dashed lines (like phantom lines and center lines). If the full scale of your model is small, and you scale it up to print on a sheet, then you will find that the lines become wider (if you double the size, a .01 line width becomes .02, etc.). Similarly your dash lengths will also increase in size. This is what leads to extra wide lines.
Conversely if your full scale is very large, you will be scaling it down to print on a sheet. In this case lines become thinner (if the scale it by ½, the .01 line becomes .005, etc), and your dashed lines become shorter. When the dashes in a line become very short, the spaces also become very short, and the line will appear to be solid on your output.
There are some possible solutions to these problems:
The OCE plotter is sometimes mistaken as an HP 3500 model. You can correct this by changing the HPPL parameter on the plotter model to HP650C.
Calculating the printable area for a custom sheet is complicated. The best way to show how to do this is to run through an example. Suppose we have a cut sheet that is slightly larger than an A3 size drawing (331 x 480 MM). We know the plotter can print out an A3 drawing on this paper (297x421). What are the printable width and height we should use? Here are the calculations. Start with 298 x 421 as the target page size to give us 1mm extra:
298 x
421mm
(target page size)
11.73228
x 16.5748 (convert mm to inches by dividing by 25.4)
1.466535
x 2.07185 (inches
divided by 8)
439.9606
x 621.5551 (above figures multiplied by resolution
(300) provide scanwidth)
54.99508
x 77.69439 (scanwidth divided
by 8)
Because of
the rounding issues related to the rendering of data to this page size, round
the ending numbers up and work back to the following starting point:
55 x
78
(rounded scanwidth divided by 8)
440 x
624
(multiply by 8 to get scanwidth)
1.4666
x 2.08 (divide by 300 to
get scanwidth divided by resolution)
11.7333
x 16.64 (multiply by 8 to get
page size in inches)
298.0267
x 422.656 (multiply by 25.4 to get closest match
to target page size in mm)