Solid Edge Revision Manager Object Library
DisplayAlerts Property
Description
Enables or disables the display of alerts and messages.
Property type
Read-write property
Syntax
Visual Basic
Public Property DisplayAlerts As Long
Example
Imports RevisionManager
Imports System.Runtime.InteropServices

Module Example

    Sub Main()
        Dim objApplication As RevisionManager.Application = Nothing

        Try
            ' Start Revision Manager.
            objApplication = New RevisionManager.Application
            objApplication.DisplayAlerts = False
        Catch ex As Exception
            ' Write any errors to console.
            Console.WriteLine(ex.Message)
        Finally
            ' Release COM Objects.
            If Not (objApplication Is Nothing) Then
                objApplication.Quit()
                Marshal.ReleaseComObject(objApplication)
                objApplication = Nothing
            End If
        End Try
    End Sub

End Module
See Also

Application Object  | Application Members

Send comments on this topic.