| Solid Edge Revision Manager Object Library > Application Object : GetGlobalParameter Method |
| Visual Basic |
|---|
Public Function GetGlobalParameter( _ ByVal Parameter As ApplicationGlobalConstants, _ ByRef Value As Variant _ ) As Long |
| Value | Description |
|---|---|
| seApplicationGlobalAdminFileLocation | |
| seApplicationGlobalApplyStatusToLinks | |
| seApplicationGlobalAvailableRootFolder | |
| seApplicationGlobalBaselinedRootFolder | |
| seApplicationGlobalCheckInOnClose | |
| seApplicationGlobalInReviewRootFolder | |
| seApplicationGlobalInsightCacheLocation | |
| seApplicationGlobalInsightFolderMappingFileLocation | |
| seApplicationGlobalInWorkRootFolder | |
| seApplicationGlobalLogFilesLocation | |
| seApplicationGlobalLookAheadVersion | |
| seApplicationGlobalMakeRevisionsObsolete | |
| seApplicationGlobalObsoleteRootFolder | |
| seApplicationGlobalOfflineMode | |
| seApplicationGlobalReleasedRootFolder | |
| seApplicationGlobalRevisionDelimiter | |
| seApplicationGlobalSearchScope | |
| seApplicationGlobalTeamcenterFormula | |
| seApplicationGlobalUpdateDraft | |
| seApplicationGlobalUploadOnClose |
Imports RevisionManager Imports System.Runtime.InteropServices Module Example Sub Main() Dim objApplication As RevisionManager.Application = Nothing Dim strLocalCacheLocation As String = Nothing Try ' Start Revision Manager. objApplication = New RevisionManager.Application objApplication.GetGlobalParameter(ApplicationGlobalConstants.seApplicationGlobalInsightCacheLocation, strLocalCacheLocation) Catch ex As Exception ' Write any errors to console. Console.WriteLine(ex.Message) Finally ' Release COM Objects. If Not (objApplication Is Nothing) Then objApplication.Quit() Marshal.ReleaseComObject(objApplication) objApplication = Nothing End If End Try End Sub End Module