|  Copy | This method makes a new copy (revision) of the document, updating the parent document. The document's status is set to igStatusAvailable. NewRevision and NewDocNum can be specified to set the project properties in the new document. The copy becomes the current document. This method returns a long value. | 
|  IsDocumentFOP | Given a file, this method determines whether it is an FOP or not. If yes, whether it is an FOP master or a member. | 
|  OpenInSEEditor |  | 
|  Rename | This method renames or moves a document and updates the links to a new location while preserving the current document status. This method returns a long value. | 
|  Replace | This method specifies a new file to replace the current file. The parent document is updated appropriately. This method returns a Long value. | 
|  Revise | This method revises the referenced Document object. | 
|  SaveAllLinks | This method saves all linked documents in the LinkedDocuments property of the current document. | 
|  SetPath | This method sets the full path of the referenced linked document object without changing the geometric version, thereby allowing files to be moved and stay up-to-date. |