| Solid Edge Revision Manager Object Library : IDocAuto Object |
Copy | This method makes a new copy (revision) of the document, updating the parent document. The document's status is set to igStatusAvailable. NewRevision and NewDocNum can be specified to set the project properties in the new document. The copy becomes the current document. This method returns a long value. |
IsDocumentFOP | |
OpenInSEEditor | |
Rename | This method renames or moves a document and updates the links to a new location while preserving the current document status. This method returns a long value. |
Replace | This method specifies a new file to replace the current file. The parent document is updated appropriately. This method returns a Long value. |
Revise | This method revises the referenced Document object. |
SaveAllLinks | This method saves all linked documents in the LinkedDocuments property of the current document. |
SetPath | This method sets the full path of the referenced linked document object without changing the geometric version, thereby allowing files to be moved and stay up-to-date. |
_FullName | |
AbsolutePath | This read-only property returns a string that contains the absolute path of the document. |
Application | The Application object in which the referenced object is active. |
DocNum | This property returns a string containing the Document number. |
FullName | Returns the name and path of the referenced object. |
LinkedDocuments | This read-only property returns the LinkedDocuments object for the referenced Document object. |
Occurrences | This read-only Long property returns the number of occurrences (subassemblies or parts) for the referenced Document object. |
Parent | Returns the parent object for the referenced object. |
Revision | This read-only property returns a string that contains the Document revision number. |
Status | This read-only property returns a constant value from the DocumentStatus constant set that specifies the status of the referenced Document. |