Solid Edge Revision Manager Object Library
DeleteDocumentsFromServer Method
Specifies the number of documents to delete from the server.
Specifies the documents to delete from the server. This is the URL path of the documents on the Sharepoint server.
Specifies the number of documents successfully deleted from the server.
Specifies the documents successfully deleted from the server.
Description
This method deletes the documents you specify from the server.
Syntax
Visual Basic
Public Function DeleteDocumentsFromServer( _
   ByVal NumberOfDocumentsToBeDeleted As Long, _
   ByVal ListOfDocumentsToBeDeleted As Variant, _
   ByRef NumberOfSuccessfullyDeletedDocuments As Long, _
   ByRef SuccessfullyDeletedDocuments As Variant _
) As Long
Parameters
NumberOfDocumentsToBeDeleted
Specifies the number of documents to delete from the server.
ListOfDocumentsToBeDeleted
Specifies the documents to delete from the server. This is the URL path of the documents on the Sharepoint server.
NumberOfSuccessfullyDeletedDocuments
Specifies the number of documents successfully deleted from the server.
SuccessfullyDeletedDocuments
Specifies the documents successfully deleted from the server.
Example
Imports RevisionManager
Imports System.Runtime.InteropServices

Module Example

    Sub Main()
        Dim objApplication As RevisionManager.Application = Nothing
        Dim objInsight As RevisionManager.Insight = Nothing
        Dim aFilesToDelete(0) As String
        Dim NumberOfSuccessfullyDeletedDocuments As Long
        Dim aSuccessfullyDeletedDocuments As Object

        Try
            ' Start Revision Manager.
            objApplication = New RevisionManager.Application

            ' Get reference to Insight object.
            objInsight = objApplication.Insight

            aFilesToDelete(0) = "http://solidvm/Engineering/PreReleased/PreReleasedDocLib/Summit.par"

            objInsight.DeleteDocumentsFromServer(aFilesToDelete.Length, aFilesToDelete, NumberOfSuccessfullyDeletedDocuments, aSuccessfullyDeletedDocuments)
        Catch ex As Exception
            ' Write any errors to console.
            Console.WriteLine(ex.Message)
        Finally
            ' Release COM Objects.
            If Not (objInsight Is Nothing) Then
                Marshal.ReleaseComObject(objInsight)
                objInsight = Nothing
            End If

            If Not (objApplication Is Nothing) Then
                objApplication.Quit()
                Marshal.ReleaseComObject(objApplication)
                objApplication = Nothing
            End If
        End Try
    End Sub

End Module
See Also

IInsight Object  | IInsight Members

Send comments on this topic.