Solid Edge Revision Manager Object Library
GetFiles Method
Specifies the URL path of the parent location on the SharePoint server.
Specifies the number of files found.
Specifies the files found.
Specifies the filter criterion, such as “par, asm, dft”, for the files to be searched.
Description
This method returns a file listing for the specified location.
Syntax
Visual Basic
Public Function GetFiles( _
   ByVal ParentUrl As String, _
   ByRef numberOfFilesFound As Long, _
   ByRef ListOfFilesFound As Variant, _
   Optional ByVal FileFilter As Variant _
) As Long
Parameters
ParentUrl
Specifies the URL path of the parent location on the SharePoint server.
numberOfFilesFound
Specifies the number of files found.
ListOfFilesFound
Specifies the files found.
FileFilter
Specifies the filter criterion, such as “par, asm, dft”, for the files to be searched.
Example
Imports RevisionManager
Imports System.Runtime.InteropServices

Module Example

    Sub Main()
        Dim objApplication As RevisionManager.Application = Nothing
        Dim objInsight As RevisionManager.Insight = Nothing
        Dim ParentUrl As String
        Dim NumberOfFilesFound As Long
        Dim aListOfFilesFound As Object = Nothing
        Dim FileFilter As Object

        Try
            ' Start Revision Manager.
            objApplication = New RevisionManager.Application

            ' Get reference to Insight object.
            objInsight = objApplication.Insight

            ParentUrl = "http://solidvm/Engineering/PreReleased/PreReleasedDocLib"
            'FileFilter = ".asm,.par,.psm,.cfg,.dft"
            FileFilter = ".par"

            objInsight.GetFiles(ParentUrl, NumberOfFilesFound, aListOfFilesFound, FileFilter)

        Catch ex As Exception
            ' Write any errors to console.
            Console.WriteLine(ex.Message)
        Finally
            ' Release COM Objects.
            If Not (objInsight Is Nothing) Then
                Marshal.ReleaseComObject(objInsight)
                objInsight = Nothing
            End If

            If Not (objApplication Is Nothing) Then
                objApplication.Quit()
                Marshal.ReleaseComObject(objApplication)
                objApplication = Nothing
            End If
        End Try
    End Sub

End Module
See Also

IInsight Object  | IInsight Members

Send comments on this topic.