| Item |
Description |
| PR 2130405 |
Problems occur when "Addin" is registered in "Quick Access Toolbar" |
| PR 1566510 |
OpenSave macro fails with runtime error if file has status 'in work' |
| PR 1729888 |
third party add-in added to QAT works first time but if SE is closed and re-opened |
| PR 2130772 |
CommandBarButton::BeginGroup Property has no effect |
| PR 2129831 |
In SynchronousParts, "CopySurface.Type Property" cannot be acquired |
| PR 2129884 |
Implemented InterpartConstructions and InterpartConstruction automation methods |
| PR 1751696 |
SEPreview causes application termination |