Solid Edge ST6 SDK
Solid Edge ST2 MP8 - Readme

--------------
Legal Notices
--------------
©2010 Siemens Product Lifecycle Management Software Inc.

All Rights Reserved
Software, file formats, and audiovisual displays may be used pursuant to the
applicable Software License Agreement and contain confidential and proprietary
information of Siemens Product Lifecycle Management Software Inc.; which is
protected by copyright and trade secret law. Such materials may not be reproduced
or transferred to other documents or used or disclosed to others for manufacturing
or for any other purpose except as specifically authorized within the terms of the
Software License Agreement, or as specifically authorized in writing by Siemens
Product Lifecycle Management Software Inc.

Siemens Product Lifecycle Management Software Inc.
5800 Granite Parkway
Suite 600
Plano, TX. 75024


--------------------
End of Legal Notices
--------------------

--------------
Release Notes:
--------------

Product:        Solid Edge
Version:        102.00.08.04
Date:           28-Jul-2010

Maintenance Packs are all inclusive and can be installed on top of the base
release or any released Maintenance Pack.

This Maintenance Pack can be installed on top of Versions:
102.00.00.116, 102.00.01.04, 102.00.02.06, 102.00.03.04. 102.00.04.03, 102.00.05.04,
or 102.00.06.04, 102.00.07.04.


This release of Solid Edge has been certified to run on the following:

   - Windows XP Professional© operating system (32-bit or 64-bit)
   - Windows Vista Business© or Vista Enterprise© operating system (32-bit or 64-bit)
   - Windows 7 Professional©, Enterprise©, or Ultimate© operating system (32-bit or 64-bit)
   - Internet Explorer 7 or 8 (IE 6.0 minimum)


User Account Control (UAC) -- Due to continued reports of problems with Solid Edge installation and removal, Solid Edge licensing, Insight web parts and other cases writing to text files in the program folder, it is recommended that the UAC be turned off when running on Windows 7 or Vista.  

        Windows 7: Control Panel -> User Accounts -> Change User Account Control settings ->
                   Never notify

        Vista:  Control Panel -> User Accounts and Family Safety -> User Accounts ->
                Turn User Account Control Off.

--------------------
End of Release Notes
--------------------

-------------------
Installation Notes:
-------------------

After downloading the Maintenance Pack to your machine, dbl click the downloaded
file and the Maintenance Pack will install.

-------------------
End of Installation
-------------------

--------------------------------------------------
This Maintenance Pack addresses the following PRs:
--------------------------------------------------

=====Assembly=====

PR 1707367: Unable to rename Group in ASM
PR 1779936: Coordinate systems are not selectable
PR 1791681: Component image doesn't work
PR 6364289: Upgraded ST2 translators
PR 1789244: Line changes position after creation
PR 6367560: Assembly Sketch will not Maintain Associativity if assembly is read-only
PR 6373440: Inconsistency with how Solid Edge updates a part that is driven by inter-part links in an assembly
PR 1796899: Unable to connect an XpresRoute path to the center point of a circle
PR 6374271: Copied sketches do not update when the parent sketch is modified
PR 6383384: Solid Edge crashes in Assembly while trying to add a coordinate system

=====Draft=====

PR 1791433: The shading tone changes in this file when updated in ST2,
PR 2149008: Solid Edge crashes when trim is executed with Control-Key active
PR 6365525: Save as to AutoCAD translates spaces in layer names as underscores
PR 6367433: Item number edit is lost if the enter key is not pushed prior to changing dialogs
PR 6370637: Display problems in a draft file
PR 1789362: Threads are not generated for offset split cylinder threads
PR 1796408: Trim command causes Solid Edge to abort when moving the cursor over elements
PR 1771612: Unable to start the parts list command in this file
PR 1796054: Parts list disappears when this file is opened in ST2
PR 2146859: Parts List title changed when opening this file in ST2
PR 6381097: CUT LENGTH custom property is not displayed

===Insight/View & Markup===

PR 6361582: Poor performance on Open dialog w/ searchscope.txt located on network
PR 6378285: Get an Application memory error when exiting Edge and or Revision Manager
PR 1795355: 64-Bit View and Markup can't be started with Solid Edge Premium License when Solid Edge is running
PR 1797106: Symmetric Diameter Dimension from sketch is not migrated to Revolved Protrusion

=====Part/Profile/Sheet Metal=====

PR 6359760: Time to read volume increases exponentially.
PR 1791848: not all pattern members match up with the patterned feature
PR 1793304: Main body disappears when a section view is applied
PR 6283714: Analysis results do not change after changing material type
PR 6318659: Changing dimension value in the form of value+units is not working
PR 6359300: Solid Edge Simulation is duplicating a load in an assembly
PR 6368495: Persistent symmetrical relations are ignored during dimension edit
PR 1795384: Unable to create coplanar axis with three holes and plane
PR 6264561: Close corner creates an incorrect flat pattern
PR 6273212: Failure to move a face on a symmetric Contour Flange with locked dimensions
PR 6372520: Problem adding draft to projected profile sketch

===== Solid Edge Embedded Client=====

PR 2141263: Smart Codes are generating duplicate fields in Compose Item ID dialog
PR 6366794: Overlay Template is causing the upgrade to Teamcenter 8.1 to stop
PR 6369259: Save As of the provided assembly fails
PR 6359038: Transposed properties in save as operation
PR 6367066: Save As and Replace multiple actions in single Structure Editor are failing
PR 6381802: Custom BVR type is not deleting entries from BVR, but instead incrementing
PR 6384204: Solid Edge crashes when trying to open the provided assembly that requires BOM Sync

---
End
---