--------------
Legal Notices
--------------
©2010 Siemens Product Lifecycle Management Software Inc.
All Rights Reserved
Software, file formats, and audiovisual displays may be used pursuant to the
applicable Software License Agreement and contain confidential and proprietary
information of Siemens Product Lifecycle Management Software Inc.; which is
protected by copyright and trade secret law. Such materials may not be reproduced
or transferred to other documents or used or disclosed to others for manufacturing
or for any other purpose except as specifically authorized within the terms of the
Software License Agreement, or as specifically authorized in writing by Siemens
Product Lifecycle Management Software Inc.
Siemens Product Lifecycle Management Software Inc.
5800 Granite Parkway
Suite 600
Plano, TX. 75024
--------------------
End of Legal Notices
--------------------
--------------
Release Notes:
--------------
Product: Solid Edge
Version: 102.00.09.05
Date: 03-Sep-2010
Maintenance Packs are all inclusive and can be installed on top of the base
release or any released Maintenance Pack.
This Maintenance Pack can be installed on top of Versions:
102.00.00.116, 102.00.01.04, 102.00.02.06, 102.00.03.04. 102.00.04.03, 102.00.05.04,
102.00.06.04, 102.00.07.04, or 102.00.08.04.
This release of Solid Edge has been certified to run on the following:
- Windows XP Professional© operating system (32-bit or 64-bit)
- Windows Vista Business© or Vista Enterprise© operating system (32-bit or 64-bit)
- Windows 7 Professional©, Enterprise©, or Ultimate© operating system (32-bit or 64-bit)
- Internet Explorer 7 or 8 (IE 6.0 minimum)
User Account Control (UAC) -- Due to continued reports of problems with Solid Edge installation and removal, Solid Edge licensing, Insight web parts and other cases writing to text files in the program folder, it is recommended that the UAC be turned off when running on Windows 7 or Vista.
Windows 7: Control Panel -> User Accounts -> Change User Account Control settings ->
Never notify
Vista: Control Panel -> User Accounts and Family Safety -> User Accounts ->
Turn User Account Control Off.
--------------------
End of Release Notes
--------------------
-------------------
Installation Notes:
-------------------
After downloading the Maintenance Pack to your machine, dbl click the downloaded
file and the Maintenance Pack will install.
-------------------
End of Installation
-------------------
--------------------------------------------------
This Maintenance Pack addresses the following PRs:
--------------------------------------------------
===API===
PR 1800096: CommandInfo::Caption() property will always returns empty for command ID 32810
PR 1796603: Usage of the optional arguments inTube.Path does not return objects
PR 6342066: API 'SelectSet.Item' is not working with Partslist object in ST2
=====Assembly=====
PR 1771221: Problem positioning the Steering wheel in ASM with active faces
PR 6372092: Selecting parts in large assembly taking a long time
PR 6380041: Cannot save assembly after disconnecting/reconnecting network
PR 6381545: Crash occurs when editing the definition of assembly body (weld bead)
PR 1747914: Xpress Route piping generates wrong Pipe-Segments
PR 6383680: Command ribbon goes blank after minimizing and exiting XpresRoute
PR 6394295: Redo crash after moving face in assembly which consumed a Hole
PR 1799206: Step file generated by MDT will not import correctly
=====Draft=====
PR 1780242: Parts lists converted to User Tables does not sort correctly
PR 1799845: Layer selection with CTRL doesn't work correctly on Windows 7
PR 6349921: Cannot place parts list
PR 6370007: Drawing view is partially hidden while placing dimensions
PR 1800681: Cropped edges in a detail view are not displayed correctly
PR 1801220: Copying contents from parts list adds a space when data is empty
PR 5909261: Offset threads are incorrect
PR 6386462: Balloons connected to draft quality views re-connect to active parts list
PR 6394499: Change to table style are not saved when using ST2 MP 8
PR 1798883: abort during update of DQ view of large assembly in 64-bit SE
PR 6181503: intermittent failure of copy paste associated with blocks
PR 6360214: Multiple center marks in patterned holes
PR 6397789: dimensions detach on update of assembly sections
===Insight/View & Markup===
PR 6386220: Free Viewer always fails to display on first attempt
PR 1798985: Duplicate SEDocIDs reported when opening an assembly and versioning is turned on
PR 6396560: Insight Search for Broken Links will not process when folder name has a period
=====Part/Profile/Sheet Metal=====
PR 1707788: Threads missing on drawing views of a PWD file
PR 2150937: Fit window with hidden coordinate system is incorrect
PR 6287312: Close corner feature failing during a recompute
PR 1788005: loss of performance in ST2 compared to V19 when opening files and display
PR 6396740: Crash after editing a profile of a cutout in part
===== Solid Edge Embedded Client=====
PR 1799015: Solid Edge documents cannot be saved when mapping UOM
PR 1797685: Can't "Save As" to create a new Item from an existing Released Item
PR 2152202: Opening a draft file performance very poor after upgrading to ST2
PR 6398819: Provided an option to open draft documents and not include InterPart Links
PR 1803773: multiplied BOM structure in PSE with SE ST2
PR 6354328: Data Prep: Analyze Errors on Part Linked to Excel file
---
End
---