Solid Edge ST6 SDK
Solid Edge ST3 MP3 - Readme

--------------
Legal Notices
--------------
©2011 Siemens Product Lifecycle Management Software Inc.

All Rights Reserved
Software, file formats, and audiovisual displays may be used pursuant to the
applicable Software License Agreement and contain confidential and proprietary
information of Siemens Product Lifecycle Management Software Inc.; which is
protected by copyright and trade secret law. Such materials may not be reproduced
or transferred to other documents or used or disclosed to others for manufacturing
or for any other purpose except as specifically authorized within the terms of the
Software License Agreement, or as specifically authorized in writing by Siemens
Product Lifecycle Management Software Inc.

Siemens Product Lifecycle Management Software Inc.
5800 Granite Parkway
Suite 600
Plano, TX. 75024


--------------------
End of Legal Notices
--------------------

--------------
Release Notes:
--------------

Product:        Solid Edge
Version:        103.00.03.04
Date:           24-Feb-2011

Maintenance Packs are all inclusive and can be installed on top of the base
release or any released Maintenance Pack.

This Maintenance Pack can be installed on top of Versions:
103.00.00.114, 103.00.01.05, or 103.00.02.04.


This release of Solid Edge has been certified to run on the following:

- Windows XP Professional operating system (32-bit or 64-bit)
- Windows Vista Business or Vista Enterprise operating system (32-bit or 64-bit)
- Windows 7 Enterprise, Ultimate and Professional (32-bit or 64-bit)
- Internet Explorer 8 (IE 6.0 meets minimum requirements)
 
Please see the Solid Edge Readme file (Readme.htm) in the ...\Program Files\Solid Edge ST3
folder for additional details.


--------------------
End of Release Notes
--------------------

-------------------
Installation Notes:
-------------------

After downloading the Maintenance Pack to your machine, dbl click the downloaded
file and the Maintenance Pack will install.

-------------------
End of Installation
-------------------

--------------------------------------------------
This Maintenance Pack addresses the following PRs:
--------------------------------------------------

===API===
PR 6426380: Not getting Colors in SEPartReader, SEReader

===Assembly===
PR 1824462: Fixed crashes identified by crashlog files
PR 1826468: Path name length is limited to 129 characters in Property Manager
PR 6462576: Solid Edge crashes after selecting part of SysLib after placing it
PR 6465652: Abort if save is clicked while config file open dialog is active
PR 1829176: Unable to activate zones with double-click
PR 6471148: Display performance is slow on rotations and zooming
PR 6474039: Fixed crashes identified by crashlog files
PR 1815765: Unable to open Catia V5 R20 part files
PR 1828742: Solid Edge Frame Design / Routing API.
PR 6417945: the default location of the Quickbar / Assembly Pathfinder is not correct in Sketch
PR 6429834: Patterned frame members list is on separate line item in Parts List
PR 6461646: scroll to part results being obscured by the relation tree
PR 6470893: Solid Edge is slow to open a Parasolid assembly
PR 1819591: Assembly aborts when creating relationships
PR 6469074: Assembly reports are not picking up custom property values
PR 6472642:  New Menu Starting Wrong Template

===Draft===
PR 6327121: Abort on close if dim tracker has been run and something remained in the select set
PR 6357213: Callout Text gets merged if Alignment is changed to Center or Right
PR 6412216: Dimensions detach on update
PR 6427966: Part aborts revolving a synchronous cutout
PR 6429679: Exiting profile causes an abort
PR 6454096: Cannot exit edit boundary environment after ctrl-drag of 2d object
PR 6456030: Solid Edge open DWG Options/Review are not giving the correct sheet information
PR 6456838: Can't place a dimension in a Detail View using dimension axis
PR 6464949: Parts list moves up and left by .175 mm when opened
PR 1816750: Cannot select elliptical arcs in hole table command
PR 2162210: "Thread Display Mode" changes value when Apply button is clicked on other property pages

===Insight/View & Markup===
PR 6457292: Failed to generate document libraries property mapping information
PR 6465929: Insight server log files cannot be generated for SharePoint 2010
PR 6466137: Registry key VMOnSaveEmbedViewingLink not delivered in ST 3

===Part/Profile/Sheet Metal===
PR 1776878: Callout for %HS is incorrect on Part Copies
PR 1824462: a crash that may occur when imprinting curves
PR 6367518: If Relationship Colors is on, no indication when dimensions are failed
PR 6434556: a crash occurring when locating items in pathfinder after closing a file
PR 6453116: Immediately after rotate you see a flash of the model in a different orientation
PR 6456053: Sync Hole gets deleted if it’s used sketch is deleted after a Move to Sync
PR 6467561: the Solid Edge process hangs around after selecting a region then exiting
PR 6468272: Unable to edit a dimension value with a key-in after scrolling with mouse wheel
PR 1809044: a crash is occurring when trying to open a Solid Edge file
PR 6471224: the concentric live rules turning red when using local symmetry option
PR 6471336: Dimension display disappears during edit formula
PR 6473059: sync move appearing sluggish on keypoint locate
PR 6474371: Cannot pattern a hem
PR 6475818: SendMail & Crashlog tracking failing under Lotus Notes
PR 1827775: Displaying the FOP table tooks a long time
PR 2163514: "Show Only Overridden Variables" of the family of parts not being displayed
PR 6477746: Cylinder from a Lofted Flange in ordered sheet metal part has incorrect flat result


---
End
---