Solid Edge ST6 SDK
Solid Edge ST3 MP6 - Readme

--------------
Legal Notices
--------------
©2011 Siemens Product Lifecycle Management Software Inc.

All Rights Reserved
Software, file formats, and audiovisual displays may be used pursuant to the
applicable Software License Agreement and contain confidential and proprietary
information of Siemens Product Lifecycle Management Software Inc.; which is
protected by copyright and trade secret law. Such materials may not be reproduced
or transferred to other documents or used or disclosed to others for manufacturing
or for any other purpose except as specifically authorized within the terms of the
Software License Agreement, or as specifically authorized in writing by Siemens
Product Lifecycle Management Software Inc.

Siemens Product Lifecycle Management Software Inc.
5800 Granite Parkway
Suite 600
Plano, TX. 75024


--------------------
End of Legal Notices
--------------------

--------------
Release Notes:
--------------

Product:        Solid Edge
Version:        103.00.06.05
Date:           14-Jun-2011

Maintenance Packs are all inclusive and can be installed on top of the base
release or any released Maintenance Pack.

This Maintenance Pack can be installed on top of Versions:
103.00.00.114, 103.00.01.05, 103.00.02.04, 103.00.03.04, 103.00.04.05, or
103.00.05.03.

This release of Solid Edge has been certified to run on the following:

- Windows XP Professional operating system (32-bit or 64-bit)
- Windows Vista Business or Vista Enterprise operating system (32-bit or 64-bit)
- Windows 7 Enterprise, Ultimate and Professional (32-bit or 64-bit)
- Internet Explorer 8 (IE 6.0 meets minimum requirements)
 
Please see the Solid Edge Readme file (Readme.htm) in the ...\Program Files\Solid Edge ST3
folder for additional details.


--------------------
End of Release Notes
--------------------

-------------------
Installation Notes:
-------------------

After downloading the Maintenance Pack to your machine, dbl click the downloaded
file and the Maintenance Pack will install.

-------------------
End of Installation
-------------------

--------------------------------------------------
This Maintenance Pack addresses the following PRs:
--------------------------------------------------

===API===

PR 6525375: BalloonDisplayedText showing symbols instead of display values
PR 1845612: API method SeekWriteAccess doesn't work properly in ST3

===Assembly===

PR 1819823: Cannot import STEP files
PR 6482973: Assembly relation tree in ST3 obscuring selected parts
PR 6524547: SESysInfo reporting negative memory value for graphic cards w/2GB or more onboard memory
PR 6530354: crash after editing connect relation
PR 6530975: Check interference doesn't consider weld features when selecting subassembly
PR 6532294: Relation Tree not showing document icon
PR 1822686: JT file will open in Traditional but will not open in Synchronous
PR 1828686: Missing parent for sketches in an assembly are not reported
PR 6425708: Reference plane not hidden after exit of Assemble command
PR 6468554: Missing files after import of a X_T file
PR 6489805: When using Publish Virtual/Publish SE aborts
PR 6533309: Abort when adding assembly relationships
PR 6534186: Rotating an assembly causes assigned textures to change color during rotation
PR 1828736: Long beam is not cut to C channel profile (frame module)
PR 1845357: seCatiaV5.exe crashes
PR 1849144: Unable to finish tube placement on German OS
PR 6443468: Batch translators are not generating output
PR 6484486: Cannot export Solid Edge files to STEP
PR 6534753: Application Display settings will now properly detect the new Intel HD Onboard driver
PR 2169599: A fully constrained assembly becomes under-defined on flipping to rigid from adjustable
PR 6471511: Unable to Translate Inventor Assemblies with Data Migration tool
PR 6535868: List Control tab options are enabled with 'use assembly item numbers' is on
PR 6541886: Crash at: OccurrenceNode::GetSite
PR 6550314: Crash when activating assembly parts via the pathfinder

===Draft===

PR 1844982: "check config" on drawing view properties was not working
PR 1846422: Parts list quantity is incorrect when using assembly item numbers
PR 6458478: SE crash occurred while inserting image in draft document (Workflow specific)
PR 6484441: Reference dimensions have extra brackets when exported
PR 6531106: Fixed crash identified by crashlog at: HGetQuantityOverrideFromOccurrence
PR 1819327: dxf_Export is not including some crosshatching
PR 1822869: rotating the contents of a draft file causes Solid Edge to crash
PR 1823915: Cutting plane lines are missing in exported AutoCAD DWG file
PR 1830725: Parts list has an asterisk next to the item number
PR 1833156: the drawing view "show fill" option not honored
PR 1836348: It's necessary to click twice on Break Line option in the Callout command bar
PR 1843290: Symbols not placing correctly when Inserted as Geometry
PR 1847031: Geometry in a 2D Model view cannot be moved/copied, huge file size
PR 2165599: Can't maintain separate grid settings when two draft documents are open
PR 2165638: Existing Solid Edge draft template issue in windows 7
PR 2166696: Dimension tracker copy to clipboard is not working
PR 2168599: View not being refreshed after activating hidden layer
PR 6419394: Opening of 2000/2002 DWG file does translate any geometry 
PR 6438019: Trim Corner selection is picking the wrong line
PR 6487857: DV tracker update instructions were incorrect for part copy
PR 6529930: Detail View Caption can't be moved correctly if envelope is an ellipse
PR 1826475: Selection mode remains active after balloon number change
PR 1817696: Embedded Objects are exported to DXF in the wrong position
PR 1824327: Fill Text with Background color rectangle position incorrect
PR 1832830: Seacad "template file" is empty if you don't go through seacad option steps
PR 1833975: Attempting to open a dgn file aborts if the look in button is selected
PR 1840830: DV caption is exported to layer "0"
PR 1842175: Cutting plane line cannot be selected with "Active Layer Only" option
PR 1847435: Tab key function for upper and lower Tolerance needs to be sequential
PR 2167888: Right Justified callout text is scrambled in .dwg
PR 2169063: Starting location of offset thread not displayed with solid line
PR 6511394: Prefix copier doesn't copy the tolerance type correctly for Class tolerance
PR 6535524: Parts list does not honor property text formatting codes
PR 6536661: Parts list reverses order each update if renumber and sort by item descending
PR 1684703: Sketch in a section view was not sectioned properly
PR 1823726: Text placed in rotated drawing views is lost after SEtoAcad translation
PR 6541869: Crash at: JDimChainAngular::Disconnect

===Insight/View & Markup===

PR 1842460: Cache Manager does not work
PR 1846854: Assembly doesn't open - No error message
PR 6461727: Search not finding Custom Properties
PR 6332833: Insight Web parts: The Viewer MP's are not getting pushed to IE clients.
PR 6399126: Insight connect crash occurred while saving PCF file (Workflow specific)
PR 1845749: Calculated Columns will not sync anymore
PR 1835210: MP info not shown in View & Markup/Help About on 64bit computers
PR 1835727: Incorrect characters in SEWebParts on Insight MP3
PR 1840719: Error Message when copying Excel Docs within a Asm Structure in RevMan
PR 1846854: Assembly doesn't open - No error message

===Part/Profile/Sheet Metal===

PR 1783293: File open dialog is slow to show large folders
PR 1844377: PartCopy from an assy will only work if the assembly is also opened
PR 6522205: Abort at JUnitsOfMeasure::~JUnitsOfMeasure
PR 6524170: tangent relate failing when the elements did not share an edge
PR 1823155: changing the value of a round using all available memory which results in a crash
PR 1843475: Flat pattern from mirror is different from original
PR 1845013: Hole Feature will not cut through the part
PR 1842597: Ribbon bar added by custom add-in is not customizable
PR 6534273: Sync threaded hole problem when using saved settings
PR 1847811: Ctrl+A in Profile environment also deletes synchronous body
PR 2170648: Selecting User-Defined Sets causes an abort
PR 6441781: Binder names not all converted to Unicode, yielding garbled display
PR 6522975: Crash when performing an undo of a move to sync
PR 6532739: Crash at: JMostRecentFiles::Add is at top of the stack trace
PR 6537877: Sync Pattern does not create all occurrences

===Solid Edge Embedded Client===

PR 1800213: Smart Codes form is locking up when saving a new file
PR 1834093: Wrong dataset name is used in ST2
PR 1837961: Automatic update of linked NX part does not work correctly
PR 1838542: Revise non-default dataset names are renamed to default.
PR 6528853: Couple issues with assemblies and missing components in SE & replace part
PR 6495119: SaveAs of a FOP master and select no to copy links copies the links anyway
PR 1844966: Time to drag and drop & open from the Edgebar takes too long
PR 1845018: SEEC Create in Place does not show default values of mapped properties in CPD
PR 6482635: Unable to Save As FOP member in Structure Editor
PR 6484834: CPD is not renaming the Item Revision properly for the Dataset Name
PR 6448444: Structure Editor is not displaying assigned LOV when creating New
PR 6530136: AddToTeamcenter is clearing Document Number value during Dry Run
PR 1844966: Time to drag and drop & open from the Edgebar takes too long
PR 1847283: NULL Attribute Values not honored
PR 6492500: Save As behavior in SEEC behaves differently to Save As behavior in SESE


---
End
---