--------------
Legal Notices
--------------
©2011 Siemens Product Lifecycle Management Software Inc.
All Rights Reserved
Software, file formats, and audiovisual displays may be used pursuant to the 
applicable Software License Agreement and contain confidential and proprietary 
information of Siemens Product Lifecycle Management Software Inc.; which is 
protected by copyright and trade secret law. Such materials may not be reproduced 
or transferred to other documents or used or disclosed to others for manufacturing 
or for any other purpose except as specifically authorized within the terms of the 
Software License Agreement, or as specifically authorized in writing by Siemens 
Product Lifecycle Management Software Inc.
Siemens Product Lifecycle Management Software Inc.
5800 Granite Parkway
Suite 600
Plano, TX. 75024
--------------------
End of Legal Notices
--------------------
--------------
Release Notes:
--------------
Product:        Solid Edge 
Version:        103.00.07.05
Date:           19-Jul-2011
Maintenance Packs are all inclusive and can be installed on top of the base 
release or any released Maintenance Pack.
This Maintenance Pack can be installed on top of Versions: 
103.00.00.114, 103.00.01.05, 103.00.02.04, 103.00.03.04, 103.00.04.05,
103.00.05.03, or 103.00.06.05.
This release of Solid Edge has been certified to run on the following:
- Windows XP Professional operating system (32-bit or 64-bit)
- Windows Vista Business or Vista Enterprise operating system (32-bit or 64-bit) 
- Windows 7 Enterprise, Ultimate and Professional (32-bit or 64-bit) 
- Internet Explorer 8 (IE 6.0 meets minimum requirements) 
 
Please see the Solid Edge Readme file (Readme.htm) in the ...\Program Files\Solid Edge ST3
folder for additional details.
--------------------
End of Release Notes
--------------------
-------------------
Installation Notes:
-------------------
After downloading the Maintenance Pack to your machine, dbl click the downloaded 
file and the Maintenance Pack will install.
-------------------
End of Installation
-------------------
--------------------------------------------------
This Maintenance Pack addresses the following PRs:
--------------------------------------------------
===API===
PR 2170447: After running a VB code get mass the Pathfinder displays features twice
PR 2170530:  Solid Edge crashing after running VB program
PR 1852995: Top most occurrences can't be added to select-set if some other occurrence is edited
PR 6562493: Engineering Reference controls show up on add-ins tab.
===Assembly===
PR 1829833:  Frames disappear when editing an assembly feature
PR 1841232: "Save As" of a sub-assembly does not create a configuration file
PR 1842409: FlashFit allowing invalid axial relationships to be created
PR 1846264: Frame-parts are not shown in the graphic window, even if they are listed in Path
PR 1851600: "User defined Quantity" will overwrite "Item Number"
PR 6538332: Beam curve is not displayed for beam study created in IPA'd assembly
PR 6538456: Crash while creating a frame using these steps
PR 6544680: Draft item numbers don't match assembly item numbers - exploded, not level-based
PR 6553615: First part placement not working correctly after installing ST3 MP6
PR 1819901: Inactive and Simplified assemblies not cut by Section View
PR 1826046: Having problems in finding area properties of a closed region assembly
PR 1851679: Total length of sketches not working correctly
PR 6556773: Fixed a crash in JGetMembassyEx submitted via auto-crashlog capture
PR 6435856: File Close after Save causes an abort with these 2 files
PR 6523676: Rename variable in Variable Table Takes too long to process
PR 6562486: Binder doesn't appear after installing MP6
===Draft===
PR 1851392: Callout attached to secondary edge of hole feature in copied view is incorrect
PR 2170472: XP only - Print of drawing results in some White space from .tiff logos
PR 6532700: Create and Connect Custom Form to SE Draft Dataset 
PR 6550243: WireHarness from a subassembly is not visible in top level assembly drawing
PR 1852903: Copying a drawing view did not copy associated config/model view/zone 
PR 6417548: Memory not being released on file close of .dft file on SE 64-bit.
PR 6549536: Trimming geometry in a RigidSet leads to poor performance 
PR 6554374: Callout not recognizing threads applied to counterbore
PR 6503052: Revision Block text boxes getting stretched
PR 6553340: Limit tolerance modifier doesn't work if decimal delimiter is a comma
===Insight/View & Markup===
PR 1824391:  Revise within Solid Edge will not take care of path from indirect files
PR 1830889:  64bit ST3 German Insight Search delivers nothing for Title and SEStatus
PR 6546240:  standalone search is crashing on all systems
PR 6557181:  InsightWebService.dll needs to be versioned
PR 6566194: Define Web Part URL is not working
PR 1853954: Life Cycle hangs when NUM_DOCLIBS_PER_QUERY set to 1
PR 1855603: SearchDuplicateIDs.exe reports unusable results
PR 6557429: Crash editing sync file in assembly after synchronizing through Cache Assistant
PR 1854804: Problem with revision manager and releasing - Error Code 0x80070024
===Part/Profile/Sheet Metal===
PR 1835004: Crash in draft setting dimension class
PR 1841949: Error in solving with certain mesh size for surface mesh
PR 1846755: Parallel reference plane dimension does not show when dynamic editing
PR 1851997: BooleanFeature::SetParameters does not accept optional args
PR 6193723: A hole fails to move after editing via live section.
PR 6421392: Offset edge command
PR 6534489: Force load is not correctly transferred to Femap resulting in incorrect results
PR 6542276: Dimension change icon not displaying during face edit
PR 1841267: Placing a synchronous feature library member fails
PR 1853256: When using 'Smart Measure' and moving over the model SE takes awhile to return
PR 1854648: Dimension.StatusOfDimension, API doesn't return expected information
PR 1854842: Custom exposed variables are not updating in draft FOP table unless applied in model
PR 6556488: Performance problem when recomputing a document with lots of part copies
PR 6556735: Pattern Profile is incorrect in ST4, a regression from ST3 
PR 6558597: Always being asked to update an FOP member even if no modification are made
===Solid Edge Embedded Client===
PR 6539916: Access violation when trying to load documents which are unloadable
PR 1844966: Time to drag and drop & open from the edgebar takes too long.
PR 6492696: SEEC terminates when Open Existing Document command is invoked
PR 6532700: Create and Connect Custom Form to SE Draft Dataset
PR 6540867: Prop txt value is not being updated on a new drawing unless the drawing is reopened
PR 6542515: Performance Related to Retrieving and Saving Model Type
PR 6543107: Assembly: Publish does not Assign Item Numbers
PR 1849660: Smart Code with "Assign" in parameters is not displaying Assign field 
PR 6538854: Placing another occurrence does searching links... 
PR 6547043: Open Part with Part Copy to NX results in Broken Link
PR 1844958: Poor performance of the Save Copy As command.
PR 1844966: Drag and drop & open from Edgebar takes too long
PR 6499778: Saved Searches not saving and deleting searches correctly
PR 6561032: User has to open certain files twice to bring them to cache
PR 6553675: It takes a long time to download templates
---
End 
---