| Item |
Description |
| PR 1860707 |
Tube creation was dramatically slowed-down in ST4 due to material update. |
| PR 6587188 |
User requests new event be fired |
| PR 6570990 |
Fixed an abort at HReGenerateSlot |
| PR 6590564 |
Fixed a problem saving 3D-PDFs via automation |
| PR 6562523 |
center-plane relationship automation support |
| PR 6574228 |
API access to Assembly variables in broken in ST4 |
| PR 1853189 |
It is not possible to set/get occurrence visibility in edit mode via API |
| PR 6585353 |
BalloonDisplayedText API does not return the correct info. |
| PR 1861355 |
Product Aborts when loading a customization file with "deny" security |
| PR 1844579 |
Need Automation support for creating PMI dimensions |
| PR 1852602 |
Replace part which belongs to a part family doesn't invoke OnFileOpenUI |
| PR 6578131 |
Added automation method to get associated assembly occurrence from draft |
| PR 1860716 |
Writing properties and dynamic attributes is very slow in ST4 after placing part |