Solid Edge ST6 SDK
Solid Edge ST4 MP10 - Readme

--------------
Legal Notices
--------------
©2012 Siemens Product Lifecycle Management Software Inc.

All Rights Reserved
Software, file formats, and audiovisual displays may be used pursuant to the
applicable Software License Agreement and contain confidential and proprietary
information of Siemens Product Lifecycle Management Software Inc.; which is
protected by copyright and trade secret law. Such materials may not be reproduced
or transferred to other documents or used or disclosed to others for manufacturing
or for any other purpose except as specifically authorized within the terms of the
Software License Agreement, or as specifically authorized in writing by Siemens
Product Lifecycle Management Software Inc.

Siemens Product Lifecycle Management Software Inc.
5800 Granite Parkway
Suite 600
Plano, TX. 75024


--------------------
End of Legal Notices
--------------------

--------------
Release Notes:
--------------

Product:        Solid Edge
Version:        104.00.10.03
Date:           07-Dec-2012


Maintenance Packs are all inclusive and can be installed on top of the base
release or any released Maintenance Pack.

This Maintenance Pack can be installed on top of Versions:
104.00.00.82, 104.00.01.08, 104.00.02.05, 104.00.03.05, 104.00.04.05,
104.00.05.05, 104.00.06.05, 104.00.07.04, 104.00.08.08, or 104.00.09.04.


--------------------
End of Release Notes
--------------------

-------------------
Installation Notes:
-------------------

After downloading the Maintenance Pack to your machine, unbundle the zip file and
then dbl click on exe to install the Maintenance Pack.

Windows 7 Installation tips: In addition to turning off UAC, right click on the exe
and select "run as administrator" to complete the installation.

Windows 7 Tip: Most of the UAC security conflicts on Win7 can be avoided by installing
Solid Edge somewhere other than the default “Program Files” folder. Install in a location
like c:\SolidEdge\ that the user has full permission to write to.

-------------------
End of Installation
-------------------

--------------------------------------------------
This Maintenance Pack addresses the following PRs:
--------------------------------------------------

===API===
PR 2208599: Can't use the StudyOwner.Count property in ST4
PR 1914096: GetReferenceToGraphicMember2 returns a runtime error
PR 1915928: When opening an alternate assembly with the API function an exception occurs
PR 1888771: Resolved issues with Ribbon Bar Customizing
PR 1911009: Split Button & Drop Button doesn't work for macros
PR 2205600: Changing Drawing View Style by API is strange when the views are made in V20
PR 2207742: NormalToFaceCutOuts.Add methd does not return the expected result

===Assembly===
PR 1892314: dimensions are not updating properly after deleting an over constrained dimension
PR 1904399: Assembly hole feature will have the wrong diameter if profile is copy/pasted
PR 1914438: Empty Assembly takes 70MB
PR 1916242: line segment - keypoints <--last selection not remembered
PR 1916906: Probe does not work on ST2 files when opened in ST4
PR 6671120: When creating a pipe routes with Schedule 40 piping it will place a Schedule 10
PR 6781360: Crash while editing XpresRoute path.
PR 6795685: Abort when selecting a face in Assemble using Flash-Fit in some scenarios
PR 1898966: Assembly Features are missing in drawing views
PR 2204078: Aborting using Measure Angle
PR 6765034: crash after deleting group of parts
PR 6806302: Undo does not work for Assembly feature edits

===Draft===
PR 1906280: If you fit this DWG, the drawing disappears
PR 1914540: V20 detail envelope caption text moves when opened in ST4 and ST5
PR 1916499: Crash after pasting into block view
PR 1916758: Reattached Center mark loose projection lines
PR 1917507: Primary caption will not be shown since ST4, regression against ST3
PR 2203988: Starting point of dimension's projection line shifts if ST2 drawing open in ST4
PR 2208005: Folded DV's caption is reset to initial value
PR 2205355: Trouble when Zoom and Pan are done in text input
PR 1921768: Item numbers change in Draft when model is not found
PR 2208364: The dimension cannot be selected

===Part/Profile/Sheet Metal===
PR 1911559: Abort after 2nd "save as flatten"
PR 1917066: Assembly aborts using 3D Input Device from 3DConnexions
PR 2206976: The size and place of the result dialog of Inspect does not be kept
PR 6794786: ribs not moving correctly with steering wheel after copy
PR 6795920: SE crashes in this workflow
PR 1919262: unlocked dimension in a sketch causes an abort during a move to synchronous

===Solid Edge Embedded Client===
PR 1911563: Problem with SE Structure Editor not showing all links
PR 1918111: SEEC - Save As Creates Precise BOM
PR 6756792: Save generates non-graphic part message in log file
PR 6772588: Copy and Paste of Item ID is not populating subsequent Item dataset names after
PR 6777503: No error message given when pool manager is down
PR 6741867: ItemID Not Generated Like RAC: USER_EXIT Customization
PR 6757392: Cannot renumber item number for an occurrence property

---
End
---