--------------
Legal Notices
--------------
©2012 Siemens Product Lifecycle Management Software Inc.
All Rights Reserved
Software, file formats, and audiovisual displays may be used pursuant to the 
applicable Software License Agreement and contain confidential and proprietary 
information of Siemens Product Lifecycle Management Software Inc.; which is 
protected by copyright and trade secret law. Such materials may not be reproduced 
or transferred to other documents or used or disclosed to others for manufacturing 
or for any other purpose except as specifically authorized within the terms of the 
Software License Agreement, or as specifically authorized in writing by Siemens 
Product Lifecycle Management Software Inc.
Siemens Product Lifecycle Management Software Inc.
5800 Granite Parkway
Suite 600
Plano, TX. 75024
--------------------
End of Legal Notices
--------------------
--------------
Release Notes:
--------------
Product:        Solid Edge 
Version:        104.00.03.05
Date:           20-Jan-2012
Maintenance Packs are all inclusive and can be installed on top of the base 
release or any released Maintenance Pack.
This Maintenance Pack can be installed on top of Versions: 
104.00.00.82, 104.00.01.08, or 104.00.02.05.
--------------------
End of Release Notes
--------------------
-------------------
Installation Notes:
-------------------
After downloading the Maintenance Pack to your machine, unbundle the zip file and 
then dbl click on exe to install the Maintenance Pack.
Windows 7 Installation tips: In addition to turning off UAC, right click on the exe 
and select "run as administrator" to complete the installation. 
Windows 7 Tip: Most of the UAC security conflicts on Win7 can be avoided by installing 
Solid Edge somewhere other than the default “Program Files” folder. Install in a location 
like c:\SolidEdge\ that the user has full permission to write to. 
-------------------
End of Installation
-------------------
--------------------------------------------------
This Maintenance Pack addresses the following PRs:
--------------------------------------------------
===API===
PR 1866474: Added API to get FillStyles from assembly document
PR 1872556: DFT preview (DraftX.ocx): Painting loops when using Visual Styles
PR 1876421: Tab "AddIns" is renamed to addin name when environment is changed twice
===Assembly===
PR 1870427:  Cannot include associatively in the assembly file
PR 1870669:  Assembly driven-part features not updating after modifying model 
PR 2169467:  Issue with frames and alternate assembly
PR 2175535:  Frame error after deleting frame from an FOA
PR 6593960:  Crash when opening exploded configuration after deleting a part
PR 6621982:  Assembly aborts when this file is opened
PR 6622485:  Replace Part is crashing in the provided test case
PR 6616058:  Customized tab does not show icons
PR 1869519:  Frame/pipe cut lengths are not reported correctly to Draft 
PR 6624346:  Solid Edge crashed when dropping flow lines
PR 6405597:  File cannot be saved if disconnected/reconnected to network
PR 1872065:  An undesired part appears during animation
PR 6617834:  Parts being placed are not locatable while section view is active
PR 6618964:  Solid Edge crashed when closing a sectioned part opened from assembly
PR 6624747:  Solid Edge closes (no crashlog generated) when trying open these SW files
PR 1868523:  Adjustable part with limits set does not report a violation when exceeded
PR 1879322:  Drop a pattern on an edit open of a sub-assembly does not delete the pattern
PR 6561285:  IPA from draft into assembly is slow in ST3 (when using file open dialog)
===Draft===
PR 1828172:  Solid Edge is generating AutoCAD text control characters as real characters 
PR 1873892:  Item number in a balloon will not update immediately
PR 6594495:  Unable to extract properties thru callout on some blocks
PR 6617549:  Getting a random crash when using trim in Draft
PR 1871852:  Parts list is empty after update
PR 2140142:  Japanese layer names are not correctly displayed by the AutoCAD Wizard
PR 2174964:  Unnecessary leader (Arrow) is displayed
PR 1877387:  Text moves away from position
PR 1877959:  Save As Image options are incorrect in ST4; JPG and TIF options are swapped
PR 6591043:  64-bit will not print correctly to a color to plotter, but 32-bit will on ST3
PR 6606179:  Feature control frames do not move with element if CREATED with a break line
PR 1761690:  Solid Edge will split one AutoCAD text string into two Solid Edge text strings
PR 6584190:  Text justification on bend table callout interferes w/leader after modification 
===Part/Profile/Sheet Metal===
PR 6596102:  Deleting features causes Solid Edge to crash when running add-in
PR 1857104:  Wrong threaded Holes from previous Solid Edge version
PR 1862813:  Inconsistent unit for moments of inertia
PR 1866347:  Save as flat with etch of single line text has unstable behavior
PR 1866914:  Dimensions in Sync FOP members are not updating correctly
PR 1872043:  Save as Flat doesn't export etches to DXF using existing flat pattern
PR 6595700:  File contains a property without valid name 
PR 6599032:  Using ‘K’ key to enable snapping when moving a face ignores 'M' hotkey 
PR 6612183:  Solid Edge aborts using the profile include command between parts
PR 6612842:  When creating overlapping flanges, the software automatically merges surfaces
PR 6618955:  Gage field in Material Table is empty
PR 1867080:  Mesh is not contiguous at several places in this model
PR 6622842:  Solid Edge crashes when editing a value in FOP table 
PR 6626403:  The Live Rule shortcut V (pause live rules) is not working
PR 6628193:  Perpendicular indicator is not being shown
PR 1870381:  Sweep using a derived curve as your path is only highlighting half of the curve
PR 1867194:  Can’t copy User defined Pattern features when converted to Sync can't be copied 
PR 1875752:  Fill Pattern with Center Orient does not select center of circle
PR 1875019:  Unable to modify parametric sketches
PR 2179818:  Solid Edge crashes when editing the profile of Hole183 feature
PR 1879843: Problem with step translator on french localized ST4 mp1/mp2
===Insight===
PR 1869597: Print Drawings tool isn't downloading the drawings to cache
===Solid Edge Embedded Client===
PR 1863800:  Runtime exception when deleting the SEEC-Cache after a Solid Edge crash  
PR 6634888:  The SolidEdgeFramework.ISEECEvents.SEEC_BeforeCPDDisplay fails for revise
PR 6586191:  Opening a Draft of an assembly and performing a Save As operation in Structure Editor will not prompt the user to perform the Save As on the inter-part link in the assembly.
---
End 
---