--------------
Legal Notices
--------------
©2012 Siemens Product Lifecycle Management Software Inc.
All Rights Reserved
Software, file formats, and audiovisual displays may be used pursuant to the
applicable Software License Agreement and contain confidential and proprietary
information of Siemens Product Lifecycle Management Software Inc.; which is
protected by copyright and trade secret law. Such materials may not be reproduced
or transferred to other documents or used or disclosed to others for manufacturing
or for any other purpose except as specifically authorized within the terms of the
Software License Agreement, or as specifically authorized in writing by Siemens
Product Lifecycle Management Software Inc.
Siemens Product Lifecycle Management Software Inc.
5800 Granite Parkway
Suite 600
Plano, TX. 75024
--------------------
End of Legal Notices
--------------------
--------------
Release Notes:
--------------
Product: Solid Edge
Version: 104.00.07.04
Date: 05-Jul-2012
Maintenance Packs are all inclusive and can be installed on top of the base
release or any released Maintenance Pack.
This Maintenance Pack can be installed on top of Versions:
104.00.00.82, 104.00.01.08, 104.00.02.05, 104.00.03.05, 104.00.04.05,
104.00.05.05, or 104.00.06.05.
--------------------
End of Release Notes
--------------------
-------------------
Installation Notes:
-------------------
After downloading the Maintenance Pack to your machine, unbundle the zip file and
then dbl click on exe to install the Maintenance Pack.
Windows 7 Installation tips: In addition to turning off UAC, right click on the exe
and select "run as administrator" to complete the installation.
Windows 7 Tip: Most of the UAC security conflicts on Win7 can be avoided by installing
Solid Edge somewhere other than the default “Program Files” folder. Install in a location
like c:\SolidEdge\ that the user has full permission to write to.
-------------------
End of Installation
-------------------
--------------------------------------------------
This Maintenance Pack addresses the following PRs:
--------------------------------------------------
===API===
PR 1898844: Cannot create reference to sub assembly coordinate system using API
===Assembly===
PR 1880141: Frame cross section not being centered on frame path segments
PR 1883573: Solid Edge shutting down when editing an assembly in property manager
PR 6578406: Frames seems excessively slow to produce members or changes
PR 6601371: Discrete & Range Limits removed from Angle Constraint after Edit
PR 6720944: Unable to transfer parts into a subassembly
PR 1895773: Reproducible network problems, so that an opened file cannot be saved
PR 6678070: Fastener system is not picking up the desired washer size
PR 2197531: hidden parts are getting turned back on after IPA/Close
PR 1897377: Dimension does not update in XpresRoute
PR 1834267: Tear-off sketch is offset from original sketch
Note: This fix applies to newly created sketches/planes, existing data is still incorrect.
===Draft===
PR 1898998: Drawing view shading is not correct when display depth is specified
PR 6706497: Text box not automatically adjusting aspect ratio
PR 6720817: Cannot open embedded excel attachment by double clicking in ST4
PR 6726715: Unable to see added rows and columns to embedded .xlsx file
PR 1875965: Dimensions of 2D model view and Blocks are displayed at scale 1:1
PR 1901768: Connectors show lines back to origin when opened in ST4 MP4 or later
PR 1902461: Unable to open dwg files made in AutoCAD LT 2006
PR 1902946: Feature control frame is modifying the leader line angle, when moving
PR 1903162: crosshatch is missing in drawing view with PMI sections
PR 6734597: Detail view is OOD and does not update with Update Views
===Insight===
PR 1893522: File load failure opening assembly after setting inactivate drawing view for review
PR 2190774: Insight upload and Add-To-Library failures using all Chinese Insight (server and client)
PR 6691601: Unable to successfully run the Create Full Text Search Index command
PR 6740350: File names for draft files set incorrectly when revising parts
===Part/Profile/Sheet Metal===
PR 1897941: Simulation Express, temporary files created in Temp folder are not deleted
PR 6635204: Cannot open NX8 part file in ST4 MP2
PR 1902199: Extent surface to keypoint does not work
PR 1902800: Problem with coordinate system that is relative to another coordinate system
===Solid Edge Embedded Client===
PR 1858790: Cannot reset the sort order on criteria in the Open -> Search dialog
PR 1893845: During Save Operation, Item ID overrides Item Name, LOV disappears
PR 6634718: Publishing virtual components creates incorrect child count in sub-assemblies
PR 6669077: Teamcenter error shown on saving part file without assigning values for mapped property
PR 6721594: Solid Edge Crashes during file open
PR 6719747: ST2 listed assemblies during BOM synch check and ST4 does not
PR 1880013: Multi-CAD w/ NX structures not synchronized after changes to NX structure
PR 1902443: Can't use SEEC ST4 MP6 with "comma" decimal separator
PR 6680750: SEEC Administrator Changes to Support Teamcenter 9.1
PR 6723514: Can't open NX assembly in Solid Edge in Teamcenter managed environment
PR 6738220: Enhance TALLog to include Timers around more Teamcenter Service calls
PR 6740845: Solid Edge aborts opening NX assembly files with SEEC
---
End
---