--------------
Legal Notices
--------------
©2012 Siemens Product Lifecycle Management Software Inc.
All Rights Reserved
Software, file formats, and audiovisual displays may be used pursuant to the 
applicable Software License Agreement and contain confidential and proprietary 
information of Siemens Product Lifecycle Management Software Inc.; which is 
protected by copyright and trade secret law. Such materials may not be reproduced 
or transferred to other documents or used or disclosed to others for manufacturing 
or for any other purpose except as specifically authorized within the terms of the 
Software License Agreement, or as specifically authorized in writing by Siemens 
Product Lifecycle Management Software Inc.
Siemens Product Lifecycle Management Software Inc.
5800 Granite Parkway
Suite 600
Plano, TX. 75024
--------------------
End of Legal Notices
--------------------
--------------
Release Notes:
--------------
Product:        Solid Edge 
Version:        105.00.01.15
Date:           24-Sep-2012
This Maintenance Pack can be installed on top of Version: 
105.00.00.102
Note: Maintenance Packs are all inclusive and can be installed on top of the base 
release or any released Maintenance Pack.
Please note there are two critical Solid Edge ST5 View and Markup PRs (listed below) that are not addressed in MP1. We understand this may preclude upgrading to ST5. We are currently working toward the resolution of these items in an upcoming ST5 MP. 
1. PR 2204400 – Solid Edge files with Japanese characters in file name cannot be opened by V&M
2. PR 6761505 – PCF files with Japanese characters in file name cannot be opened by V&M
--------------------
End of Release Notes
--------------------
-------------------
Installation Notes:
-------------------
After downloading the Maintenance Pack to your machine, unbundle the zip file and 
then dbl click on exe to install the Maintenance Pack.
Windows 7 Installation tips: In addition to turning off UAC, right click on the exe 
and select "run as administrator" to complete the installation. 
Windows 7 Tip: Most of the UAC security conflicts on Win7 can be avoided by installing 
Solid Edge somewhere other than the default “Program Files” folder. Install in a location 
like c:\SolidEdge\ that the user has full permission to write to. 
-------------------
End of Installation
-------------------
--------------------------------------------------
This Maintenance Pack addresses the following PRs:
--------------------------------------------------
===API===
PR 1903366: Replace via API does not work as via User Interface
PR 1906499: No pattern in the 3D PDF (Testcase Specific)
PR 6758285: Add in groups and tabs remain after manually disconnecting an addin
PR 6764639: Implemented API GetRayIntersections for PartDocument
PR 1875930: API: wrong Text Box Width and Weight when adding multi line text
PR 1905243: Error in API Function SolidEdgeDraft::SectionsPtr->Count
PR 2201877: API: Parents Object of the fill pattern cannot be acquired
PR 6775244: Unpinned add-in docking pane can have incorrect text displayed 
PR-1909277: ST5 license manager doesn't install on 2003 server
 Note: a new License Manager has been posted to: http://ftp.ugs.com/solid_edge/ST5/LicenseManager/ 
===Assembly===
PR 1903074: QAT will be deleted after modification
PR 2197077: Error - No License - WEBPUBLISHER
PR 6743243: The Select icon on the Radial Menu is inconsistent
PR 6757664: Simplified assembly saved as .sev is not displayed correctly in the viewer
PR 1901251: FOA file aborts on open
PR 1902264: A reproducible crash on redo after deleting assembly features.
PR 1902643: Pattern fails to update correctly when used with family of assemblies
PR 1907507: Failing relationships when assembly features are recomputed in ST4
PR 1909992: no longer being able to connect the apex of two cones with the assembly connects relationship
PR 2198695: Positioning of node in Frame Simulation always offsets from Line End 1 
PR 2201232: Frame is failing on a 3D path after a number of segments are selected 
PR 6623403: Conflicting error message on feature compute.
PR 6677853: Trimmed frame is not updating correctly 
PR 6693525: The Preview is in one location but when I finish the cmd it shifts
PR 6716296: Adjust IAC Tooltip Presentation for Unmanaged and Managed Documents 
PR 6736612: SE hangs when opening this Catia V4 document
PR 6739621: Sync face will not create parallel relationship with ordered face 
PR 6739706: Construction Display button not working when editing existing assembly relationships
PR 6741063: Crash because Interpart Assembly Copy dialog isn't modal after error message
PR 6741881: Edit IAC is kicking me out of a In place Activate Session
PR 6742610: Putting a file in MRU list that we don't create, customers click, get can't find
PR 6742634: Assembly is in a bad state after replacing several parts and choosing Cancel
PR 6742719: Interpart Assembly Copy Mirror components get out of position on save 
PR 6743337: Read-only Assistant status icon for Working is missing
PR 6744796: When creating parallel plane in frame assembly you cannot type distance in inches
PR 6745567: Solid Edge crash using replace part
PR 6745667: Mirror feature edit - output can be selected as input as well 
PR 6745769: Crash using Replace Part on a Sub Assembly while you are IPA
PR 6752175: Assembly PathFinder shows check for parts - but no parts are visible
PR 6752269: Place part results in an abort
PR 6752684: Parts disappearing after changing display configuration and mirroring parts
PR 6753747: Some rigid sets are not staying rigid when a part is being moved
PR 6758938: Bend Radius change is not honored in a SharePoint managed assembly
PR 6764470: Interpart Assembly Copy is taking a long time with a large assembly (10,000+, 700 unique)
PR 6765110: The assembly relationship command offset field is not receiving focus correctly
PR 6765737: Not being able to use captured relationships with floating offset sometimes
PR 6765748: Capture Fit does not allow selection of target for Connect relationships
PR 6769604: Relationship placement not filtering fence selection
PR 6770537: Crash when clicking select tool during an animation
PR 6608469: Assembly contains only one subassembly but nothing is visible at the top level
PR 1909977: Mate relationship behavior after replace from ST4 to ST5 due to float repair
PR 2201912: Circle not locating properly when creating 3D segment in XpresRoute in sub-assembly
PR 6752039: Include command not picking up background components
PR 6769125: Multiple Solutions dialog one hour after updating all links
PR 6769819: Assembly file not shrinking as expected when components are deleted
===Draft===
PR 1879173: Subscript text size cannot be changed via stack options
PR 1883640: Item numbers change in Draft when model is not found
PR 1894329: Callout horizontal alignment on working sheet does not match background sheet
PR 1904828: Solid Edge Crash when Editing Text
PR 1905926: Solid edge crashes with Cutting Plane command when applying Smart Dimension
PR 1906525: Underlined balloons added in ST4 to ST3 ones are orientated to the wrong side
PR 1906788: Limit tolerance format code is not displaying in Callout text on scalar values
PR 1908269: ST4 Drawing opens with empty Drawing Views
PR 1908994: Callouts for index reference date created and date modified fail to show data
PR 2202615: Draft callout gives wrong placement of text when edit
PR 2203816: "Low on Memory" message when opening draft file
PR 6584288: Solid Edge Options in 2D Drafting cannot be accessed
PR 6737136: Extension line gets added while placing PMI callout in this workflow
PR 6738709: Error message of invalid aspect ratio is shown twice
PR 6743630: Dimension edit box is not displayed in sync environment for ordered variables
PR 6744344: Detail view is incorrect after update, annotations move out/detach
PR 6745047: Dimensions detach upon update
PR 6745507: Aspect Ratio behavior is incorrect for numbered list with right justification
PR 6745929: No Units modifier (/NU) shows in the table data
PR 6746218: Try to open file and Solid Edge exits
PR 6747251: Section view of sketch fails in ST5
PR 6752231: Circle and Rectangle settings are reversed for some localization
PR 6757698: Tables group header continuity is not maintained
PR 6767274: Clicking Back or Cancel on the Drawing View Layout step causes SE to crash
PR 6770416: FOP Table changes on file open
PR 1909452: Dimensions detaching or not binding correctly on update of views with PMI sections specified
PR 6776073: New callouts with property text don't honor the user's return/new lines
===Part/Profile/Sheet Metal===
PR 6744870: Cannot save file when creating spur gear in the part environment
PR 6757659: Simplified parts saved as .sev are not simplified in the viewer
PR 1902823: Differences in Flat Pattern between ST2 and ST4 
PR 1903647: Thread information not being present in Synchronous part copy
PR 1906993: Path to "Gagetable.xls" should be updated if used from ST4-Folder
PR 1907418: Solid Edge is closing when using show variability
PR 1910286: Poor performance when using lots of profile elements to create an extrusion
PR 2200996: The move-face command is terminating if "Ctrl+F" is used
PR 2202748: Abort when using mouse wheel to scroll through MRU
PR 2204085: Linked InterPart Copy not updating when parent part is edited 
PR 6724478: Red Pencils in PathFinder after Edit Profile with no changes
PR 6726578: Truncation on Pathfinder on Japanese systems
PR 6728937: Relief faces tip after changing gage properties 
PR 6733949: Creating first component of worm gear set hangs
PR 6735152: Results using "General Bodies" mesh type looks wrong
PR 6735355: Part disappears when adding a pattern of holes
PR 6736612: Solid Edge hangs when opening this Catia V4 document
PR 6738361: Boolean Subtract of a Rib is "remembering" rib attributes in sync part 
PR 6739099: Dimension edit fails
PR 6739119: Dimension changes worked in ST4 but not ST5
PR 6740341: Trying to move a Sync face crashes Solid Edge
PR 6740964: Can't move thickness face of sheet metal file
PR 6743259: Draft for flat pattern will not show text 
PR 6743886: Smart dimension to SM bend is being placed as 'By 2 Points' 
PR 6744004: Locked linear dim changes value when flange is rotated or angular dim changed 
PR 6744102: Pattern fails to create all occurrences 
PR 6744153: Remove and split not working for persisted Relationships
PR 6744326: Material table sheet metal settings b3ecomoing disabled on systems using a comma for decimal point
PR 6746589: The previous undo transaction gets undone when canceling a Face Relate command
PR 6746790: Crash after closing variable table in this workflow 
PR 6747704: Not seeing the failure code during preview
PR 6749372: Floor reflection is much different with white background in ST5 vs ST4
PR 6754167: Toggling DB to construction makes deleting construction faces impossible
PR 6758483: ESC is not canceling translate of move handle
PR 6759202: Sync Circular Pattern Origin does not move with pattern object
PR 6759882: No edit handle for Sync Offset relationship
PR 6759942: Dimensions constraining a rotation despite relaxing all PMI in Live Rules
PR 6762767: Angular PMI between feature origins using fins is not editable 
PR 6765887: Unable to select in Assembly a part created by adding construction bodies
PR 6768638: Solid Edge aborts when a circle with a vertical alignment constraint is split
PR 6769624: File type of DXF is exposed in the part Save as drop down list 
PR 6771702: Steering wheel loses full display after F3 key and click
PR 6771967: Boolean takes an enormous amount of time to complete on this imported model
PR 1910128: Cannot change thickness in sheet metal file from ST4, please repair in ST5 
PR 6587966: Relate Faces - Concentric not working in assembly
PR 6763790: Holes cannot be recognized after import.
PR 6772511: Cannot set "Font" in the Results environment when ribbon is collapsed
PR 6774769: Hole diameter changes when mirrored
PR 6777256: 3rd mesh and solve causes extra model information in results
===Insight===
PR 6739228: Two "Home" tabs in View & Markup
PR 6739959: Random files are automatically selected upon going into folder for LCA
PR 6740007: Limit search to this search server application and scope - default incorrect
PR 6742746: Revise fails on released 3D files
PR 6743345: Nothing happens when selecting Help link (or F1) in SE Viewer
PR 6747560: In this workflow no action takes place on file using Upload All and Check In All
PR 6750411: Revision Manager Assistant command name needs modifications
PR 6754271: Cache Assistant crashes when you attempt to work offline
===Solid Edge Embedded Client===
PR 1878276: Save as is not using the dataset name from the source files.
PR 1899293: Non SE datasets are loaded in ST Cache during load process
PR 1902441: Save as into existing item revision doesn't work (naming rule)
PR 1902765: Error on save as translated from read-only part opened from assembly 
PR 1903302: SEEC Revise with SEEC_Image_Generate_3D=false creates JT file if already present
PR 1905070: Data preparation - Filename with accents 
PR 1907261: Assigning Rev ID before Item ID in Save As incorrectly names dataset
PR 6587748: Problem with Multi-CAD Create inter-part relationships.
PR 6730948: Setting the revision and then the Item ID causes the dataset name to not display
PR 6738220: Enhance TALLog to include Timers around more Tc Service calls
PR 6739686: User cannot change value that does not match revision naming rule
PR 6740151: Edge crashes on saving the file to Teamcenter sub folder's and then exit
PR 6743218: When saving a draft, Meta Model values are missing from the first several rows
PR 6743245: Saving Draft & part together loses LOV values on the CPD
PR 6744582: Mandatory Properties for excel(.xlsx)are not prepopulated on CPD
PR 6746704: Open - BOM Dialog display for Empty Item Revision
PR 6748390: Item Revision... query will not return TC item revisions with no SE datasets
PR 6760443: Custom Property on a draft file is converting from date field to text field
PR 6762079: CPD does not show Revision Naming Rule when item id also has a Naming Rule
PR 6765062: Yes/No dropdown not offered to user for some preferences
PR 6766266: IPA title bar does not update to show the new revision
PR 1901182: Property manager needs hour(s) to show properties
PR 6762629: CPD is displaying Supplemental Revision Type and Description on the RNR drop down
PR 6764742: Teamcenter virtual components are not found
PR 6771310: Replace Part with Copy keeps released status if original has the release status
---
End 
---