Problem Reports
| Item |
Description |
| PR 1690493 |
Fixed a problem where the Custom Edgebar tab does not show up in a legacy addin |
| PR 1619947 |
Fixed a problem where a call to SurfaceBoundaries.Add fails with 'type mismatch'. |
| PR 1691736 |
Fixed a problem where Class DividedPart does not support Automation from V100 |
| PR 1663220 |
Added a Block delete API. |
| PR 1675689 |
Fixed a problem where 64-bit Solid Edge crashes in Models::AddSweptProtrusion |
| PR 4007438 |
Fixed a problem where you were unable to create previews under properties via automation |
| PR 1693313 |
Added the ability to add both a bitmap and text on UI buttons created by addins |
New APIs
SolidEdgeAssembly
SolidEdgeDraft
SolidEdgeFramework
SolidEdgeFrameworkSupport
SolidEdgePart
See Also