Solid Edge ST6 SDK
Solid Edge ST MP4 - Readme

--------------
Legal Notices
--------------
©2009 Siemens Product Lifecycle Management Software Inc.

All Rights Reserved
Software, file formats, and audiovisual displays may be used pursuant to the
applicable Software License Agreement and contain confidential and proprietary
information of Siemens Product Lifecycle Management Software Inc.; which is
protected by copyright and trade secret law. Such materials may not be reproduced
or transferred to other documents or used or disclosed to others for manufacturing
or for any other purpose except as specifically authorized within the terms of the
Software License Agreement, or as specifically authorized in writing by Siemens
Product Lifecycle Management Software Inc.

Siemens Product Lifecycle Management Software Inc.
5800 Granite Parkway
Suite 600
Plano, TX. 75024


--------------------
End of Legal Notices
--------------------

--------------
Release Notes:
--------------

Product:        Solid Edge
Version:        100.00.04.04
Date:           11-Feb-2009

This Maintenance Pack can be installed on top of Versions:
100.00.00.133, 100.00.01.07, 100.00.02.07, 100.00.03.03

Note: Maintenance Packs are all inclusive and can be installed on top of the base
release or any released Maintenance Pack.

--------------------
End of Release Notes
--------------------

-------------------
Installation Notes:
-------------------

After downloading the Maintenance Pack to your machine, dbl click the downloaded
file and the Maintenance Pack will install.

-------------------
End of Installation
-------------------

--------------------------------------------------
This Maintenance Pack addresses the following PRs:
--------------------------------------------------

=====Assembly=====

PR 2095252: Files are not saved even though "save" is selected in Out of Memory dialog
PR 2111882: Display of this assembly is wrong after opening and closing a part
PR 6082317: Added functionality to IPA between mixed Traditional/Synchronous files
PR 1706324: Cannot get a Tangent Relationship to behave as needed in this case
PR 1706787: Changing scenery style in Explode Render Animate locks up Solid Edge
PR 6084919: After adding an Assembly Feature, revolved cutout, a part within a subassembly is rotating
PR 6091109: Assembly pattern no longer gets created in the correct position
PR 6097391: Family of Assemblies properties are not saved when using file properties dialog
PR 6083619: The provided assembly file will not open or will crash on open.

=====Part/Profile/Sheet Metal=====

PR 6048513: Fit window is not centering the coordinate system when that is the only thing in the file
PR 1705364: Unable to edit pattern a twice in this Synchronous part
PR 2113984: The right side flange cannot be changed from a square to a round Bend-relief

=====Draft=====

PR 2113468: Mirror sketch is not including horizontal/vertical relationships
PR 1707517: After deleting a 2D Draft view, and saving the file, the Draft file cannot be reopened
PR 1698068: Smart length dimensions cannot be changed in isometric views

===API===

PR 2112041: "run-time error '13' type mismatch" error occurs in Synchronous Mode SDK
PR 6090872: SEFacet fails to provide data for weldment files (.pwd)

===Mold Tooling===

PR 6082126: Parting Zone Dimension step hangs the process on Finish

===Insight===

PR 6094992: Insight Cache Manager Tool is disappearing when adding files to cache

---
End
---