Solid Edge ST6 SDK
Solid Edge ST MP5 - Readme

--------------
Legal Notices
--------------
©2009 Siemens Product Lifecycle Management Software Inc.

All Rights Reserved
Software, file formats, and audiovisual displays may be used pursuant to the
applicable Software License Agreement and contain confidential and proprietary
information of Siemens Product Lifecycle Management Software Inc.; which is
protected by copyright and trade secret law. Such materials may not be reproduced
or transferred to other documents or used or disclosed to others for manufacturing
or for any other purpose except as specifically authorized within the terms of the
Software License Agreement, or as specifically authorized in writing by Siemens
Product Lifecycle Management Software Inc.

Siemens Product Lifecycle Management Software Inc.
5800 Granite Parkway
Suite 600
Plano, TX. 75024


--------------------
End of Legal Notices
--------------------

--------------
Release Notes:
--------------

Product:        Solid Edge
Version:        100.00.05.04
Date:           19-Mar-2009

This Maintenance Pack can be installed on top of Versions:
100.00.00.133, 100.00.01.07, 100.00.02.07, 100.00.03.03, 100.00.04.04

Note: Maintenance Packs are all inclusive and can be installed on top of the base
release or any released Maintenance Pack.

--------------------
End of Release Notes
--------------------

-------------------
Installation Notes:
-------------------

After downloading the Maintenance Pack to your machine, dbl click the downloaded
file and the Maintenance Pack will install.

-------------------
End of Installation
-------------------

--------------------------------------------------
This Maintenance Pack addresses the following PRs:
--------------------------------------------------

=====Assembly=====

PR 1700993: Adjustable part with a value range doesn't work correctly
PR 1709984: Non-reproducible Solid Edge ST crash – crashlog only
PR 6039860: Constantly crashing after Solid Edge ST was installed
PR 6073633: Menu flyouts added to QAT are blank in subsequent sessions
PR 6088990: Editing assembly features has performance issues
PR 6087130: Poor performance on open/show with patterns

=====Part/Profile/Sheet Metal=====

PR 1698243: Image component not found in foundation license
PR 1708094: It is no longer possible to copy a face in ST after installing MP3
PR 2115603: Cannot create the 'Contour Flange' w/chain opt @ "0" radius
PR 4680817: Elements move when sketching a b-spline through key-points
PR 5936821: When connecting a curve to a circle, the circle will move even when constrained
PR 2115753: Solid Edge aborts after clicking Undo for a Copy to PMI action

=====Draft=====

PR 5858671: Added a "Print as Black" option to “Save as PDF”
PR 2112299: Cannot create the 'Section Only' with PMI model view.
PR 2116184: Solid Edge aborts when changing dimension style options
PR 6088495: Added support for "Export Annotation Color = -1" to retain annotation colors
PR 1628650: Updating drawing views does not update the model display
PR 1709146: Low Memory Warning when there appears to be plenty of virtual memory available
PR 1713403: Replacing multiple occurrences of a block isn't working
PR 6103977: Dimensions included from PMI Model Views should not be editable

===API===

PR 6088584: Problem scanning links in assemblies using RevMan API

===Insight===

PR 1706912: Edit Profile window pops up when standard parts are generated on Insight
PR 6095144: Subsequent attempts to update a released assembly are successful after first failure
PR 1706501: German Insight Version will not set the value for SEModel_Type
PR 6031094: Copy Action is cleared when multiple items are selected and use Update Links option

---
End
---