Solid Edge ST6 SDK
Solid Edge ST MP8 - Readme

--------------
Legal Notices
--------------
©2009 Siemens Product Lifecycle Management Software Inc.

All Rights Reserved
Software, file formats, and audiovisual displays may be used pursuant to the
applicable Software License Agreement and contain confidential and proprietary
information of Siemens Product Lifecycle Management Software Inc.; which is
protected by copyright and trade secret law. Such materials may not be reproduced
or transferred to other documents or used or disclosed to others for manufacturing
or for any other purpose except as specifically authorized within the terms of the
Software License Agreement, or as specifically authorized in writing by Siemens
Product Lifecycle Management Software Inc.

Siemens Product Lifecycle Management Software Inc.
5800 Granite Parkway
Suite 600
Plano, TX. 75024


--------------------
End of Legal Notices
--------------------

--------------
Release Notes:
--------------

Product:        Solid Edge
Version:        100.00.08.03
Date:           18-Jun-2009

This Maintenance Pack can be installed on top of Versions:
100.00.00.133, 100.00.01.07, 100.00.02.07, 100.00.03.03, 100.00.04.04,
100.00.05.04, 100.00.06.03, 100.00.07.04

Note: Maintenance Packs are all inclusive and can be installed on top of the base
release or any released Maintenance Pack.

--------------------
End of Release Notes
--------------------

-------------------
Installation Notes:
-------------------

After downloading the Maintenance Pack to your machine, dbl click the downloaded
file and the Maintenance Pack will install.

-------------------
End of Installation
-------------------

--------------------------------------------------
This Maintenance Pack addresses the following PRs:
--------------------------------------------------

=====Assembly=====

PR 1725020: Coordinate System loses parent if edited while hidden
PR 6003437: View range is not correct in Sync Assembly, affects IPA
PR 1730742: Part number is no longer in the pathfinder when imported from .xpk
PR 1724695: Assembly sketch with Peer locate option turned on causes an abort

=====Part/Profile/Sheet Metal=====

PR 1713228: Coordinate system name is not being updated correctly in pathfinder
PR 1723082: Flat Pattern of a corner creates faces that are not at 90 degrees

=====Draft=====

PR 1707553: Save failures in Draft
PR 2112712: Fixed a problem with SE: The problem of the "saved setting" of draft callout
PR 2112715: Preview of a "saved setting" Draft callout is wrong
PR 6055072: Unable to select and modify dimensions in a Sync Part file
PR 6084779: XLS object should respect fence select settings with fence delete
PR 1722079: Draft files abort when opened with drawing views activated
PR 2121064: Solid Edge crashed without creating a crashlog using Save As *.dxf
PR 6080344: Property text not updating
PR 1725655: Solid Edge crashed creating a draft quality View w/active parts for dimensioning

===API===

PR 1729751: Fixed a problem with API: Problems in SE ST with Addin and Edgebar page

===Insight/View & Markup===

PR 1728732: Unable to save a Synchronous file to German Insight Server
PR 1701613: Russian file names not displayed in Russian Solid Edge Viewer
PR 1728953: View & Markup does not show sheet tabs since MP6
PR 1720400: Cannot open Parasolid files with Hebrew filenames
PR 2123356: .cfg files remain checked out in cache
PR 2123494: Replace Duplicate Documents dialog appears from automation after setting DisplayAlerts off

=====Embedded Client=====

PR 1707560: "save as" does not change origination date on title block
PR 1729540: Structure Editor does not clone the assembly provided
PR 1729792: Multiple draft image files are generated in Solid Edge & Teamcenter
PR 6163450: Fixed a problem with Structure Editor does not display non-graphic structure

---
End
---