Solid Edge ST6 SDK
Solid Edge ST MP9 - Readme

--------------
Legal Notices
--------------
©2009 Siemens Product Lifecycle Management Software Inc.

All Rights Reserved
Software, file formats, and audiovisual displays may be used pursuant to the
applicable Software License Agreement and contain confidential and proprietary
information of Siemens Product Lifecycle Management Software Inc.; which is
protected by copyright and trade secret law. Such materials may not be reproduced
or transferred to other documents or used or disclosed to others for manufacturing
or for any other purpose except as specifically authorized within the terms of the
Software License Agreement, or as specifically authorized in writing by Siemens
Product Lifecycle Management Software Inc.

Siemens Product Lifecycle Management Software Inc.
5800 Granite Parkway
Suite 600
Plano, TX. 75024


--------------------
End of Legal Notices
--------------------

--------------
Release Notes:
--------------

Product:        Solid Edge
Version:        100.00.09.04
Date:           29-Jul-2009

This Maintenance Pack can be installed on top of Versions:
100.00.00.133, 100.00.01.07, 100.00.02.07, 100.00.03.03, 100.00.04.04,
100.00.05.04, 100.00.06.03, 100.00.07.04, 100.00.08.03

Note: Maintenance Packs are all inclusive and can be installed on top of the base
release or any released Maintenance Pack.

--------------------
End of Release Notes
--------------------

-------------------
Installation Notes:
-------------------

After downloading the Maintenance Pack to your machine, dbl click the downloaded
file and the Maintenance Pack will install.

-------------------
End of Installation
-------------------

--------------------------------------------------
This Maintenance Pack addresses the following PRs:
--------------------------------------------------

=====Assembly=====

PR 1696220: Moment of inertia (Izz) is incorrect
PR 1716353: List both traditional and synchronous templates in the create in place dialog
PR 1723047: When the Edit Table is opened no variables are listed in this assembly
PR 1724073: Some corrupt files are wrongly recognized as academic
PR 6176542: Solid Edge crashes when moving the mouse over a harness collector node
PR 6182029: GDI fixes
PR 6182040: Docking Pane Menu contains phantom entries
PR 6182893: Solid Edge crashes on RMB click on line segment in XpresRoute
PR 6160128: Smart face options go away when IPA from synchronous to Tradition and back
PR 6087964: Assembly feature modifications shown in IPA Sync Part documents
PR 1736156: Editing a frame to add segments results in the entire frame disappearing
PR 6188503: Attempting to edit PMI in a shared file after an edit causes error and abort
PR 6188832: Added the ability for the NX adapter to write the xml file to disk
PR 6189445: Fasteners system parts do not move in synchronous environment

=====Part/Profile/Sheet Metal=====

PR 1733558: No automatic connection to pattern circle is created
PR 6168468: Simplified b-splines command workflow is not working
PR 6170573: Fit is not working correctly when a Coordinate System is displayed
PR 1716100: B-Splines in a flattened sheet metal instead of circles for countersink hole features
PR 1727290: When placing a feature in a weldment (PWD) file, the affected parts will not highlight.
PR 1716100: B-Splines in a flattened sheet metal instead of circles for countersink
PR 1722291: Automatic document preservation for synchronous part results in an empty file
PR 1731318: Flat Pattern from MP7 has geometry errors
PR 6183932: Solid Edge crashed when trying to select an element from a sketch
PR 6190217: Customer has random aborts on multiple machines, resolved based on provided crashlogs

=====Draft=====

PR 1713011: Section view is not updating properly
PR 1735543: Hole references are being deleted after setting
PR 6130685: Solid Edge crashes when retrieving dimensions from a 2D view with a hole table in it
PR 6165420: Solid Edge crashes when closing a file after editing balloon
PR 2114351: a part edge cannot be displayed correctly using "Show Edges"
PR 6190581: Sketch elements with annotation (text) are overlapped on export to dwg/dxf

===API===

PR 6173069: Cannot turn off a balloon leader using API
PR 6168832: Type lib missing for new button styles
PR 6169546: Command tooltip can become the control caption
PR 6170564: Call to GetVariables method fails for synchronous documents
PR 6176448: document.AttachedProperties() is not working for synchronous document
PR 6059635: Frame API problems, rotation angles, counts, and visibility

===Insight/View & Markup===

PR 5572121: Parts always display as simplified when opened in View and Markup
PR 6174009: Solid Edge aborts executing particular Insight workflow (PMI dimensions)
PR 1736499: Wrong query result when the "SearchIn" definition contains a non existing site
PR 1737677: Where Used query ignores specified DocLib Count in the registry
PR 1737833: Insight Query with a question mark in the filename doesn't work
PR 6180206: Moving an assembly from In Work to Available will not change associated draft files
PR 6191824: Workflow allows duplicate doc name using the Save Copy As command

=====Embedded Client=====

PR 1705408: A new assembly created with NX Manager fails to open
PR 6159299: Login through SEEC fails if subgroup name is specified
PR 6169714: Open Version from Cache takes longer than expected
PR 6164362: Solid Edge crashes when attempting file open when office 2007 has been installed
PR 6180370: The component sequence number in the IXF file is not getting updated correctly
PR 6169714: Open Version from Cache is taking longer than expected

---
End
---