| Class Module | Description |
|---|---|
| AdjustablePart | Adjustable part object. |
| AFGrooveWeld | |
| AFGrooveWelds | |
| AngularRelation3d | A 3-D relation object. |
| ArcSegment | Represents an occurrence of an ArcSegment element in an Assembly document. |
| ArcSegments | Represents a collection of ArcSegment objects. |
| AsmRefPlane | A planar object that provides a flat surface on which to create a profile within profile-based features. |
| AsmRefPlanes | A collection of Assembly RefPlane objects. |
| AssemblyBodies | |
| AssemblyBody | |
| AssemblyCopies | |
| AssemblyCopy | |
| AssemblyDocument | A document type used exclusively for assemblies. |
| AssemblyDrivenPartFeatures | |
| AssemblyDrivenPartFeaturesExtrudedCutout | |
| AssemblyDrivenPartFeaturesExtrudedCutouts | |
| AssemblyDrivenPartFeaturesHole | |
| AssemblyDrivenPartFeaturesHoles | |
| AssemblyDrivenPartFeaturesRevolvedCutout | |
| AssemblyDrivenPartFeaturesRevolvedCutouts | |
| AssemblyFamilyMember | Represents an occurrence of a member assembly in a family of assemblies. |
| AssemblyFamilyMembers | Represents a collection of AssemblyFamilyMember objects. |
| AssemblyFeatures | |
| AssemblyFeaturesExtrudedCutout | |
| AssemblyFeaturesExtrudedCutouts | |
| AssemblyFeaturesExtrudedProtrusion | |
| AssemblyFeaturesExtrudedProtrusions | |
| AssemblyFeaturesHole | |
| AssemblyFeaturesHoles | |
| AssemblyFeaturesMirror | |
| AssemblyFeaturesMirrors | |
| AssemblyFeaturesPattern | |
| AssemblyFeaturesPatterns | |
| AssemblyFeaturesRevolvedCutout | |
| AssemblyFeaturesRevolvedCutouts | |
| AssemblyFeaturesRevolvedProtrusion | |
| AssemblyFeaturesRevolvedProtrusions | |
| AssemblyFeaturesSweptProtrusion | |
| AssemblyFeaturesSweptProtrusions | |
| AssemblyFilletWeld | |
| AssemblyFilletWelds | |
| AssemblyGroup | The AssemblyGroup object consists of methods that add components to or removes components from a group. |
| AssemblyGroups | The AssemblyGroups object represents a collection of AssemblyGroup objects. |
| AssemblyMirror | |
| AssemblyMirrors | |
| AssemblyPattern | Represents an assembly pattern. |
| AssemblyPatternOccurrence | An assembly pattern occurrence. |
| AssemblyPatterns | Represents a collection of AssemblyPattern objects. |
| AssemblyProperties | Collection of AssemblyProperty objects. |
| AssemblyProperty | Allows creation and manipulation of wiring attributes. |
| AssemblyStitchWeld | |
| AssemblyStitchWelds | |
| AssemblyThread | |
| AssemblyThreads | |
| AxialRelation3d | Makes the cylindrical axis of a feature on one part colinear with the cylindrical axis of a feature on another part. |
| Bundle | |
| Bundles | |
| Cable | |
| Cables | |
| CamFollowerRelation3d | Defines a cam-follower relationship between two objects. |
| CenterPlaneRelation3d | Defines a center-plane relationship between objects. |
| ComponentLayout | |
| ComponentLayouts | |
| Configuration | A set of assembly configuration settings. |
| Configurations | Represents a collection of Configuration objects. |
| CurveSegment | Represents an occurrence of a curve segment element. |
| CurveSegments | Collection of CurveSegment objects. |
| FastenerSystem | Represents Fastener System. |
| FastenerSystems | Represents Fastener Systems. |
| GearRelation3d | Defines a gear relationship between two objects. |
| GroundRelation3d | Defines that a part remains fixed in its current position and orientation. |
| Harness | |
| Harnesses | |
| ItemNumbers | |
| Layout | An Assembly Layout object |
| Layouts | Collection of Assembly Layouts. |
| LineSegment | Represents an occurrence of a LineSegment element in an Assembly document. |
| LineSegments | Represents a collection of LineSegment objects. |
| Occurrence | An instance of an Occurrence or subassembly within an assembly. |
| Occurrences | A collection of occurrence objects. |
| Part | An instance of a part or subassembly within an assembly. |
| Parts | A collection of Part objects. |
| Path | Represents an occurrence of a curve segment element. |
| PathRelation3d | Defines a Path relationship between two objects. |
| Paths | Collection of keypoint curve objects. |
| PhysicalProperties | Contains the results of physical property calculations on the referenced object. |
| Pipe | |
| Pipes | |
| PlanarRelation3d | Makes the planar face of a feature on one part parallel with the planar face of a feature on another part. |
| PointRelation3d | An assembly 3-D point relation helper object. |
| Queries | Represents a collection of Query objects. |
| Query | Represents an instance of a Query on an associated AssemblyDocument object. |
| Relations3d | A collection of relationships for parts and subassemblies that are contained in the referenced assembly. |
| RigidSetRelation3d | |
| SegmentAngularRelation3d | Represents an occurrence of an Segment Angular constraint in an Assembly document. |
| SegmentDirectionRelation3d | Represents a relationship for which the specified relative orientations between constrained elements is maintained. |
| SegmentDistanceRelation3d | Represents a relationship for which the distance between constrained elements is maintained. |
| SegmentPointRelation3d | Represents a relationship for which the specified point relationship for a constrained element is maintained. |
| SegmentRadiusRelation3d | Represents a relationship for which a specified radius is maintained for a constrained element. |
| SegmentRelations3d | Represents a collection of all relationships applied to tubing segments within an AssemblyDocument object. |
| Segments | Represents a collection of all segment-based objects (ex. LineSegment, ArcSegment) for the associated Assembly document. |
| SegmentTangentRelation3d | Represents a relationship for which the specified tangency condition for constrained elements is maintained. |
| SimplifiedAssemblies | Simplified Assemblies |
| SimplifiedAssembly | Simplified Assembly |
| StructuralFrame | The StructuralFrame object represents a structural frame constructed along path segments in an assembly document. |
| StructuralFrames | The StructuralFrames object represents a collection of StructuralFrame objects. |
| SubassemblyBodies | |
| SubassemblyBody | |
| SubOccurrence | An instance of an SubOccurrence or subassembly within an assembly. |
| SubOccurrences | A collection of sub occurrence objects. |
| TangentRelation3d | Defines a tangent relationship between two objects. |
| TopologyReference | Represents an object that references a topological object (an edge or a face, for example). |
| Tube | An object that encapsulates all tube-related information (for example, Tube path, material, bend radii, and wall thickness) in the associated Occurrence object. |
| VirtualComponent | A virtual component object. |
| VirtualComponentOccurrence | A virtual component occurrence object. |
| VirtualComponentOccurrences | A collection of VirtualComponentOccurrence objects. |
| Wire | |
| WirePath | An occurrence of a wire path. |
| WirePathCableMembers | Represents a collection of cable member WirePath objects. |
| WirePaths | A collection of WirePath objects. |
| WirePathSegments | Represents a collection of segment WirePath objects. |
| WireRun | An occurrence of a wire run. |
| WireRunPaths | Represents a collection of WireRun path objects. |
| WireRuns | A collection of WireRun objects. |
| Wires | |
| Zone | The Zone object represents a zone in an assembly document. |
| Zones | The Zones object returns a collection of all the zones defined for the assembly document. |
| Enumeration | Description |
|---|---|
| AssemblyBaseStylesConstants | Assembly Base Styles Constants |
| AssemblyCopyActionConstants | |
| AssemblyCopyComponentConstants | |
| AssemblyCopyStatusConstants | |
| AssemblyCopyTypeConstants | |
| AssemblyFamilyMemberPropertyConstants | Assembly Family Member Property Constants |
| AssemblyGlobalConstants | Assembly Global constants |
| AssemblyPathfinderUpdateConstants | Assembly Pathfinder Update Constants |
| AssemblyReportTypeConstants | Assembly Report Type Constants |
| AssemblyWireHarnessReportTypeConstants | Assembly Wire Harness Report Type Constants |
| ConfigurationTypeConstants | Configuration Type Constants |
| ConstraintReplacementConstants | |
| CurveSegmentPathAdditionStatusConstants | Curve Segment Path Addition Status Constants |
| CurveSegmentPathRemovalStatusConstants | Curve Segment Path Removal Status Constants |
| CurveSegmentValidationConstants | Curve Segment Validation Constants |
| CurveSegmentWhichKeypointsConstants | Curve Segment Which Keypoints Constants |
| HarnessSaveAsEcadStatusConstants | Harness Save As ECAD Status Constants |
| HarnessTypeConstants | Harness Type Constants |
| InterferenceStatusConstants | Interference Status constants |
| ItemNumberModeConstants | |
| MoveMultipleMoveTypeConstants | Move Multiple Move Type Constants |
| MoveMultipleRelationshipConstants | Move Multiple Relationship Constants |
| OccurrenceStatusConstants | Assembly Occurrence Status Constants |
| PipeFittingEndTreatmentConstants | Pipe Fitting End Treatment Constants |
| PipeFittingTypeConstants | Pipe Fitting Type Constants |
| QueryConditionConstants | Query Condition Constants |
| QueryPropertyConstants | Query Property Constants |
| QueryScopeConstants | Query Scope Constants |
| Relation3dDetailedStatusConstants | Assembly Relation3d Detailed Status Constants |
| Relation3dGearRatioTypeConstants | Relation3d Gear Ratio Type Constants |
| Relation3dGearTypeConstants | Relation3d Gear Type Constants |
| Relation3dGeometryConstants | Assembly Relation3d Geometry Constants |
| Relation3dOrientationConstants | Relation3d Orientation Constants |
| Relation3dStatusConstants | Assembly Relation3d Status Constants |
| seAssemblyBodyTypeConstants | Assembly Body Type Constants |
| SegmentRelation3dDirectionConstants | Segment Relation3d Direction Constants |
| SegmentRelation3dDistanceConstants | Segment Relation3d Distance Constants |
| SegmentRelation3dGeometryConstants | Segment Relation3d Geometry Constants |
| SegmentRelation3dStatusConstants | Segment Relation3d Status Constants |
| SimplifiedAssemblyMode | Defines the whether the particular document has modeled or visible simplification |
| StructuralFrameEndConditionConstants | Structural Frame End Condition Constants |
| TubePropertyPidConstants | Tube Property Pid Constants |
| TubeSegmentAdditionStatusConstants | Tube Segment Addition Status Constants |
| TubeSegmentRemovalStatusConstants | Tube Segment Removal Status Constants |
| UpdateStructureCacheConstants | Update Structure Cache Constants |
| VirtualComponentPublishConstants | Virtual Component Publish Constants |
| VirtualComponentStatusConstants | Virtual Component Status Constants |
| VirtualComponentTypeConstants | Virtual Component Type Constants |
| VisibilityBasedSimplifiedAssemblyCopyType | Defines the whether faces or bodies are copied to the simplified assembly representation after visibility processing |
| WirePathConstants | Wire Path Constants |