| Solid Edge Constants Type Library : AcceleratorTypeConstants Enumeration |
| Member | Value | Description |
|---|---|---|
| seContainerInPlace | 4 | The accelerator for an environment that is being used as an in-place container for another embedded object. |
| seContainerInPlaceLink | 7 | The accelerator for an environment that exists as an in-place container for another linked object. |
| seEmbeded | 2 | The accelerator for an environment that serves an embedded Solid Edge object. |
| seExecutable | 1 | The accelerator of a normal environment of a Solid Edge executable (for example, Assembly). This is the type of the accelerator used when a file is opened in Solid Edge. |
| seMainFrame | 5 | The accelerator for the main frame (the Application environment), which is activated when no Solid Edge files are open. The Application environment contains a single accelerator of this type. No other environment contains an accelerator of this type. |
| seServerInPlace | 3 | The accelerator for an environment that is serving a Solid Edge object in a container. |
| seServerInPlaceLink | 6 | The accelerator for an environment that is serving a Solid Edge object linked to a container. |