| Solid Edge Constants Type Library : ApplicationGlobalConstants Enumeration |
| Member | Value | Description |
|---|---|---|
| seApplicationGlobalActivateAllParts | 66 | |
| seApplicationGlobalAdminFileLocation | 53 | AdminFileLocation |
| seApplicationGlobalANSIInchToleranceFile | 97 | ANSI Inch Tolerance File |
| seApplicationGlobalANSIMetricToleranceFile | 98 | ANSI Metric Tolerance File |
| seApplicationGlobalApplicationDisplay | 18 | Application display mode for new windows |
| seApplicationGlobalApplyActivationOverridesToParts | 65 | |
| seApplicationGlobalApplySimplifyOverridesToParts | 67 | |
| seApplicationGlobalApplySimplifyOverridesToSubAssemblies | 69 | |
| seApplicationGlobalApplyStatusToLinks | 36 | Apply Status To Links |
| seApplicationGlobalAutomaticSave | 12 | |
| seApplicationGlobalAutomaticSaveTime | 13 | |
| seApplicationGlobalAutoSharpenLevel | 110 | Automatic sharpen level |
| seApplicationGlobalAvailableRootFolder | 39 | Available Root Folder |
| seApplicationGlobalBaselinedRootFolder | 44 | Baselined Root Folder |
| seApplicationGlobalChangedPartActivation | 140 | |
| seApplicationGlobalCheckInOnClose | 20 | Check In On Close |
| seApplicationGlobalColorActive | 2 | The color for active elements |
| seApplicationGlobalColorBackground | 3 | The color for the background |
| seApplicationGlobalColorConstruction | 4 | The color for construction elements |
| seApplicationGlobalColorDisabled | 5 | The color for disabled items |
| seApplicationGlobalColorFailed | 6 | The color for failed items |
| seApplicationGlobalColorHandle | 7 | The color for handles |
| seApplicationGlobalColorHighlight | 8 | The color for highlighted elements |
| seApplicationGlobalColorLiveSectionCenterline | 92 | |
| seApplicationGlobalColorLiveSectionEdge | 91 | |
| seApplicationGlobalColorLiveSectionOpacity | 94 | |
| seApplicationGlobalColorLiveSectionRegion | 93 | |
| seApplicationGlobalColorManagerCopyIndividualFaceColors | 58 | |
| seApplicationGlobalColorManagerShowAssemblyStyleOverrides | 57 | |
| seApplicationGlobalColorManagerShowPartFaceColors | 56 | |
| seApplicationGlobalColorManagerUseIndividualPartStyles | 55 | |
| seApplicationGlobalColorManagerUseToolsOptionsColorSettings | 54 | |
| seApplicationGlobalColorProfile | 9 | The color for profiles, sketches and layouts |
| seApplicationGlobalColorRefPlane | 31 | |
| seApplicationGlobalColorSelected | 10 | The color for items in the select set |
| seApplicationGlobalColorSheet | 11 | The color for the sheet |
| seApplicationGlobalColorSheetTab1 | 138 | Specifies the first of two alternating colors for the sheet tabs. |
| seApplicationGlobalColorSheetTab2 | 139 | Specifies the second of two alternating colors for the sheet tabs. |
| seApplicationGlobalCommandBarMode | 105 | Displays mode in command bar or quick bar. |
| seApplicationGlobalCurvatureCombDensity | 34 | |
| seApplicationGlobalCurvatureCombMagnitude | 35 | |
| seApplicationGlobalCustomSettingFile | 63 | |
| seApplicationGlobalDefaultSharpness | 19 | Default sharpness for new windows |
| seApplicationGlobalDisplayArcQuality | 1 | |
| seApplicationGlobalDisplayQuality | 0 | |
| seApplicationGlobalDisplaySectionCaps | 15 | Enable the display of section caps with dynamic sections |
| seApplicationGlobalDisplayStatistics | 14 | Enable display timing statistics in the status bar |
| seApplicationGlobalDocumentNameFormula | 88 | |
| seApplicationGlobalDynamicTransition | 17 | Dynamic view transition smoothness |
| seApplicationGlobalECORootFolder | 50 | ECO Root Folder |
| seApplicationGlobalECRRootFolder | 49 | ECR Root Folder |
| seApplicationGlobalEnableDynamicTolerance | 45 | Enable dynamic tolerancing of facet data |
| seApplicationGlobalEnableThreadedDisplay | 30 | Enable multithreaded displays |
| seApplicationGlobalHideAllComponents | 64 | |
| seApplicationGlobalHoleSizeFile | 61 | |
| seApplicationGlobalInReviewRootFolder | 43 | In Review Root Folder |
| seApplicationGlobalInsightCacheLocation | 22 | Set InsightCacheLocation |
| seApplicationGlobalInsightFolderMappingFileLocation | 23 | Set InsightFolderMappingFileLocation |
| seApplicationGlobalInWorkRootFolder | 41 | Obsolete Root Folder |
| seApplicationGlobalISOToleranceFile | 99 | ISO Tolerance File |
| seApplicationGlobalLogFilesLocation | 21 | Set LogFilesLocation |
| seApplicationGlobalLookAheadVersion | 26 | LookAheadVersion |
| seApplicationGlobalMakeRevisionsObsolete | 38 | Make Revisions Obsolete |
| seApplicationGlobalObsoleteRootFolder | 40 | Obsolete Root Folder |
| seApplicationGlobalOfflineMode | 25 | Set OfflineMode |
| seApplicationGlobalOnLineHelpLocation | 144 | |
| seApplicationGlobalOpacityRefPlane | 32 | |
| seApplicationGlobalOpenAsReadOnly3DFile | 89 | |
| seApplicationGlobalOpenAsReadOnly3DFile_IndirectFiles | 95 | |
| seApplicationGlobalOpenAsReadOnlyDftFile | 90 | |
| seApplicationGlobalOpenAsReadOnlyDftFile_IndirectFiles | 96 | |
| seApplicationGlobalOverlayColor | 28 | The color for visible edge overlay |
| seApplicationGlobalOverlayColorMode | 29 | The color mode for visible edge overlay [1=Absolute, 2=Relative] |
| seApplicationGlobalPackagedCollaborationRootFolder | 48 | Packaged Collaboration Root Folder |
| seApplicationGlobalPipeThreadfsFile | 62 | |
| seApplicationGlobalPrereleaseRootFolder | 47 | Prerelease Root Folder |
| seApplicationGlobalReleasedRootFolder | 42 | Released Root Folder |
| seApplicationGlobalRevisionDelimiter | 33 | Sets Revision Delimiter |
| seApplicationGlobalSaveMultiCADDatasettoTC | 135 | |
| seApplicationGlobalSearchScope | 24 | Set SearchScope |
| seApplicationGlobalSectionCurvatureCombDensity | 141 | |
| seApplicationGlobalSectionCurvatureCombMagnitude | 142 | |
| seApplicationGlobalSessionDraftOpenInactive | 60 | Draft inactive mode on open (boolean) |
| seApplicationGlobalSheetTabDisplayInfo | 136 | Specifies what information is displayed in the sheet tab : 0 = sheet number; 1 = sheet name; 2 = sheet number and sheet name |
| seApplicationGlobalSheetTabDisplayInfoSeparator | 137 | Specifies the separator string used between the sheet number and sheet name when both are displayed in the sheet tabs. |
| seApplicationGlobalShowUnitsInValueFields | 104 | Shows units of measure in value fields. |
| seApplicationGlobalSoftwareVHL | 16 | Enable software VHL/Disable hardware VHL |
| seApplicationGlobalStatusBarCmdFinder | 84 | Status Bar Command Finder |
| seApplicationGlobalStatusBarCommonViews | 78 | Status Bar Common Views |
| seApplicationGlobalStatusBarFit | 73 | Status Bar Fit |
| seApplicationGlobalStatusBarLookAtFace | 77 | Status Bar Look At Face |
| seApplicationGlobalStatusBarNamedViews | 80 | Status Bar Named Views |
| seApplicationGlobalStatusBarPan | 74 | Status Bar Pan |
| seApplicationGlobalStatusBarPreviousView | 79 | Status Bar Previous View |
| seApplicationGlobalStatusBarRecordVideo | 145 | |
| seApplicationGlobalStatusBarRotateView | 75 | Status Bar Rotate View |
| seApplicationGlobalStatusBarSketchView | 86 | Status Bar Sketch View |
| seApplicationGlobalStatusBarSpinAbout | 76 | Status Bar Spin About |
| seApplicationGlobalStatusBarUploadToYouTube | 146 | |
| seApplicationGlobalStatusBarViewStyles | 81 | Status Bar View Styles |
| seApplicationGlobalStatusBarZoom | 71 | |
| seApplicationGlobalStatusBarZoomArea | 72 | Status Bar Zoom Area |
| seApplicationGlobalStatusBarZoomSlider | 82 | Status Bar Zoom Slider |
| seApplicationGlobalStatusBarZoomTool | 83 | Status Bar Zoom Tool |
| seApplicationGlobalSystemInfo | 46 | Retrieve system information [readonly] |
| seApplicationGlobalTeamcenterFormula | 87 | |
| seApplicationGlobalTeamCenterMode | 59 | |
| seApplicationGlobalTemplateRootFolder | 51 | |
| seApplicationGlobalUpdateDraft | 37 | Update draft files also |
| seApplicationGlobalUploadOnClose | 27 | Upload On Close |
| seApplicationGlobalUseAllSimplifiedParts | 68 | |
| seApplicationGlobalUseAllSimplifiedSubAssemblies | 70 | |
| seApplicationGlobalUseDetailEnvelopeDisplayAsCircle | 102 | Show Detail Envelope as Circle when TRUE. |
| seApplicationGlobalUseDetailEnvelopeStandard | 101 | Use to set the Detail Envelope Standard Constants. Valid values are defined by enum DetailEnvelopeStandardConstants. |
| seApplicationGlobalUseDimensionStyleElementMapAngularCoordinateDim | 118 | |
| seApplicationGlobalUseDimensionStyleElementMapAngularDim | 117 | |
| seApplicationGlobalUseDimensionStyleElementMapBalloon | 123 | |
| seApplicationGlobalUseDimensionStyleElementMapBHC | 122 | |
| seApplicationGlobalUseDimensionStyleElementMapBlockLabels | 134 | |
| seApplicationGlobalUseDimensionStyleElementMapCallouts | 124 | |
| seApplicationGlobalUseDimensionStyleElementMapCenterline | 120 | |
| seApplicationGlobalUseDimensionStyleElementMapCenterMark | 121 | |
| seApplicationGlobalUseDimensionStyleElementMapChamferDim | 119 | |
| seApplicationGlobalUseDimensionStyleElementMapCircularDiameterDim | 114 | |
| seApplicationGlobalUseDimensionStyleElementMapConnectors | 126 | |
| seApplicationGlobalUseDimensionStyleElementMapCoordinateDim | 116 | |
| seApplicationGlobalUseDimensionStyleElementMapDatumFrames | 130 | |
| seApplicationGlobalUseDimensionStyleElementMapDatumPoints | 131 | |
| seApplicationGlobalUseDimensionStyleElementMapDatumTargets | 132 | |
| seApplicationGlobalUseDimensionStyleElementMapEdgeCondition | 129 | |
| seApplicationGlobalUseDimensionStyleElementMapFCF | 133 | |
| seApplicationGlobalUseDimensionStyleElementMapLeaders | 125 | |
| seApplicationGlobalUseDimensionStyleElementMapLinDim | 111 | |
| seApplicationGlobalUseDimensionStyleElementMapRadialDiameterDim | 113 | |
| seApplicationGlobalUseDimensionStyleElementMapRadialDim | 112 | |
| seApplicationGlobalUseDimensionStyleElementMapSTSymbols | 127 | |
| seApplicationGlobalUseDimensionStyleElementMapSymmetricDiameterDim | 115 | |
| seApplicationGlobalUseDimensionStyleElementMapWeldSymbols | 128 | |
| seApplicationGlobalUseDimensionStyleMapping | 52 | |
| seApplicationGlobalUseDrawingViewShowCroppingEdges | 103 | Show cropping edges when TRUE. |
| seApplicationGlobalUseDrawingViewShowEdgesHiddenTangentEdgesHiddenByOtherParts | 107 | Show tangent edges that are hidden by other parts when TRUE. |
| seApplicationGlobalUseDrawingViewShowEdgesHiddenTangentEdgesSelfHidden | 106 | Show the hidden tangent edges when TRUE. |
| seApplicationGlobalUseISOToleranceTable | 100 | Use ISO Tolerance Table when TRUE. Use ANSI Tolerance Table when FALSE. |
| seApplicationGlobalUseOnLineHelp | 143 | |
| seApplicationGlobalUserType | 85 | Global User Type |
| seApplicationGlobalZebraFolderMapping | 109 | Set ZebraFolderMapping |
| seApplicationGlobalZebraFormula | 108 |
Solid Edge ST5 - What's New | Solid Edge ST4 - What's New | Solid Edge ST4 MP8 - What's New | Solid Edge ST3 - What's New | Solid Edge ST2 - What's New | Solid Edge ST - What's New | Solid Edge V20 - What's New | Solid Edge V19 - What's New | Solid Edge V18 - What's New | Solid Edge V18 SP4 - What's New | Solid Edge V17 - What's New