| Solid Edge Constants Type Library : CuttingPlaneLineCommandConstants Enumeration |
| Member | Value | Description |
|---|---|---|
| CuttingPlaneLineChangeTrim | 10956 | |
| CuttingPlaneLineChangeTrimCorner | 10957 | |
| CuttingPlaneLineDimensionAngleBetween | 10918 | |
| CuttingPlaneLineDimensionDistanceBetween | 10917 | |
| CuttingPlaneLineDrawingArcbyCenterPoint | 10903 | |
| CuttingPlaneLineDrawingLine | 10900 | |
| CuttingPlaneLineEditRedo | 57644 | |
| CuttingPlaneLineEditRedoList | 10113 | |
| CuttingPlaneLineEditUndo | 57643 | |
| CuttingPlaneLineEditUndoList | 10112 | |
| CuttingPlaneLineHelpAboutSolidEdge | 57664 | |
| CuttingPlaneLineHelpHelp | 57669 | |
| CuttingPlaneLineHelpHelpforAutoCADUsers | 40250 | |
| CuttingPlaneLineHelpProgrammingwithSolidEdge | 40232 | |
| CuttingPlaneLineHelpSolidEdgeHelp | 57666 | |
| CuttingPlaneLineHelpSolidEdgeontheWeb | 40500 | |
| CuttingPlaneLineHelpSolidEdgeWelcome | 40017 | |
| CuttingPlaneLineHelpTipoftheDay | 10702 | |
| CuttingPlaneLineHelpTutorials | 40218 | |
| CuttingPlaneLineHelpWhatsNew | 40253 | |
| CuttingPlaneLineRelationshipsColinear | 10946 | |
| CuttingPlaneLineRelationshipsConnect | 10940 | |
| CuttingPlaneLineRelationshipsHorizontalVertical | 10941 | |
| CuttingPlaneLineRelationshipsParallel | 10939 | |
| CuttingPlaneLineRelationshipsPerpendicular | 10942 | |
| CuttingPlaneLineToolIntelliSketch | 10507 | |
| CuttingPlaneLineToolSelectTool | 45000 | |
| CuttingPlaneLineViewFit | 10202 | |
| CuttingPlaneLineViewPreviousView | 10200 | |
| CuttingPlaneLineViewRefreshWindow | 32876 | |
| CuttingPlaneLineViewZoom | 10209 | |
| CuttingPlaneLineViewZoomArea | 10201 | |
| CuttingPlaneLineViewZoomTool | 33500 |