| Solid Edge Constants Type Library : InterferenceOptionsConstants Enumeration | 
| Member | Value | Description | 
|---|---|---|
| seIntfOptIgnoreSameNominalDia | 1 | If constant is passed in and an interference exists with the same nominal diameter, it is ignored. If the constant is not passed in, the interference is considered. | 
| seIntfOptIgnoreThreadVsNonThreaded | 2 | If constant is passed in and an interference exists between threaded fasteners and non-threaded holes, it is ignored. If the constant is not passed in, the interference is passed. |