Private Sub btnBlockAngleAndScale_Click(sender As System.Object, e As System.EventArgs) Handles btnBlockAngleAndScale.Click
Dim objApplication As SolidEdgeFramework.Application = Nothing
Dim objDraftDoc As SolidEdgeDraft.DraftDocument = Nothing
Dim objSheet As SolidEdgeDraft.Sheet = Nothing
Dim objBlockOccurrences As SolidEdgeDraft.BlockOccurrences = Nothing
Dim objBlockOcc As SolidEdgeDraft.BlockOccurrence = Nothing
Dim dAngle As Double
Dim dScale As Double
Dim objType As Type = Nothing
Try
objApplication = Marshal.GetActiveObject("SolidEdge.Application")
If objApplication Is Nothing Then
' Get the type from the Solid Edge ProgID
objType = Type.GetTypeFromProgID("SolidEdge.Application")
' Start Solid Edge
objApplication = Activator.CreateInstance(objType)
' Make Solid Edge visible
objApplication.Visible = True
End If
objDraftDoc = objApplication.ActiveDocument
objSheet = objDraftDoc.ActiveSheet
objBlockOccurrences = objSheet.BlockOccurrences
For Each objBlockOcc In objBlockOccurrences
dAngle = objBlockOcc.RotationAngle
dScale = objBlockOcc.ScaleFactor
Next
Catch ex As Exception
MsgBox(ex.ToString)
End Try
End Sub