Optional Boolean argument, with the default being true. When true, the graphics in the select set will be deleted after being copied to the block view as is done in the UI. If false, the graphics will be left as is.
Description
Replace block view contents with the contents in the select set.
Optional Boolean argument, with the default being true. When true, the graphics in the select set will be deleted after being copied to the block view as is done in the UI. If false, the graphics will be left as is.