| Solid Edge Draft Type Library : Block Object | 
|  Delete | Deletes the referenced object. | 
|  Application | Returns the active application object. | 
|  AttributeSets | Returns the AttributeSets collection object for the referenced object. | 
|  DefaultView | Gets or sets the default view associated with a block. | 
|  IsAttributeSetPresent | Returns True if a specified Attribute Set exists on the referenced object. | 
|  Name | Returns the name of the referenced object. | 
|  OccurrenceCount | Returns the number of objects in the referenced collection. | 
|  Parent | Returns the parent object for the referenced object. | 
|  ScaleDimAndAnnot | Whether or not dimensions and annotations should use the block scale. | 
|  Views | Block views collection |