Solid Edge Draft Type Library
Form Property
Description
Returns the closure state of the referenced object.
Property type
Read-only property
Syntax
Visual Basic
Public Property Form As Geom2dFormConstants
Remarks
Certain feature objects (such as the ExtrudedProtrusion object) require that a profile exhibits closure, but does not need to be physically closed. Another form of closure (implied closure) exists when both free ends of an open profile connect to a part edge. This connection with the part edge results in an enclosed area on the profile plane.
See Also

DVBSplineCurve2d Object  | DVBSplineCurve2d Members

Send comments on this topic.