|  Application | Returns the active application object. | 
|  AttributeSets | Returns the AttributeSets collection object for the referenced object. | 
|  Caption | Sets and returns the caption of the referenced object. | 
|  CaptionDefinitionText | Sets and returns the definition text for the caption. Definition text can contain codes for Property Text and Symbols. | 
|  CaptionDisplayedText | Returns the text for the caption as displayed after processing Property Text and Symbols. | 
|  DetailView | Returns the detail view associated with the detail envelope. | 
|  Diameter | Sets and returns the diameter of the referenced object. | 
|  DisplayAsCircle | Specifies whether to always display the detail envelope as a circle, even when the envelope's geometry is not a circle. | 
|  DisplayCaption | Specifies whether or not the caption of the referenced object is displayed. | 
|  DisplayStandard | Specifies the standard for displaying the detail envelope. | 
|  DisplayViewSheetNumber | Sets and returns whether the ViewSheetNumber definition string is displayed in the caption. | 
|  Document | Returns the document to which the referenced object belongs. | 
|  Index | Returns the numeric index for the active object. | 
|  IsAttributeSetPresent | Returns True if a specified Attribute Set exists on the referenced object. | 
|  Key | Returns a key (a string) to find the object relative to its owning parents. | 
|  Layer | Sets and returns the named layer on which the referenced object resides. | 
|  LineType | Sets and returns the line display type of the drawing view. | 
|  LineWidth | Sets and returns the line width (in paper space units) for the referenced object. | 
|  Name | Returns the name of the referenced object. | 
|  Parent | Returns the parent object for the referenced object. | 
|  Profile | Returns the profile associated with the parent object. | 
|  SourceDrawingView | Returns the DrawingView object from which the detail drawing view is derived. | 
|  StyleName | Sets and returns the name of the style that is applied to the referenced object. | 
|  TextColor | Sets and returns the color of the text for the caption of the referenced object. | 
|  TextFont | Sets and returns the text font of the caption of the referenced object. | 
|  TextFontStyle | Sets and returns the text font style of the caption of the referenced object. | 
|  TextHeight | Sets and returns the text height of the caption of the referenced object. | 
|  TextRatio | Sets and returns the text ratio of the caption of the referenced object. | 
|  Type | Specifies the type of the object being referenced. | 
|  ViewSheetNumberDefinitionText | Sets and returns the View Sheet Number (%VN) definition string.  This is intended for use with %{View Sheet Number|DV} property text and may include other formatting options. | 
|  Visible | Specifies whether or not the referenced object is displayed to the screen. | 
|  ZOrder | Specifies the front-to-back order in which an object is displayed relative to other objects. |