|  Application | Returns the active application object. | 
|  AutoOrient | Set printer orientation (portrait/landscape) based on sheet dimensions. Only valid when SheetsPerPage = igSingleSheets. | 
|  BestFit | Scale sheet so that it fills selected paper size. The scale cannot exceed 1.0. Only valid when SheetsPerPage = igSingleSheets. SingleSheetScale is ignored if this property is true. | 
|  Center | Sheets will be centered on page. Only valid when SheetsPerPage = igSingleSheets. | 
|  Copies | Number of copies to be printed | 
|  DisplayCutLine | Cut line will be printed in middle of gap. Only valid when SheetsPerPage = igMultipleSheets. | 
|  DisplaySheetBoundary | Sheet boundary will be printed. Only valid when SheetsPerPage = igMultipleSheets. | 
|  Gap | Size of gap printed between sheets. Only valid when SheetsPerPage = igMultipleSheets. | 
|  MultipleSheetScale | Scale to be applied to sheets when printing. Only valid when SheetsPerPage = igMultipleSheets. | 
|  Orientation | Orientation of print output - portrait or landscape. When SheetsPerPage = igSingleSheets, Orientation is only valid when AutoOrient = false. | 
|  PaperHeight | Height of paper selected for printing | 
|  PaperSize | Size of paper selected for printing. Not all sizes are supported on all printers. | 
|  PaperWidth | Width of paper selected for printing | 
|  Parent | Returns the parent object for the referenced object. | 
|  PrintAsBlack | All colors will print as black. | 
|  Printer | Selected printer. The default printer will be used if not set. | 
|  PrintToFile | Print to file. | 
|  PrintToFileName | Print file name including full path. Only valid when SheetsPerPage = igMultipleSheets. | 
|  PrintToFilePath | Path to write print files. The file names will be automatically generated. Only valid when SheetsPerPage = igSingleSheets. | 
|  ScaleLineTypes | Line types will scale when printing. | 
|  ScaleLineWidths | Line widths will scale when printing. | 
|  ScaleTooLarge | This property defines what action will be taken when printing a sheet that will not fit on the selected paper size. The options are igDraftPrintScaleToFit and igDraftPrintSkipDocument. | 
|  SheetsPerPage | Print either single sheet or multiple sheets per page. | 
|  SingleSheetScale | Scale to be applied to sheets when printing. The scale cannot exceed 1.0. This scale is only used when Best Fit is False. Only valid when SheetsPerPage = igSingleSheets. | 
|  Units | Units of Margins and Gap - millimeters or inches. | 
|  UsePrinterClipping | Use printer clipping algorithm. | 
|  UsePrinterMargins | Use the printer's default margins. Only valid when SheetsPerPage = igMultipleSheets. |