Solid Edge Draft Type Library
DisplayAnnotation Property
Collapse All
Expand All
Solid Edge Draft Type Library
>
DrawingView Object
: DisplayAnnotation Property
Description
Specifies whether or not the annotation geometry is to be displayed. The annotation is typically either the DetailEnvelope object or the ViewPlane object.
Property type
Read-write property
Syntax
Visual Basic
Public Property DisplayAnnotation As Boolean
See Also
DrawingView Object
|
DrawingView Members
Send comments
on this topic.