Solid Edge Draft Type Library
GetReferenceToGraphicMember2 Property
Description
Generates a Reference object to user-drawn 2D graphics and creates a dimension to them by passing the Reference to the method that creates the dimension. Use this method with Microsoft Visual Basic.NET.
Property type
Read-only property
Syntax
Visual Basic
Public Property GetReferenceToGraphicMember2( _
   ByVal GraphicMember As Object _
) As Reference
Parameters
GraphicMember
See Also

DrawingView Object  | DrawingView Members  | Solid Edge V18 - What's New

Send comments on this topic.