Solid Edge Draft Type Library
RetrieveCenterLinesCenterMarks Method
Specifies whether to retrieve (True) or remove (False) center lines and center marks.
Specifies a dimension style name. If no style name is specified, the active dimension style name is used.
Specifies whether to retrieve or remove center line type. The default is True.
Specifies whether to retrieve (remove center mark type. The default is True.
Specifies whether to retrieve or remove center mark projection lines. The default is False.
Specifies whether to retrieve or remove center marks with connected centers. The default is False.
Specifies whether to retrieve or remove center lines to circles. The default is True.
Specifies whether to retrieve or remove center lines to partial cylinders. The default is True.
Specifies whether to retrieve or remove center marks to circles. The default is True.
Specifies whether to retrieve or remove center marks to arcs. The default is True.
The default is True.
The default is True.
The default is True.
The default is True.
Description
This method retrieves or removes the center lines and center marks as specified for the referenced DrawingView object.
Syntax
Visual Basic
Public Sub RetrieveCenterLinesCenterMarks( _
   Optional ByVal IsRetrieve As Boolean = True, _
   Optional ByVal DimensionStyleName As String, _
   Optional ByVal TypeCenterLine As Boolean = True, _
   Optional ByVal TypeCenterMark As Boolean = True, _
   Optional ByVal ProjectCenterMark As Boolean = False, _
   Optional ByVal ConnectCenters As Boolean = False, _
   Optional ByVal GetCenterLineToFullCylinder As Boolean = True, _
   Optional ByVal GetCenterLineToPartialCylinder As Boolean = True, _
   Optional ByVal GetCenterMarkToCircle As Boolean = True, _
   Optional ByVal GetCenterMarkToArc As Boolean = True, _
   Optional ByVal GetCenterMarkToEllipse As Boolean = True, _
   Optional ByVal GetCenterMarkToPartialEllipse As Boolean = True, _
   Optional ByVal EnableCenterMarkRangeCheck As Boolean = True, _
   Optional ByVal EnableCenterLineRangeCheck As Boolean = True, _
   Optional ByVal dCenterLineMinRadius As Double = 0, _
   Optional ByVal dCenterLineMaxRadius As Double = 0, _
   Optional ByVal dCenterMarkMinRadius As Double = 0, _
   Optional ByVal dCenterMarkMaxRadius As Double = 0 _
) 
Parameters
IsRetrieve
Specifies whether to retrieve (True) or remove (False) center lines and center marks.
DimensionStyleName
Specifies a dimension style name. If no style name is specified, the active dimension style name is used.
TypeCenterLine
Specifies whether to retrieve or remove center line type. The default is True.
TypeCenterMark
Specifies whether to retrieve (remove center mark type. The default is True.
ProjectCenterMark
Specifies whether to retrieve or remove center mark projection lines. The default is False.
ConnectCenters
Specifies whether to retrieve or remove center marks with connected centers. The default is False.
GetCenterLineToFullCylinder
Specifies whether to retrieve or remove center lines to circles. The default is True.
GetCenterLineToPartialCylinder
Specifies whether to retrieve or remove center lines to partial cylinders. The default is True.
GetCenterMarkToCircle
Specifies whether to retrieve or remove center marks to circles. The default is True.
GetCenterMarkToArc
Specifies whether to retrieve or remove center marks to arcs. The default is True.
GetCenterMarkToEllipse
The default is True.
GetCenterMarkToPartialEllipse
The default is True.
EnableCenterMarkRangeCheck
The default is True.
EnableCenterLineRangeCheck
The default is True.
dCenterLineMinRadius
dCenterLineMaxRadius
dCenterMarkMinRadius
dCenterMarkMaxRadius
See Also

DrawingView Object  | DrawingView Members  | Solid Edge V17 - What's New

Send comments on this topic.