AngularLocation | Returns the angular location of the hole for the referenced HTHole object. |
Application | Returns the active application object. |
CounterboreDepth | Sets and returns the counterbore depth. |
CounterboreSize | Returns the counterbore size. |
CountersinkAngle | Sets and returns the countersink angle. |
CountersinkSize | Returns the countersink size. |
Depth | Sets and returns the distance that the referenced object extends or removes material from a solid. |
Label | Returns the label. |
Notes1 | Sets and returns the contents of the Notes1 string. |
Notes2 | Sets and returns the contents of the Notes2 string. |
Notes3 | Sets and returns the contents of the Notes3 string. |
Parent | Returns the parent object for the referenced object. |
Prefix | Sets and returns the prefix text. |
RadialLocation | Returns the radial location of the hole for the referenced HTHole object. |
Size | Returns the size. |
Suffix | Sets and returns the suffix text. |
ThreadSize | Returns the thread size of the hole for the referenced HTHole object. |
Type | Specifies the type of the object being referenced. |
XLocation | Returns the X location of the hole. |
YLocation | Returns the Y location of the hole. |