Solid Edge Draft Type Library
Add Method
Specifies the name of the ModelLink to be created.
Description
Adds an occurrence of the referenced object.
Syntax
Visual Basic
Public Function Add( _
   ByVal FileName As String _
) As ModelLink
Parameters
FileName
Specifies the name of the ModelLink to be created.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgeDraft.DraftDocument
    Dim objModelLinks As SolidEdgeDraft.ModelLinks
    Dim objModelLink As SolidEdgeDraft.ModelLink
    Const TESTFILE = "T:\vbtests\testcases\chead.par"
    ' Report errors
    Const PI = 3.14159265358979
    ' Create/get the application with specific settings
    On Error Resume Next
    Set objApp = GetObject(, "SolidEdge.Application")
    If Err Then
        Err.Clear
        Set objApp = CreateObject("SolidEdge.Application")
        Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'Get the ModelLinks collection from the Document
    Set objModelLinks = objDoc.ModelLinks
    'Add a model to the Document
    Set objModelLink = objModelLinks.Add(Filename:=TESTFILE)

    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objModelLinks = Nothing
    Set objModelLink = Nothing
End Sub
See Also

ModelLinks Collection  | ModelLinks Members

Send comments on this topic.