|  AlternatePositionMemberName | Returns the name of the alternate position assembly member that this ModelMember represents. | 
|  Application | Returns the active application object. | 
|  ComponentName |  | 
|  ComponentType | Returns the component type for the ModelMember. | 
|  DeriveFillStyleFromPart | Specifies whether or not the fill style should be derived from the underlying part. | 
|  DisplayAsReference | Displays the specified parts as reference parts. | 
|  DisplayType | Specifies the display type for the ModelMember. | 
|  DVArcs2d | Returns the DVArc2d collection of the ModelMember. | 
|  DVBoundaries2d | Returns the drawing view hatch boundaries collection. | 
|  DVBSplineCurves2d | Returns the DVBSplineCurve2d collection of the ModelMember. | 
|  DVCircles2d | Returns the DVCircle2d collection of the ModelMember. | 
|  DVEllipses2d | Returns the DVEllipse2d collection of the ModelMember. | 
|  DVEllipticalArcs2d | Returns the DVEllipticalArc2d collection of the ModelMember. | 
|  DVLines2d | Returns the DVLine2d collection of the ModelMember. | 
|  DVLineStrings2d | Returns the DVLineString2d collection of the ModelMember. | 
|  DVPoints2d | Returns the DVPoint2d collection of the ModelMember. | 
|  FileName | Returns the file name for the referenced object. | 
|  FillStyleName | Specifies the style used for the fill on sectioned parts. | 
|  GraphicMembers | Returns the GraphicMember collection of the ModelMember. | 
|  HatchAngle | Sets and returns the hatch angle that is applied to the selected parts. This value is always in radians. | 
|  HatchSpacing | Sets and returns the hatch spacing that is applied to the selected parts. This value is always in millimeters. | 
|  HiddenEdgeStyleName | Sets and returns the name of the hidden edge style that is applied to the referenced object. | 
|  ImmediateParent | Returns the immediate parent for the referenced object. | 
|  IsAlternatePosition | Specifies whether or not this ModelMember represents an alternate position of an alternate position assembly.. | 
|  IsFlat | Returns True if the ModelMember represents a flat sheet metal part. | 
|  IsPrimaryAlternatePosition | Specifies whether or not this ModelMember represents the primary position of an alternate position assembly. | 
|  IsSimplified | Returns True if the ModelMember represents a simplified part. | 
|  ModelMembers | Returns the ModelMember collection of the ModelMember. | 
|  ModelNode | Returns the corresponding ModelNode object. | 
|  Parent | Returns the parent object for the referenced object. | 
|  ShowEdgesHiddenByOtherParts | Specifies whether edges hidden by other parts are to be displayed. | 
|  ShowEdgesHiddenTangentEdgesHiddenByOtherParts | Specifies whether tangent edges that are hidden should be displayed. This setting can be set to TRUE only if ShowEdgesHiddenByOtherParts is set to TRUE. | 
|  ShowEdgesHiddenTangentEdgesSelfHidden | Specifies whether tangent edges that are hidden should be displayed. This setting can be set to TRUE only if ShowHiddenEdges is set to TRUE. | 
|  ShowFill | Specifies whether or not the fill will be shown on sectioned parts. | 
|  ShowHiddenEdges | Specifies whether hidden edges are to be displayed. | 
|  ShowSectionHatch | Specifies whether section hatches are to be displayed. | 
|  ShowTangentEdges | Specifies whether tangent edges are to be displayed. | 
|  TangentEdgeStyleName | Sets and returns the name of the tangent edge style that is applied to the referenced object. | 
|  VisibleEdgeStyleName | Sets and returns the name of the visible edge style that is applied to the referenced object. |