|  Application | Returns the active application object. | 
|  BottomNote1 | Sets and returns the Bottom Note 1 text for the referenced object. | 
|  BottomNote2 | Sets and returns the Bottom Note 2 text for the referenced object. | 
|  BottomNote3 | Sets and returns the Bottom Note 3 text for the referenced object. | 
|  BottomNoteAngle | Returns the bottom note angle of the referenced ModelWeld object. | 
|  BottomNoteCSize | Returns the bottom note compound size of the referenced ModelWeld object. | 
|  BottomNoteDepth | Returns the bottom note depth of the referenced ModelWeld object. | 
|  BottomNoteZ | Sets and returns the Bottom Note Z text for the referenced object. | 
|  BottomPosOffset | Returns the bottom position offset of the referenced ModelWeld object. | 
|  BottomTreatmentType | Sets and returns the treatment display style to use for the bottom treatment portion of the referenced object. | 
|  BottomType | Sets and returns the bottom type for the referenced object. | 
|  BottomTypeCompound | Returns the bottom weld compound symbol type of the referenced ModelWeld object. | 
|  CenterType | Sets and returns the center type for the referenced object. | 
|  CrossSectionArea | Returns the cross-sectional area of the referenced ModelWeld object. | 
|  DashLine | Sets and returns the relative position of the dash lines for the referenced weld symbol object. | 
|  Length | Specifies the length of the referenced object. | 
|  OffsetTopBottom | Specifies whether the top and bottom weld types are offset or aligned. | 
|  Parent | Returns the parent object for the referenced object. | 
|  Symmetrical | Specifies whether or not the referenced object is symmetrical. | 
|  Tail | Specifies whether the less than symbol appears at the end of the breaklline. | 
|  TailNote | Sets and returns the tail note text. | 
|  TailNote2 | Sets and returns the tail note text for the referenced ModelWeld object. | 
|  TopNote1 | Sets and returns the Top Note 1 text. | 
|  TopNote2 | Sets and returns the Top Note 2 text. | 
|  TopNote3 | Sets and returns the Top Note 3 text. | 
|  TopNoteAngle | Returns the top note angle of the referenced ModelWeld object. | 
|  TopNoteCSize | Returns the top note compound size of the referenced ModelWeld object. | 
|  TopNoteDepth | Returns the top note depth of the referenced ModelWeld object. | 
|  TopNoteZ | Sets and returns the Top Note Z text. | 
|  TopPosOffset | Returns the top position offset of the referenced ModelWeld object. | 
|  TopTreatmentType | Sets and returns the display style to use for the top treatment portion of the referenced object. | 
|  TopType | Sets and returns the top type for the referenced object. | 
|  TopTypeCompound | Returns the top weld compound symbol type of the referenced ModelWeld object. | 
|  WeldAllAround | Specifies whether or not the 'weld all around' display style is included in the referenced object. | 
|  WeldBeadWeldImport | Specifies the weld import status of the referenced weld bead. | 
|  WeldBeadWeldmentShape | Specifies the weldment shape of the referenced weld bead. | 
|  WeldBeadWeldmentType | Specifies the weldment type of the referenced weld bead. | 
|  WeldBeadWeldStandard | Specifies the weld standard of the referenced weld bead. | 
|  WeldBeadWeldType | Specifies the weld type of the referenced weld bead. | 
|  WeldInField | Specifies whether or not the 'weld in field' display style is included in the referenced object. | 
|  ZSymbol | Specifies whether or not the Z weld symbol modifier is included in the referenced object. |