| Solid Edge Draft Type Library : SheetSetup Object |
ClearDrawingViewForSheetScale | Allows the user to set the sheet scale manually through SetDefaultDrawingViewScale |
GetDefaultDrawingViewScale | Gets the default drawing view scale. |
GetDefaultDrawingViewScaleFactor | Gets the default drawing view scale factor. |
SetDefaultDrawingViewScale | Manually sets the default drawing view scale. This call has no effect if the scale is being derived from a drawing view. |
Application | Returns the active application object. |
DefaultDrawingViewScaleOption | Sets and returns the default drawing view scale option. |
DrawingViewForSheetScale | Drawing View from which sheet scale will be derived. |
IsManualSheetScale | Returns true if sheet scale is not controlled by a drawing view. |
Parent | Returns the parent object for the referenced object. |
SheetHeight | Sets and returns the height of the sheet for the referenced SheetSetup object. |
SheetSizeOption | Sets and returns the size of the sheet. |
SheetWidth | Sets and returns the width of the sheet. |