Solid Edge Draft Type Library
BeginSheetViewDynamics Method
Description
Sets up the view for fast display dynamics.
Syntax
Visual Basic
Public Sub BeginSheetViewDynamics() 
Example
Imports System.Runtime.InteropServices

Public Class frm2DDisplayProformance
    Private Sub btn2DDisplayProformance_Click(sender As System.Object, e As System.EventArgs) Handles btn2DDisplayProformance.Click
        Dim objApplication As SolidEdgeFramework.Application = Nothing
        Dim objDraftDoc As SolidEdgeDraft.DraftDocument = Nothing
        Dim objSheetWin As SolidEdgeDraft.SheetWindow = Nothing
        Dim objType As Type = Nothing
        Try
            ' Create/get the application with specific settings
            objApplication = Marshal.GetActiveObject("SolidEdge.Application")

            If objApplication Is Nothing Then
                ' Get the type from the Solid Edge ProgID
                objType = Type.GetTypeFromProgID("SolidEdge.Application")
                ' Start Solid Edge
                objApplication = Activator.CreateInstance(objType)
                ' Make Solid Edge visible
                objApplication.Visible = True
            End If

            ' Get the reference to the open document
            objDraftDoc = objApplication.Documents.Add("SolidEdge.Draftdocument")
            objSheetWin = objDraftDoc.Windows

            'Sets up the view for fast display 
            Call objSheetWin.BeginSheetViewDynamics()
            Call objSheetWin.ZoomArea(objSheetWin.Left, objSheetWin.Top, objSheetWin.Width, objSheetWin.Height)
            Call objSheetWin.ZoomArea(objSheetWin.Left + 10, objSheetWin.Top + 10, objSheetWin.Width - 10, objSheetWin.Height - 10)
            Call objSheetWin.ZoomArea(objSheetWin.Left + 20, objSheetWin.Top + 20, objSheetWin.Width - 20, objSheetWin.Height - 20)
            Call objSheetWin.ZoomArea(objSheetWin.Left + 30, objSheetWin.Top + 30, objSheetWin.Width - 30, objSheetWin.Height - 30)
            Call objSheetWin.ZoomArea(objSheetWin.Left + 40, objSheetWin.Top + 40, objSheetWin.Width - 40, objSheetWin.Height - 40)
            Call objSheetWin.ZoomArea(objSheetWin.Left + 50, objSheetWin.Top + 50, objSheetWin.Width - 50, objSheetWin.Height - 50)
            'Ends the fast display dynamics
            Call objSheetWin.EndSheetViewDynamics()
        Catch ex As Exception
            MsgBox(ex.ToString)
        End Try
    End Sub
End Class
See Also

SheetWindow Object  | SheetWindow Members

Send comments on this topic.